Simulator Analysis Event Description

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   



Contents

C6000 Simulator Analysis Events Description

The C6000 simulator analysis event description is available in this page.


Cycle Events

Event Name Description
cycle.CPU

A CPU cycle consumed

This event includes instruction execution cycle , cross path stalls and memory bank conflict stalls. This does not include memory-access stalls (except the L1D memory bank conflict stalls in the case of Functional Simulator)

cycle.Total This event count includes instruction execution cycle count, all stalls (including pipeline stalls), memory latency and system effects.


CPU Events

Event Name Description
CPU.access.data.read Data read access from CPU
CPU.access.data.write Data write access from CPU
CPU.access.summary Data read or write access from CPU
CPU.discontinuity.branch A discontinuity (or jump) occurred in the PC value due to the execution of a branch instruction.
CPU.discontinuity.interrupt.summary A discontinuity (or jump) occurred in the PC value due as a result of an interrupt taken 
CPU.discontinuity.summary PC discontinuity.  
CPU.execute_packet An execuet-packet decoded.Event will be reported against the address of the first instruction.
CPU.instruction.decoded An Instruction decoded
CPU.instruction.executed An instruction executed  
CPU.instruction.condition_false The Predicate for the instruction evaluated to false
CPU.NOP No-Operation cycles executed.
CPU.idle CPU idle cycles (IDLE instuction)
CPU.stall.mem.L1P Stall cycles due to L1P accesses.
CPU.stall.mem.L1D Stall cycles due to L1D accesses (e.g. L2 SRAM access missing in L1D).
CPU.stall.mem.bank_conflict Stall cycles due to bank conflicts.
CPU.stall.mem = CPU.stall.mem.L1P + CPU.stall.mem.L1D + CPU.stall.mem.bank_conflict.
CPU.stall.crosspath Stall cycles due to Cross Path data access.
CPU.stall.summary = CPU.stall.mem + CPU.stall.crosspath.


Miscellaneous events not exposed by default

These events are available on C64x+, C647x, miniC64 and C66x ISAs.

In order to enable below set of events (IPC and functional unit utilization),

User has to edit the simulator configuration file and add the line POWER_PROFILING ON; To do this, search for TYPE CPU; line and add the power profiling line after that.

For eg., if using on TCI6616 simulator, open the tisim_tci6616.cfg from simulation*/bin/configurations area.

MODULE CPU0;

  ....

 TYPE CPU;

 POWER_PROFILING ON;

  ...

END CPU0;


IPC events

Event Name
Description
CPU.IPC_Cycles.ipc_of_0
0 Instruction per cycle
CPU.IPC_Cycles.ipc_of_1
1 Instruction per cycle
CPU.IPC_Cycles.ipc_of_2
2 Instruction per cycle
CPU.IPC_Cycles.ipc_of_3
3 Instruction per cycle
CPU.IPC_Cycles.ipc_of_4
4 Instruction per cycle
CPU.IPC_Cycles.ipc_of_5
5 Instruction per cycle
CPU.IPC_Cycles.ipc_of_6
6 Instruction per cycle
CPU.IPC_Cycles.ipc_of_7
7 Instruction per cycle
CPU.IPC_Cycles.ipc_of_8
8 Instruction per cycle

Functional unit utilization events

Event Name
Description
CPU.func_unit_cycles.L1
Instructions(cpu cycles) executed on L1 unit
CPU.func_unit_cycles.M1
Instructions(cpu cycles) executed on M1 unit
CPU.func_unit_cycles.S1
Instructions(cpu cycles) executed on S1 unit
CPU.func_unit_cycles.D1
Instructions(cpu cycles) executed on D1 unit
CPU.func_unit_cycles.L2
Instructions(cpu cycles) executed on L2 unit
CPU.func_unit_cycles.M2
Instructions(cpu cycles) executed on M2 unit
CPU.func_unit_cycles.S2
Instructions(cpu cycles) executed on S2 unit
CPU.func_unit_cycles.D2
Instructions(cpu cycles) executed on D2 unit


Cache Events

Event Name Description
L1D.hit.read CPU read access is a hit in L1D
L1D.hit.write CPU write access is a hit in L1D
L1D.hit.summary Total hits in L1D Cache
L1D.miss.read CPU read access is a miss in L1D
L1D.miss.write CPU write access is a miss in L1D
L1D.miss.summary Total misses in L1D Cache
L1D.access All data accesses from CPU to L1D
L1D.miss.conflict L1D cache miss due to conflict (a miss is said to be of type conflict if the access is a miss in the actual cache, whereas it would have been a hit in a fully associative cache of the same size)
L1D.miss.non_conflict L1D cache miss that is not due to conflict (such misses are either cold misses or capacity misses)
L1D.miss.non_cacheable L1D miss due to an access whose address is in a non-cacheable region (due primarily to the MAR register settings)
CPU.stall.mem.L1D CPU stall cycles due to L1D
L1D.stall.write_buf_full A write buffer exists between the L1D and L2 caches. There can be up to four non-mergeable write misses outstanding in the write buffer without stalling the CPU. If a write miss occurs when the write buffer is full, this event will occur.
L1P.hit L1P cache hit
L1P.miss.summary Total L1P cache misses
L1P.access all program fetches from CPU to L1P
L1P.miss.conflict L1P cache misses that are conflict misses (a conflict miss is a miss in the actual cache, whereas the access would be a hit in a fully associative cache of the same size)
L1P.miss.non_conflict L1P cache misses that are not due to conflicts (a non conflict miss is either a cold miss or a capacity miss)
L1P.miss.non_cacheable L1P cache miss due to an access whose address is in a non-cacheable region (due primarily to the MAR register settings)
CPU.stall.mem.L1P CPU stall cycles due to L1P
L2.cache.hit.data.read L2 cache hits for L1D read requests
L2.cache.hit.data.write L2 cache hits for L1D write requests
L2.cache.hit.prog L2 cache hits for requests from L1P
L2.cache.hit.summary Total L2 Cache hits for requests from L1D and L1P
L2.cache.hit.data.summary Totol L2 cache hits for requests from L1D
L2.cache.miss.data.read L2 cache misses for read requests from L1D
L2.cache.miss.data.write L2 cache misses for write requests from L1D
L2.cache.miss.prog L2 cache misses for requests from L1P
L2.cache.miss.summary Total L2 cache misses for requests from L1D and L1P.
L2.cache.miss.data.summary Total L2 cache misses for requests from L1D
L2.cache.miss.conflict L2 cache misses that are of type conflict ( a miss is said to be a conflict miss if the access is a miss in the actual cache, whereas it would have been a hit in a fully associative cache of the same size)
L2.cache.miss.non_conflict L2 cache misses that are not due to conflict (such misses are either cold misses or capacity misses)
L2.cache.miss.non_cacheable L2 cache misses for requests whose addresses are in non-cacheable regions (due primarily to MAR register settings)
L2.cache.access Total L2 cache requests from L1D and L1P
L2.SRAM.data.read L1D read from L2 SRAM
L2.SRAM.data.write L1D write to L2 SRAM
L2.SRAM.data.summary Total L1D accesses to L2 SRAM
L2.SRAM.prog L1P read from L2 SRAM
L2.SRAM.dma.read DMA Read access to L2 SRAM
L2.SRAM.dma.write DMA Write access to L2 SRAM
L2.SRAM.dma.access DMA access to L2 SRAM
L1P.victim L1P miss caused a victim in L1P (a L1P victim is caused by an L1P miss requiring eviction).
L1P.snoop.hit L2 snoop request that is a hit in L1P
L1P.snoop.hit.victim L1P snoop hits caused due to L2 victim
L1P.snoop.hit.dma L1P snoop hits caused due to DMA access to L2 SRAM
L1P.snoop.hit.cache_control_op L1P snoop hits caused due to cache control operations (flush, write back operations to L2)
L1P.snoop.miss L2 snoop requests that miss L1P
L1P.snoop.summary Total snoops to L1P (misses, clean hits, dirty hits)
L1D.victim.dirty L1D victims that are dirty (that is, eviction of a line that has been modified)
L1D.victim.summary Total L1D victims (a L1D victim is caused by an L1D miss requiring eviction).
L1D.snoop.hit.summary L2 Snoop request that is a hit in L1D
L1D.snoop.hit.victim L1D snoop hits caused due to L2 victim
L1D.snoop.hit.dma L1D snoop hits caused due to DMA access to L2 SRAM
L1D.snoop.hit.cache_control_op L1D snoop hits caused due to cache control operations (flush, write back operations to L2)
L1D.snoop.hit.dirty L1D snoop hit to an L1D line that has been modified
L1D.snoop.hit.dirty.victim L1D snoop hits to dirty lines caused due to L2 victim
L1D.snoop.hit.dirty.dma L1D snoop hits to dirty lines caused due to DMA access to L2 SRAM
L1D.snoop.miss L2 snoop request that is a miss in L1D
L1D.snoop.summary Total L1D snoops (misses, clean hits, dirty hits)
L1D.miss.write_merge A write buffer exists between the L1D and L2 caches. The write buffer allows merging of write requests. It merges two write misses into a single transaction provided the following rules are obeyed: The double-word address of the two accesses is the same; the two accesses are to L2 configured as SRAM; the oldest write has just been placed in the write buffer queue; the newest write has not been placed in the buffer queue
L2.cache.victim.dirty Victimized line in L2 has been modified (needs to be saved to corresponding memory locations)
L2.cache.victim.data L1D access caused victim in L2
L2.cache.victim.prog L1P access caused victim in L2
L2.cache.victim.summary L2 access that causes a L2 victim (victim is caused by a miss requiring line eviction)
E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Simulator Analysis Event Description here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox