Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Sitara Linux SDK Creating a SD Card with Linux

From Texas Instruments Wiki
Jump to: navigation, search


Return to the Sitara Linux Software Developer's Guide

TIBanner.png

Overview

Starting with the Sitara Linux SDK version 05.04.00.00 there is now a script in the <SDK INSTALL DIR>/bin directory named create-sdcard.sh. The purpose of this script is to create SD cards for the following high-level use cases:

  1. Create the SD card using default images from the Sitara Linux SDK
  2. Create the SD card using custom images
  3. Create the SD card using partition tarballs (This is not common and is used most often by board vendors)

The script will give you information about each step, but the following sections will go over the details for the use cases above and walk you through how to use the script as well.

Common Steps

No matter which use case above that you are creating an SD card for the following steps are the same.

Invoking the Script

The create-sdcard.sh script can be run from any location but must be run with root permissions. This usually means using the sudo command to start execution of the script. For example:

host# sudo <SDK INSTALL DIR>/bin/create-sdcard.sh

If you fail to execute the script with root permissions you will receive a message that root permissions are required and the script will exit.

Select the SD Card Device

The first step of the script will ask you to select the drive representing the SD card that you want to format. In most cases your host root file system drive has been masked off to prevent damage to the host system. When prompted enter the device number corresponding to the SD card. For example if the output looks like:


Availible Drives to write images to: # major minor size name 1: 8 16 7761920 sdb Enter Device Number: You would enter 1 to select the sdb device

Re-Partitioning the SD Card

Any partitions of the device that are already mounted will be un-mounted so that the device is ready for partitioning.

If the SD Card already has partition you will see a prompt like the following asking you if you would like to repartition the card. If the card was not already partitioned then this step will be skipped and you can move on to the next step.

Would you like to re-partition the drive anyways [y/n] :
  • Options:
    • y - This will allow you to change the partitioning of the SD card. For example if you have a 3 partition card and want to create a 2 partition card to give additional storage space to the root file system you would select y here.
      NOTE: This operation WILL ERASE the contents of your SD card
    • n - If the SD card already has the desired number of partitions then this will leave the partitioning alone. If you select n here skip on to the Installing SD Card Content section.

Select Number of Partitions

You should now see a prompt like the following which will ask you how many partitions you want to create for the SD card

Number of partitions needed [2/3] :
  • Options:
    • 2 - This is the most common use case and will give the most space to the root file system.
    • 3 - This case should only be used by board manufacturers making SD cards to go in the box with the EVM. This requires access to the partition tarballs used for Out-Of-Box SD cards. This option should be selected if you are going to follow the SD card using partition tarballs steps below

After selecting the number of partitions move on to the next section.

Installing SD Card Content

After the SD card is partitioned you will be prompted whether you want to continue installing the file system or safely exit the script.

  • Options:
    • y - Selecting yes here will begin the process of installing the SD card contents. This operation WILL ERASE any existing data on the SD card. Refer to one of the following sections for additional instructions depending on which use case you are creating an SD card for
    • n - Selecting no here will allow you to have partitioned your card but will leave the partitions empty.

SD Card Using Default Images

The purpose of this section is to cover how to use the create-sdcard.sh script to populate an SD card that can be used to boot the device using the default images that ship with the Sitara Linux SDK.

NOTE: For devices like AM180x see the AM180x SD card boot section below for information on booting that device from an SD card. This script will create a card suitable for the root file system but additional steps are required to load the boot loaders from the SD card.

Prerequisites

  1. The Sitara Linux SDK is installed on your host system
  2. The SD card you wish to create is inserted into the host system and has a size sufficiently large to hold at least the bootloaders, kernel, and root file system.
  3. You have started running the script as detailed in the Common Steps section above.

Choose Install Pre-built Images

You should now see a prompt like:


################################################################################ Choose file path to install from 1 ) Install pre-built images from SDK 2 ) Enter in custom boot and rootfs file paths ################################################################################ Choose now [1/2] : You should choose option 1 to create an SD card using the pre-built images from the SDK.

If you executed this script from within the SDK then the script can determine the SDK path automatically and will start copying the contents to the SD card. Once the files are copied the script will exit.

If you executed the script from outside of the SDK (i.e. you copied it to some other directory and executed it there) please see the next section.

Enter SDK Path

In the case that the script was invoked from a directory without the SDK installation in the path, i.e. the script was copied to your home directory and executed there you may see a prompt like


no SDK PATH found Enter path to SDK : Enter the path to the SDK installation directory here. For example if the SDK was installed into the home directory of the sitara user the path to enter would be /home/sitara/ti-sdk-<machine>-<version>. You will be prompted to confirm the installation directory. The SD card will then be created using the default images and the script will exit when finished.

SD Card Using Custom Images

Often times you will use TFTP and NFS during development to transfer you kernel images and boot your root file systems respectively. Once you are done with your development you may want place these images onto an SD card so that they can be used stand-along without requiring a network connection to a server.

Prerequisites

  1. The Sitara Linux SDK is installed on your host system
  2. The SD card you wish to create is inserted into the host system and has a size sufficiently large to hold at least the bootloaders, kernel, and root file system.
  3. You have started running the script as detailed in the Common Steps section above.

Choose Custom Images

You should now see a prompt like:


################################################################################ Choose file path to install from 1 ) Install pre-built images from SDK 2 ) Enter in custom boot and rootfs file paths ################################################################################ Choose now [1/2] : Select option 2 to create an SD card with your custom images.

Select Boot Partition

You will now be prompted to provide a path to the location of the boot partition files. The prompt will explain the requirements of the files to be placed at the path, but the basic options are:

  1. Point to a tarball containing all of the files you want placed on the boot partition. This would include the boot loaders and the kernel image as well as any optional files like uEnv.txt
  2. Point to a directory containing the files for the boot partition like those in the first option.

The script is intelligent enough to recognize whether you provided a tarball or a directory path and will copy the files accordingly. You will be given a list of the files that are going to be copied and given the option to change the path if the list of files is not correct.

Select Root Partition

You will now be prompted to provide a path to the location of the root file sysetm partition files. The prompt will explain the requirements of the files to be placed at the path, but the basic options are:

  1. Point to a tarball of the root file system you want to use
  2. Point to a directory containing the root file sysetm such as an NFS share directory.

The script is intelligent enough to recognize whether you provided a tarball or a directory path and will copy the files accordingly. You will be given a list of the files that are going to be copied and given the option to change the path if the list of files is not correct.

SD Card Using Partition Tarballs

This option is meant for board vendors to create SD cards to go in the box with the EVM. It requires access to the three tarballs representing the the partitions of the SD card shipped with the EVM.

Prerequisites

  1. The Sitara Linux SDK is installed on your host system
  2. The SD card you wish to create is inserted into the host system and has a size sufficiently large to hold at least the bootloaders, kernel, and root file system.
  3. You have started running the script as detailed in the Common Steps section above.

Provide Tarball Location

After the SD card has been partitioned you will be prompted to

Enter path where SD card tarballs were downloaded :

Point to the directory containing the following tarball files:

  • boot_partition.tar.gz
  • rootfs_partition.tar.gz
  • start_here_partition.tar.gz

The script will show you the contents of the directory given and ask you to verify that the tarballs are present in that directory. The SD card will then be populated with the contents of the tarballs and be ready for inclusion in the box with the EVM.