SourceSafe plugin installation

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Overview:

There is a VSS plug-in for Eclipse that can be used to add Microsoft Visual SourceSafe integration into CCSv4.  More information on the plug-in is available at this link

Dependencies:

  1. CCSv4.x.  CCSv4.0 and later are based on the Eclipse open source software framework.
  2. SourceSafe client software installed.

Installation Procedure: 

1. Install JDT Unzip the JDT 3.2 runtime into the \eclipse folder in your CCSv4 installation.  The zip file contains plugins and features folders that need to be merged with the same folders in your CCSv4\eclipse folder so say yes to the prompts from windows to do this.

2. Download VSS Plug-in 

Download version 1.6.1 of the plug-in from here.  This should go to a page where you can download a zip file containing the latest plug-in.  When these instructions were written the latest version was 1.6.2 (do not install 1.6.2, you need 1.6.1, download the package that does NOT say Europa on it).

3. Close CCS

You need to close CCS as we will be adding a new plug-in.

4. Add plug-in to CCS

Copy the contents of the zip file into the CCSv4\eclipse\plugins folder.  i.e. copy the org.vssplugin_1.6.2 folder into your eclipse\plugins folder so that you get eclipse\plugins\org.vssplugin_1.6.1.

5. Restart CCS

When you restart CCS it will load the VSS plug-in.

6. Using VSS inside CCS

In CCS help there will now be a book called "VSS Plugin". If you click on the readme item inside this book it contains quite a bit of useful information on how to use this plugin.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox