SysLink FAQs

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Generic questions

Where do I get SysLink releases?

What do I get with SysLink, and how do I get started?

Each SysLink release is available as a full source release including:

To get started with SysLink, you can refer to the release documents mentioned in the release notes in the base of the product. Refer to the SysLink User Guide for high level information. The SysLink API Reference Guide provides details on the APIs, and the samples provided with SysLink demonstrate usage of the APIs.

The SysLink Install Guide provides installation and build instructions, as well as details on running the sample applications.

The Migration Guide gives migration information between DSPLink and SysLink.

What is the relation between SysLink and IPC software packages

SysLink and IPC packages are complementary packages.

If you are using Linux on the ARM and BIOS on a slave processor, then both SysLink and IPC packages needs to be used, since SysLink contains the required Linux-side components and IPC contains the BIOS side.

How does DSP/Link relate to SysLink/IPC packages?

Please refer to the following link: http://processors.wiki.ti.com/index.php/SysLink_Overview#How_is_SysLink_different_from_DSPLink

How to migrate from DSPLink to SysLink?

Please refer the SysLink Migration Guide for more information.

Build questions

Can I build both HLOS and RTOS sides of SysLink only on a Linux machine?

Yes! The SysLink make system supports build of both GPP and DSP-side on a Linux machine. In fact, it is advised to use this method when you are using Linux as the HLOS because:

Can I build SysLink RTOS side on Windows Machine?

Yes! The SysLink RTOS side code, including sample applications, can be built on a windows machine. Details are in the SysLink Install Guide.

How do I build SysLink Samples(HLOS/RTOS) for a particular Platform?

See the SysLink Install Guide.

Build warnings/errors! Where do I look?

Check out the Troubleshooting SysLink Build Issues article. This lists most of the common build failures and their possible causes, and suggests solutions.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox