TI-Android-GingerBread-2.3-DevKit-1.0 ReleaseNotes

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

TIBanner.png

Contents

TI Android GingerBread 2.3 DevKit 1.0 Release Notes

Release Notes - May 31, 2011

There is new release TI Android Gingerbread 2.3.4 DevKit v2.1 (July 11 2011) available for AM37x, AM35x.
Please refer to http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_ReleaseNotes

Introduction

This is TI-Android-GingerBread-2.3-DevKit-1.0 release based on Android GingerBread 2.3 for AM35x EVM, AM37x EVM, DM37x EVM, OMAP35x EVM, Beagleboard Rev Cx and Beagleboard XM platforms.

This release serves to provide


Component Version Base Repository Base Tag (or commit id)
OMAP Linux Kernel 2.6.32(Android Linux kernel version) The baseline was chosen from "PSP" release from http://arago-project.org/git/projects/linux-omap3.git OMAPPSP_03.00.01.06_baseline
U-Boot 2010.06.rc2 http://arago-project.org/git/projects/u-boot-omap3.git PSP 04.00.00.09
Android GingerBread 2.3 http://gitorious.org/rowboat TI-Android-GingerBread-2.3-DevKit-1.0.xml (without multimedia DSP acceleration),
TI-Android-GingerBread-DSP-2.3-DevKit-1.0.xml (with multimedia DSP acceleration)


The filesystem was built by integrating the sources from arowboat.org project hosted on arowboat gitorious Project using TI-Android-GingerBread-2.3-DevKit-1.0.xml or TI-Android-GingerBread-DSP-2.3-DevKit-1.0.xml manifest file.
The codebase for Linux kernel, SGX kernel drivers, U-Boot included in this release is also hosted at the following repositories:

Component Repository (Branch) Commit ID / Baseline
Bootloader http://gitorious.org/rowboat/u-boot-omap3 PSP 04.00.00.09
OMAP Linux Kernel http://gitorious.org/rowboat/kernel

(rowboat-eclair-2.6.32)

d9b04d8b50d19b7056ee051106057f703877dabc
SGX Release http://gitorious.org/rowboat/hardware-ti-sgx.git 3674b877cb6b7c6e0267cb46c02c0f2ef9958a7e
Adobe Flash 10 http://focus.ti.com/docs/toolsw/folders/print/adobeflash-a8.html v10.1.r105
TI DVSDK (for DM3730 only) http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/dvsdk/DVSDK_4_00/latest/index_FDS.html 4.01.00.09

For detailed information on the various software components included in the release and how to use them, please refer to the
http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3-DevKit-1.0_UserGuide.

The Android sources, SGX drivers, Kernel and U-Boot have been compiled with GNU Toolchain for ARM Processors from Android pre-built package
http://gitorious.org/rowboat/prebuilt/trees/rowboat-froyo/linux-x86/toolchain/arm-eabi-4.4.0


Documentation

Provides instructions on how to use the TI Android GingerBread 2.3 DevKit 1.0 package. A copy of the User Guide is included in the docs folder of the DevKit package. The User Guide also gives instructions on building the Android root filesystem using Android sources maintained on rowboat repositories.
Location  : http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3-DevKit-1.0_UserGuide

Provides instructions for Android developers to get access to Android sources for TI devices, setting up host environment for compilation and enabling debug environment to ease the app development, debugging and deployment. [edit]
Location  : http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3-DevKit-1.0_DeveloperGuide

Gives the benchmark numbers for various parameters and peripherals
Location  : http://processors.wiki.ti.com/index.php/Android_Benchmarks_DevKit2.3

Provides information on porting packages like WLAN/BT, Camera, PowerManagement, NAND UBIFS for other platforms,
Location  : http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3-DevKit-1.0_Porting_Guides

What's Supported

This SDK package includes support for the OMAP35x EVM, AM35x EVM, AM37x EVM, DM37x EVM, Beagleboard Rev Cx and Beagleboard XM.

Software features/components supported in this DevKit are


Complete directory structure of DevKit

  TI_Android_GingerBread_2_3_DevKit_1_0
      |-- Android_Source_Manifest
      |   |-- TI-Android-GingerBread-2.3-DevKit-1.0.xml
      |   `-- TI-Android-GingerBread-DSP-2.3-DevKit-1.0.xml
      |-- Documents
      |   |-- RowboPERF_User_Guide.pdf
      |   |-- Software_Manifests
      |   |-- Test_Performance_Results
      |   |   |-- CTS_Report.tar.gz
      |   |   |-- Performance_Results.pdf
      |   |   `-- Test_Results.pdf
      |   |-- TI-Android-GingerBread-2.3-DevKit-1.0_ReleaseNotes.pdf
      |   |-- TI-Android-GingerBread-2.3-DevKit-1.0_UserGuide.pdf
      |   `-- TI-Android-GingerBread-2.3-DevKit-1.0_DeveloperGuide.pdf 
      |-- Performance_Apps
      |   |-- 0xbench
      |   |-- 3D
      |   |-- Launcher2
      |   |-- rowboatBench
      |   |-- RowboPERF
      |   `-- StorageIO
      |-- Prebuilt_Images
      |   |-- AM35X
      |   |-- AM37X
      |   |-- beagleboard-rev-c4
      |   |-- beagleboard-xM
      |   |-- OMAP35X
      |   `-- DM37X
      |-- Tools
      |   |-- flash-utility.tar.gz
      |   |-- mk-bootscr
      |   |-- mk-mmc
      |   |-- pinmux-utility.tar.gz
      |   |-- signGP
      `-- Wireless
          `-- WL1271Android-patches.tar.gz


New in this Release



What's Not Supported


Installation and Usage

The DevKit release is maintained as a single "TI-Android-GingerBread-2.3-DevKit-1.0.tar.gz" at http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_GingerBread_2_3_DevKit_1_0/index_FDS.html and individual component packages.

The package for DM37x EVM is "DM37x EVM" in the 'DSP Accelerated Multimedia' section in the link above.

On a Linux Host PC download the single release package and execute the following components

    #> tar -xzvf TI-Android-GingerBread-2.3-DevKit-1.0.tar.gz

Please refer to the TI-Android-GingerBread-2.3-DevKit-1.0 User Guidefor more information on how to install and use the DevKit

Other individual packages can be used to refer to respective components.

The md5 checksums are provided for users to double check or verify the completeness of downloaded package.


Device Support

This release supports the following Texas Instruments devices

This release supports the following platforms


Known Issues


Component
Issue Description
Workaround
Comments
Hardware
USB EHCI Host port doesn't work on few AM37x EVMs
No workaround
No fix available currently, suggestion is to use TI USB PHY
Software
Pinmux Utility: could not resize the GUI, so could not see what the other button on the bottom right corner is.
User may need to adjust the display resolution of their Windows PC
To be fixed in future releases
Software
Pinmux Utility: could not resize the GUI, so could not see what the other button on the bottom right corner is.
Pinmux utility requires Left-click to select a peripheral interface cell. The cell should be auto selected when user right-click it.
No impact to functionality. Just a note on the user interface.
To be fixed in future releases
Software
AM35x EVM platform booting doesn't continue after below shown messages
AudioPolicyService not published, waiting...
This happens if the Filesystem was not unmounted properly.
Look for the process ID in the console messages.
Kill the process with "kill" command.
This will not appear again.

Software
ARM performance data is not shown sometimes when RowboPERF runs ARM bechmarks
The CPU tests in Rowboat Bench will generate ARM benchmarks, this can be used for same purpose

Software
Netperf Ethernet performance is low when using a buffer size of 8192
No workaround
Other buffer sizes give better performance, see the performance results sheet for this release
Software
System does not obtain IP address automatically after booting
Use netcfg <eth0> dhcp on the console.
See user guide for more details
Software
Graphics Screen resolution is changed after suspend/resume sequence
No workaround
This is only with one of the demo app, this will not affect UI. The other 3D tests in RowboPerf work good.
Software
SUSPEND power consumption is too high (~85mw)
No workaround
To be done
Software
Acquiring different WakeLocks doesn't change power consumption
No workaround
To be done
Hardware
Video display is not clear when displayed over s-video Not observed on LCD TVs
No workaround
Not consistent on all TVs
Tool
Flashing NAND using flash utility v1.3 doesn’t work over UART
USB can be used with same utility to flash the NAND

Software
"Four Dalvik VM unit tests failed during testing
failed: 057-iteration-performance
failed: 062-character-encodings
failed: 063-process-manager
failed: 071-dexfile
No workaround
To be done
Software
When the system is set to display through the S-video output, the display start flickering after a wake-up from suspend
No workaround
To be done
N/A system boot-up takes too long, UI is less responsive, or video playback is sluggish use the SD cards listed in the "SD Card Recommendations" section in the User Guide


Version

This is Release TI Android GingerBread 2.3 DevKit 1.0

The release is available from http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_GingerBread_2_3_DevKit_1_0/index_FDS.html

Technical Support and Product Updates

For further information or to report any problems, contact http://e2e.ti.com/android or http://support.ti.com.
For community support join http://groups.google.com/group/rowboat
For IRC #rowboat on irc.freenode.net
To raise any defect for this release please use http://code.google.com/p/rowboat/issues/list

E2e.jpg For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article TI-Android-GingerBread-2.3-DevKit-1.0 ReleaseNotes here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox