Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

TI-Android-ICS-4.0.3-DevKit-3.0.0 PerformanceBenchmark

From Texas Instruments Wiki
Jump to: navigation, search

TIBanner.png

Introduction

This page provides comparison among various TI processors running TI's Android-DevKit. Data published here is for the latest version of released Android-DevKit. Items yet to be measured are marked "TBD" and those that are not applicable to a particular platform are marked "N/A".

Platform Benchmarks

This is a collection of benchmarks comparing mainly CPU speed and other data transfer operations. In below tests, AM3730@1GHz, BeagleXM@1GHz, and Flashboard@1GHz.

RowboPerf: ARM

See RowboPERF User Guide for more information about these metrics. The RowboPerf application calls native executables compiled with Android's NDK to perform these tests.

ARM Benchmark ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
Dhrystone 1138 DMIPS 1138 DMIPS 1422 DMIPS
Whetstone 500 MIPS 500 MIPS 250 MIPS
Linpack 33805 Kflops 33805 Kflops 23755 Kflops

RowboPERF: 0xBench

See RowboPERF User Guide for more information about these metrics.

Linpack ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
Mflops/s 19.28 18.8 18.53
Scimark2 ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
Composite 23.94 24.24 23.9
Fast Fourier Transform 14.34 14.7 14.22
Jacobi Successive Over-relaxation 45.67 46.21 45.45
Monte Carlo integration 6.34 7.12 7.5
Sparse matrix multiply 19.04 19.1 18.93
dense LU matrix factorization 34.28 34.07 33.4

Boot Time

Numbers shown here measure the time from start of loading the kernel image to appearance of Android's Home Screen. These measurements are done using the default (pre-built) images provided with the DevKit. Please note that the very first time you boot your device, the boot time will be significantly higher.

Time (secs) ICS 4.0.3 Devkit 3.0.0
AM37302 BeagleXM3 Flashboard2
SD First Boot Time1 74 sec 134 sec 70 sec
SD Boot Time 37 sec 50 sec 38 sec

1 First boot time refers to first time the system is booted with a freshly created SD card.
2 Sandisk Extreme, SD HCI, class 10, 4 GBytes, PN:SDSDRX3-4096-A21, SD card used for the test.
3 Trascend, SD HCI, class 10, 4 GBytes, PN:TS4GUSDC10, micro-SD card used for the test.

EDMA Test

Need to devise this test.

Memory Bandwidth

Need to devise this test.


Browser Performance

Sunspider

These metrics were collected using the well-known Sunspider performance benchmarks available at http://www2.webkit.org/perf/sunspider-0.9/sunspider.html

Sunspider ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
3d 628.9 ms +/- 5.7% 610.4 ms +/- 4.7% 613.4 ms +/- 4.6%
access 282.4 ms +/- 9% 294.4 ms +/- 6.4% 283.2 ms +/- 6.5%
bitops 194.1 ms +/- 12.1% 182 ms +/- 2.3% 185.5 ms +/- 5.9%
controlflow 19.4 ms +/- 1.9% 19.9 ms +/- 1.1% 20.1 ms +/- 1.1%
crypto 193.7 ms +/- 1.2% 198.4 ms +/- 3.7% 209.9 ms +/- 4.7%
date 540.3 ms +/- 2.8% 547 ms +/- 1.4% 565.9 ms +/- 0.7%
math 234.6 ms +/- 3.2% 229.4 ms +/- 2.4% 232.5 ms +/- 3%
regexp 129.4 ms +/- 0.9% 130.6 ms +/- 0.6% 132.9 ms +/- 0.2%
string 1027.5 ms +/- 0.8% 1038.4 ms +/- 1.3% 1054.4 ms +/- 0.4%
Total 3250 ms +/- 1.4% 3250.5 ms +/- 1% 3297.8 ms +/- 1%

V8

These metrics were collected using the v8 performance benchmarks available at http://v8.googlecode.com/svn/data/benchmarks/v6/run.html

V8 ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
richards 1098.00 1139.00 1123.00
deltablue 803 887 991
crypto 1121 1114 1106
raytrace 768 762 726
earleyboyer 1551 1556 1525
regexp 182 238 237
splay 280 336 470
Score 620 727 764

AcidTests

These metrics were collected using the acid browser tests available at http://acid3.acidtests.org/

Acid3 ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
Total 100/100 100/100 100/100


File Storage Performance

These tests were performed using the StorageIO application provided in RoboPerf. The application measures the write and read speed of different storage devices using several block sizes. For these tests the file size chosen was 100 MBytes. In order for the application to run the storage device chosen for the test must be mounted in the Android file system and a have read and write access. All the tests were perform on devices with a vfat file system.

MMC/SD Performance

Throughput (MB/s) ICS 4.0.3 Devkit 3.0.0
AM37301 BeagleXM2 Flashboard1
Throughput CPU Load (%)3 Throughput CPU Load (%)3 Throughput CPU Load (%)3
Write, bs=100 KiBytes 8.749 25.75 (max 76.08) 5.508 15.34 (max 59.68) 10.085 24 (max 70.83)
Write, bs=256 KiBytes 9.081 24.67 (max 78.74) 5.568 17.55 (max 61.48) 9.733 26.32 (max 74.07)
Write, bs=512 KiBytes 9.027 24.61 (max 73.43) 5.603 16.46 (max 63.06) 9.698 26.13 (max 73.15)
Write, bs=1024 KiBytes 8.738 22.8 (max 77.29) 5.162 12.69 (max 59.11) 9.756 22.73 (max 70.85)
Write, bs=5120 KiBytes 8.937 23.59 (max 72.46) 5.586 12.06 (max 35.86) 9.812 25.47 (max 72.73)
Read, bs=100 KiBytes 14.108 25.75 (max 76.08) 13.311 15.34 (max 59.68) 14.046 24 (max 70.83)
Read, bs=256 KiBytes 14.598 24.67 (max 78.74) 13.247 17.55 (max 61.48) 14.483 26.32 (max 74.07)
Read, bs=512 KiBytes 14.642 24.61 (max 73.43) 13.144 16.46 (max 63.06) 14.503 26.13 (max 73.15)
Read, bs=1024 KiBytes 14.632 22.8 (max 77.29) 13.483 12.69 (max 59.11) 14.657 22.73 (max 70.85)
Read, bs=5120 KiBytes 14.818 23.59 (max 72.46) 13.589 12.06 (max 35.86) 14.787 25.47 (max 72.73)

1 Sandisk Extreme, SD HCI, class 10, 4 GBytes, PN:SDSDRX3-4096-A21, SD card used for the test.
2 Trascend, SD HCI, class 10, 4 GBytes, PN:TS4GUSDC10, micro-SD card used for the test.
3 CPU Load values for write and read are the same because the read and write throughput are measure in one shot, and CPU Load is measured during the whole time the test in ran.

USB Performance

Throughput (MB/s) ICS 4.0.3 Devkit 3.0.0
AM37301 BeagleXM1
Throughput CPU Load (%)2 Throughput CPU Load (%)2
Write, bs=100 KiBytes 17.386 30.72 (max 74.52) 15.877 27.98 (max 74.64)
Write, bs=256 KiBytes 18.245 31.48 (max 79.23) 17.899 27.17 (max 70.67)
Write, bs=512 KiBytes 17.543 30.65 (max 74.4) 18.144 30.46 (max 71.63)
Write, bs=1024 KiBytes 18.920 30.98 (max 76.44) 15.875 27.98 (max 70.67)
Write, bs=5120 KiBytes 19.138 31.44 (max 76.67) 16.011 28.21 (max 71.98)
Read, bs=100 KiBytes 22.028 30.72 (max 74.52) 21.478 27.98 (max 74.64)
Read, bs=256 KiBytes 22.107 31.48 (max 79.23) 21.562 27.17 (max 70.67)
Read, bs=512 KiBytes 21.727 30.65 (max 74.4) 21.655 30.46 (max 71.63)
Read, bs=1024 KiBytes 21.868 30.98 (max 76.44) 21.682 27.98 (max 70.67)
Read, bs=5120 KiBytes 23.327 31.44 (max 76.67) 21.768 28.21 (max 71.98)

1 Western Digital Elements, 1 TByte, USB 2.0, 480 Mb/s Max transfer rate, PN:WDBAAU0010HBK, external hard drive used for the test.
2 CPU Load values for write and read are the same because the read and write throughput are measure in one shot, and CPU Load is measured during the whole time the test in ran.

Connectivity Performance

These tests provide throughput comparison across commonly used transports/mediums.

Ethernet

Measures TCP Throughput between Server (running on Host PC) and Client (Android Platform) using different buffer sizes (bs in bytes) Both Server and client uses the Netperf utility. For more information about Netperf, please see Netperf Home page

TCP Throughput ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
bs=16 KiBytes 56.71 Mb/s 93.83 Mb/s Mb/s
bs=32 KiBytes 55.81 Mb/s 93.89 Mb/s Mb/s
bs=64 KiBytes 55.17 Mb/s 93.76 Mb/s Mb/s
bs=128 KiBytes 54.74 Mb/s 94.05 Mb/s Mb/s

Wireless LAN (WiFi)

Measures TCP Throughput between Server (running on Host PC) and Client (Android Platform) using different buffer sizes (bs in bytes) Both Server and client uses the Netperf utility. For more information about Netperf, please see Netperf Home page

Non-Secure

The CPU load shown is the highest number observed while running TOP for the duration of the test.

Non-Secure ICS 4.0.3 Devkit 3.0.0
AM3730 Flashboard
TCP Throughput WLAN driver Load (%) Total CPU load % TCP Throughput WLAN driver Load (%) Total CPU load %
bs=16 KiBytes 8.52 Mb/s 11.61 (max 17.59) 27.33 Mb/s 22.88 (max 28.79)
bs=32 KiBytes 12.09 Mb/s 12.6 (max 15.76) 30.16 Mb/s 24.25 (max 28.5)
bs=64 KiBytes 11.31 Mb/s 11.54 (max 15.66) 30.54 Mb/s 22.04 (max 25.51)
bs=128 KiBytes 9.21 Mb/s 10.4 (max 17.59) 30.4 Mb/s 23.03 (max 31.12)

Secure

These tests were run with a buffer size of 64 KiBytes (i.e. 64*1024 bytes). The CPU load shown is the highest number observed while running TOP for the duration of the test.

Secure ICS 4.0.3 Devkit 3.0.0
AM3730 Flashboard
TCP Throughput WLAN driver Load (%) Total CPU load % TCP Throughput WLAN driver Load (%) Total CPU load %
WPA-PSK Authentication 12.28 Mb/s 14.97 (max 21.88) 21.04 Mb/s 19.24 (max 24.87)
WPA2-PSK Authentication 12.4 Mb/s 12.22 (max 16.84) 28.24 Mb/s 20.88 (max 29.08)
WEP 40bit Encryption 11.1 Mb/s 14.34 (max 19.27) 21.06 Mb/s 19.39 (max 24.49)
WEP 128bit Encryption 11.74 Mb/s 15.29 (max 21.21) 21.1 Mb/s 20.75 (max 26.6)

ADB

Measure Android Debug Bridge (ADB) throughput between Host PC and Android device by pushing and pulling a 20MB file with random content 10 times. TX and RX numbers are from the Host PC point of view, so TX is measured by doing "adb push" on the Host PC.

USB

ADB USB Throughput ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
TX 2211.4 KB/s 2252 KB/s 2595.10 KB/s
RX 5365.20 KB/s 5975 KB/s 5514 KB/s

Ethernet

ADB Ethernet Throughput ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
TX 2806.8 KB/s 2870.6 KB/s 2734 KB/s
RX 2174.5 KB/s 2316.5 KB/s 2264.8 KB/s


Graphics Performance

RowboPERF: 0xBench 2D

See RowboPERF User Guide for more information about these metrics.

2D ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
Frame Per Sec Total CPU Load (%) Frame Per Sec Total CPU Load (%) Frame Per Sec Total CPU Load (%)
Draw Canvas (fps) 59.06 29.53 (max 78.57) 59.9 29.77 (max 69.23) 60.65 35.37 (max 76.1)
Draw Circle (fps) 48.86 95.63 (max 99.04) 53.75 93.13 (max 98.09) 51.37 96.91 (max 98.58)
Draw Circle2 (fps) 57.78 47.02 (max 87.44) 57.34 52.01 (max 79.13) 53.6 65.16 (max 78.74)
Draw Rect (fps) 35.9 82.63 (max 99.04) 31.73 85.11 (max 99.04) 29.55 87.09 (max 99.04)
Draw Arc (fps) 50.41 78.31 (max 88.29) 51.51 75.9 (max 84.83) 46.71 82.51 (max 92.23)
Draw Image (fps) 57.96 78.93 (max 87.68) 40.51 91.15 (max 100) 28.72 95.76 (max 100)
Draw Text (fps) 56.64 80.47 (max 94.26) 57.68 81.6 (max 94.26) 56.4 84.65 (max 99.04)

RowboPERF: 0xBench 3D

See RowboPERF User Guide for more information about these metrics.

3D ICS 4.0.3 Devkit 3.0.0
AM3730 BeagleXM Flashboard
Frames per Sec Total CPU load (%) Frames per Sec Total CPU load (%) Frames per Sec Total CPU load (%)
OpenGL Cube (fps) 58.3 26.62 (max 86.98) 59.33 26.37 (max 65.31) 59.87 28.98 (max 82.61)
OpenGL Blending (fps) 61.77 22.03 (max 89.42) 63.19 20.50 (max 76.44) 63.76 22.75 (max 82.61)
OpenGL Fog (fps) 61.66 21.46 (max 86.06) 63.12 21.24 (max 81.07) 63.73 22.44 (max 83.57)
OpenGL Teapot (fps) 60.6 40.45 (max 89.42) 60.60 40.25 (max 80.86) 60.59 43.43 (max 85.58)


MultiMedia Performance

Tests to measure video, audio, image and speech processing performance.

Video Decode

To measure Video decode and display performance DDR2 memory was set to 256M in the boot parameters (Default value), and the following clips were used:

MPEG4

File: mpeg4_p176x144_332kbps_aac_99kx44k.3gp

Stream #0.0(und): Video: mpeg4, yuv420p, 176x144 [PAR 12:11 DAR 4:3], 332 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 30k tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s

File: mpeg4_p352x288_811kbps_aac_99kx44k.3gp

Stream #0.0(und): Video: mpeg4, yuv420p, 352x288 [PAR 12:11 DAR 4:3], 811 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 30k tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s

File: mpeg4_p640x360_1536kbps_aac_99kx44k.3gp

Stream #0.0(und): Video: mpeg4, yuv420p, 640x360 [PAR 3:4 DAR 4:3], 1536 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 30k tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s

File: mpeg4_p704x576_15mbps_aac_127kx44k.3gp

Stream #0.0(und): Video: mpeg4, yuv420p, 704x576 [PAR 12:11 DAR 4:3], 2032 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 30k tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s

File: mpeg4_p720x480_1960kbps_aac_99kx44k.3gp

Stream #0.0(und): Video: mpeg4, yuv420p, 720x480 [PAR 8:9 DAR 4:3], 1960 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 30k tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s
Resolution ICS 4.0.3 Devkit 3.0.0
MPEG4
AM3730 BeagleXM Flashboard
Min (fps) Max (fps) Avg (fps) Media CPU Load(%) Min (fps) Max (fps) Avg (fps) Media CPU Load(%) Min (fps) Max (fps) Avg (fps) Media CPU Load(%)
176x144 29.24 30.84 30.01 13 (max 15) 29.21 30.81 30.04 12.21 (max 14) 29.24 30.77 30.03 13 (max 15)
352x288 29.25 30.74 30.01 19.26 (max 21) 29.23 30.78 30.07 19.53 (max 21) 29.27 30.82 30.04 19.58 (max 21)
640x360 27.62 30.84 29.89 31.53 (max 34) 24.42 30.83 29.82 32.11 (max 36) 29.28 30.85 30.05 32.76 (max 38)
704x576 27.78 30.66 29.93 43.89 (max 48) 21.61 30.73 29.47 45.68 (max 55) 29.28 30.68 30.01 41.63 (max 53)
720x480 27.28 30.78 29.94 41.84 (max 46) 24.8 30.72 29.74 43.89 (max 48) 29.28 30.72 30.04 41.11 (max 47)


H264

File: h264_p352x288_2757kbps_aac_99kx44k.3gp

Stream #0.0(und): Video: h264 (Constrained Baseline), yuv420p, 352x288 [PAR 12:11 DAR 4:3], 2757 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 59.94 tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s

File: h264_p640x360_4mbps_aac_127kx44k.3gp

Stream #0.0(und): Video: h264 (Constrained Baseline), yuv420p, 640x360 [PAR 3:4 DAR 4:3], 3888 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 59.94 tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s

File: h264_p704x576_4mbps_aac_127kx44k.3gp

Stream #0.0(und): Video: h264 (Constrained Baseline), yuv420p, 704x576 [PAR 12:11 DAR 4:3], 3865 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 59.94 tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s

File: h264_p720x480_963kbps_aac_46kx44k.3gp

Stream #0.0(und): Video: h264 (Constrained Baseline), yuv420p, 720x480 [PAR 8:9 DAR 4:3], 601 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 59.94 tbc
Stream #0.1(und): Audio: aac, 48000 Hz, stereo, s16, 47 kb/s
Resolution ICS 4.0.3 Devkit 3.0.0
H264
AM3730 BeagleXM Flashboard
Min (fps) Max (fps) Avg (fps) Media CPU Load(%) Min (fps) Max (fps) Avg (fps) Media CPU Load(%) Min (fps) Max (fps) Avg (fps) Media CPU Load(%)
352x288 12.45 30.64 28.6 65.89 (max 71) 17.44 30.84 28.88 34.26 (max 39) 29.3 30.83 30.04 36.34 (max 40)
640x360 9.94 30.58 28.62 69.37 (max 80) 4.21 30.41 27.29 48.37 (max 74) 20.68 30.58 28.92 67 (max 82)
704x576 16.06 30.80 22.34 80.16 (max 93) 10.13 30.19 19.57 70.89 (max 96) 12.43 29.15 20.34 87.92 (max 94)
720x480 16.67 30.71 29.32 66.16 (max 73) 21.07 30.57 29.23 69.68 (max 77) 26.66 30.37 29.42 66.42 (max 72)


H263

File: h263_p352x288_847kbps_aac_99kx44k.3gp

Stream #0.0(und): Video: h263, yuv420p, 352x288 [PAR 12:11 DAR 4:3], 847 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 29.97 tbc
Stream #0.1(und): Audio: aac, 44100 Hz, stereo, s16, 99 kb/s
Resolution ICS 4.0.3 Devkit 3.0.0
H263
AM3730 BeagleXM Flashboard
Min (fps) Max (fps) Avg (fps) Media CPU Load(%) Min (fps) Max (fps) Avg (fps) Media CPU Load(%) Min (fps) Max (fps) Avg (fps) Media CPU Load(%)
352x288 29.25 30.67 30.04 18.42 (max 20) 29.38 30.64 30.05 18.68 (max 20) 25.34 30.82 29.86 18.68 (max 20)


Power Management

To measure power consumption a Keithley 2000 multimeter with a multiple-channel scan card was used. vdd1 (core) and vdd2 (pheripherals) power was measured under different scenarios.

SUSPEND

All these measurements were made without any USB connection to the board and SmartReflex disabled.

Power consumption when the boards goes into SUSPEND mode.

Suspend Power sleep_while_idle=0,enable_off_mode=0 ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 3.34
vdd2 (mw) 4.42
vdd1+vdd2 (mw) 7.76
Suspend Power sleep_while_idle=1,enable_off_mode=0 ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 3.35
vdd2 (mw) 4.42
vdd1+vdd2 (mw) 7.77
Suspend Power sleep_while_idle=0,enable_off_mode=1 ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 0
vdd2 (mw) 0
vdd1+vdd2 (mw) 0
Suspend Power sleep_while_idle=1,enable_off_mode=1 ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 0
vdd2 (mw) 0
vdd1+vdd2 (mw) 0


Video+Audio Decode and Playback

Power Consumption while decoding and playing the Big Buck Bunny clip

Video+Audio ondemand mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 54.17
vdd2 (mw) 148.65
vdd1+vdd2 (mw) 202.82
Video+Audio performance mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 301.52
vdd2 (mw) 149.83
vdd1+vdd2 (mw) 451.35
Video+Audio powersave mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 53.82
vdd2 (mw) 147.99
vdd1+vdd2 (mw) 201.81
Video+Audio userspace(1000000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 301.6
vdd2 (mw) 149.45
vdd1+vdd2 (mw) 451.05
Video+Audio userspace(800000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 228.53
vdd2 (mw) 149.2
vdd1+vdd2 (mw) 377.73
Video+Audio userspace(600000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 156.67
vdd2 (mw) 148.4
vdd1+vdd2 (mw) 305.06
Video+Audio userspace(300000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 53.88
vdd2 (mw) 148.13
vdd1+vdd2 (mw) 202.01

3D Graphics

Power consumption while running the 3D Graphics flying Teapot demo.

3D Graphics ondemand mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 54.23
vdd2 (mw) 148.6
vdd1+vdd2 (mw) 202.83
3D Graphics performance mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 301.6
vdd2 (mw) 149.69
vdd1+vdd2 (mw) 451.29
3D Graphics powersave mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 53.81
vdd2 (mw) 148.05
vdd1+vdd2 (mw) 201.86
3D Graphics userspace(1000000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 301.64
vdd2 (mw) 149.53
vdd1+vdd2 (mw) 451.18
3D Graphics userspace(800000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 228.43
vdd2 (mw) 149.33
vdd1+vdd2 (mw) 377.76
3D Graphics userspace(600000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 156.72
vdd2 (mw) 148.57
vdd1+vdd2 (mw) 305.29
3D Graphics userspace(300000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 53.88
vdd2 (mw) 147.95
vdd1+vdd2 (mw) 201.83

Idle with PARTIAL WakeLock

Power consumption with a CPU_PARTIAL WakeLock held and without running any activity (Home screen) in the foreground.

Idle ondemand mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 54.26
vdd2 (mw) 148.67
vdd1+vdd2 (mw) 202.93
Idle performance mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 301.6
vdd2 (mw) 149.74
vdd1+vdd2 (mw) 451.33
Idle powersave mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 53.79
vdd2 (mw) 148.16
vdd1+vdd2 (mw) 201.95
Idle userspace(1000000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 301.38
vdd2 (mw) 149.27
vdd1+vdd2 (mw) 450.65
Idle userspace(800000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 228.24
vdd2 (mw) 149.03
vdd1+vdd2 (mw) 377.27
Idle userspace(600000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 156.97
vdd2 (mw) 148.73
vdd1+vdd2 (mw) 305.71
Idle userspace(300000) mode ICS 4.0.3 Devkit 3.0.0
AM3730
vdd1 (mw) 53.86
vdd2 (mw) 148.04
vdd1+vdd2 (mw) 201.9

Quadrant Benchmark

Quuadrant is a benchmark developed by aurorasoftworks to asses performance in CPU, Memory, IO, 2D graphics and 3D graphics, for more information refer to http://www.aurorasoftworks.com/

In the results shown below the results for AM3730, BeagleXm, and Flashboard are displayed in the column labeled as "your device: xxxx"

AM3730

Am3730 ICS4.0.3 Devkit3.0.0 quad.png

BeagleXM

BeagleXM ICS4.0.3 Devkit3.0.0 quad.png

Flashboard

Flashboard ICS4.0.3 Devkit3.0.0 quad.png

Versioning


This is Release Ice Cream Sandwich 4.0.3 Devkit 3.0.0. The release is available from http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_ICS_4_0_3_DevKit_3_0_0/index_FDS.html