Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

TMDSEVM6657L EVM Hardware Setup

From Texas Instruments Wiki
Jump to: navigation, search

This page will walk you through setting up your TMDXEVM6657L Evaluation Module (EVM). These guidelines also apply to the L and LE EVM models.

NoteNote: Some of the steps in this section have been updated from those used in the EVM Quick Start Guide.

Hardware Setup Overview

The picture below shows the TMDXEVM6657L EVM and the locations of relevant switches and connectors.

TMDSEVM6657L-image.jpg

Hardware Setup Steps

Warning Warning: The EVM board is sensitive to electrostatic discharges (ESD). Use a grounding strap or other device to prevent damaging the board. Be sure to connect communication cables before applying power to any equipment.


1. Attach the Ethernet cable

Using the Ethernet cable supplied, connect one end of the cable to the Ethernet port on the EVM and the other end to your PC.


2. Connect the JTAG interface

Use the USB to USB mini-B cable provided. Connect the USB mini-B connector to the USB mini-B interface on the EVM and the USB connector to your PC. This enables XDS-100 emulation and is directly useable by CCS. If you are using a different JTAG, connect it now.


3. Verify Endian mode in the SW3 settings

The Endian mode should be set to Little Endian. SW3 also contains the boot device settings.


TMD6657LSW3.png


4. Verify boot mode in the SW3 and SW5 settings

The boot mode settings below enable NOR boot by loading the boot loader from EEPROM address 0x51.

TMD6657LSW3-6.png


5. Set User Switch for the demo application

The application needs an IP address. It can use either a static IP address (pre-configured) or it can request one using DHCP. This is controlled by setting dip switch 2 of SW9.

User Switch 2 ON : DHCP
User Switch 2 OFF: Static IP

TMD6678LSW9.png


6. Attach the serial port cable

This EVM can use either a USB serial port or the standard DB-9 (use the cable shipped with the platform). By default the shunts which control this on the platforms are set to use the USB by default. We recommend changing them to use the DB-9 as there are no known issues with this approach.

TMDXEVM6657L-shunts.jpg
COM_SEL1: Select UART over 3-Pin Header


NoteNote: If the USB serial port output does not work, ensure that the cable is connected directly to a USB port on the PC/laptop rather than going through an extender or USB hub.


7. Connect the power cable

Connect the power cable to the EVM power jack on the board. To be ESD safe, plug in the other end of the power cable only after you have connected the power cord to the board. Then turn on the board.


Boot Mode Dip Switch Settings

The EVM supports booting image from various devices (EEPROM, NAND or NOR) via IBL (at I2C address 0x51), I2C EEPROM (at I2C address 0x50), and ROM Boot modes (such as Ethernet, SRIO, PCIe, SPI etc.) which address the boot source directly from the ROM code. Below is the table showing the boot mode dip switch settings for different boot mode that the EVM supports:

Boot Mode

DIP SW3

(Pin1, 2, 3, 4, 5, 6, 7, 8)

DIP SW5

(Pin1, 2, 3, 4, 5, 6, 7, 8)

IBL NOR boot on image 0 (default) (off, off, on, off, on, on, on, on)1,2,3 (on, on, on, off, on, on, on, on)4
IBL NAND boot on image 0 (off, off, on, off, on, off, on, on) (on, on, on, off, on, on, on, on)
IBL NAND boot on image 1 (off, off, on, off, off, off, on, on) (on, on, on, off, on, on, on, on)
IBL TFTP boot (off, off, on, off, on, on, off, on) (on, on, on, off, on, on, on, on)
I2C POST boot (off, off, on, off, on, on, on, on) (on, on, on, on, on, on, on, on)
ROM SPI Boot8 (off, on, off, off, on, on, on, on) (on, on, off, on, on, on, on, on)
ROM SRIO Boot5 (off, off, on, on, on, on, off, on) (off, on, on, off, off, on, on, on)
ROM Ethernet Boot6 (off, on, off, on, on, on, on, off) (on, off, on, off, off, on, on, on)
ROM PCIE Boot7 (off, on, on, off, on, on, on, on) (on, on, on, off, off, on, on, on)
No boot (off, on, on, on, on, on, on, on) (on, on, on, on, on, on, on, on)

NoteNote: : C6657 currently does not support Image 1 for NOR boot.


Footnotes:

1. Pin 1 of SW3 is the endian pin, by default, it is set to off (Little Endian) 

2. Pin 2-4 of SW3 are the boot mode pins, by default it is set to I2C boot mode (off, on, off)

3. Pin 5-8 of SW3 and pin 1-2 of SW5 are the boot parameter index pins for I2C boot (paramter index 0/1 for NOR boot image 0/1, parameter index 2/3 for NAND boot image 0/1, parameter index 4 for TFTP boot). By default, image 0 is programmed to offset byte address 0x0 on NOR, and 0x20000 (block 1 start address) on NAND, image 1 is programmed to offset byte address 0x4000000 on NAND.

4. Pin 4 of SW5 is the I2C address pin (off: 0x51, on: 0x50)  for I2C boot mode

5. This will set the board to boot from SRIO boot mode, with reference clock at 250 MHz, data rate at 3.125 GBs, and lane setup 4-1x ports and DSP System PLL at 100 MHz.

6. This will set the board to boot from Ethernet boot mode, with SerDes clock multiplier x 4, core PLL clock at 100 MHz.

7. This will set the board to boot form PCIE boot mode, with PCIE in end point mode and DSP System PLL at 100 MHz.

8. This will set the board to boot from SPI NOR via the ROM code, with boot-table contents expected in the NOR. 24bit addressing has been set.

Please refer to Technical_Reference_Manual for the boot mode switch settings on the board.

E2e.jpg
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article TMDSEVM6657L EVM Hardware Setup here.

Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity