TMS470 Optimizing C/C++ Compiler Errata
From Texas Instruments Embedded Processors Wiki
Translate this page to
Options Errata
- --ppm
- The Compiler User's Guide is missing information on the
-ppmswitch, used to generate a list of predefined and user defined macros. The details are: - -ppm[=filename]
- Generate a list of predefined and user defined macros for the source file into the file <filename>.pp and then exit. Optionally, name the output file. The output will include only those files directly included by the source file. Also see the -ppa option to continue compilation after generating the macro list (similar to gcc).
- This option became available starting with version 6.1.0.
- --no_const_clink
- The Compiler User's Guide is missing information about the
--no_const_clinkswitch. This switch prevents the compiler from generating .clink directives (conditional linking) for const global arrays. By default, these arrays are placed in a .const subsection and conditionally linked.
- Section 5.4.2 the interrupt Keyword
- The Compiler User's Guide refers the reader to section 5.9.2 for more information on the INTERRUPT pragma. The correct section is 5.8.5
- Section 5.4 Keywords
- The TMS470 C/C++ compiler does not support the near and far keywords.