Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

TMS570LS12x HDK Kit

From Texas Instruments Wiki
Jump to: navigation, search

The TMS570LS12x Hercules Development Kit (HDK) is ideal for evaluating and starting development with the Hercules platform of safety microcontrollers. The kit is comprised of a development board, a DC power supply, a mini-B USB cable, and Ethernet cable and a software installation DVD. The development board features an on board XDS100v2 JTAG emulator along with access to several key communication and peripheral interfaces. The HDK features:

  • 337p BGA TMS570LS1227 MCU, on board
  • On Board USB XDS100v2 JTAG
  • On Board SCI to USB Serial
  • 20pin ARM and MIPI JTAG connectors
  • 8 White NHET LEDs
  • 8MB SDRAM (EMIF)
  • Ambient light and temp sensor
  • 2 CAN transceivers
  • 1 RJ-45 ethernet port
  • 1 Micro SD card slot (SPI mode)

More information specific to the TMS570LS12x Hercules MCU family can be found on the TMS570 wiki page.


Kit Contents

Included in the kit are the following items:

  • The TMS570LS12x Hercules development board
  • A DVD-ROM that includes:
  • HDK quick start, and user guide
  • CodeComposer Studio v5.2 IDE
  • Flash Programming Utility
  • HALCoGen Peripheral Drivers Generation Tool
  • HET Simulator/Debugger w/ Synapticad WaveViewer
  • Example programs for the TMS570 Development Kit


Not included:

  • 12V power supply

Below are two options that electrically and mechanically will work with the HDK:

  • 12V output, 2A max output current
  • Positive center
  • Barrel plug (2.1mmx5.5mm)
  • Output Protection: Short Circuit, Over Voltage, Over Current
  • Safety approvals: CB, CE, UL, FCC, PSE, LPS, BSMI, RCM, and CCC
  • 12V output, 2A max output current
  • Positive center
  • Barrel plug (2.1mmx5.5mm)
  • Output Protection: Short Circuit, Over Voltage, Over Current
  • Safety approvals: UL/cUL, CCC, RCM, PSE


How to Order Kit

To order the TMS570LS12x Hercules Development Kit, visit the TI e-Store.

To learn more about other TMS570LS12x HDK, visit the TMS570 Tools & Software webpage.


HDK Board Schematic

The PDF format schematic drawings for the TMS570LS12x HDK is available here: TMS570LS12_HDK_Schematics.pdf

The Cadence Capture Format format schematic drawings for the TMS570LS31x HDK is available here: TMS570LS12_HDK_Schematics.zip

The gerber files for the TMS570LS12x HDK are available here: TMS570LS12_HDK_Gerbers.zip

The BOM for the TMS570LS12x HDK are available here: TMS570LS12_HDK_BOM.zip

Orcad Symbol

337pin ZWT BGA package symbol: TMS570LS12x_ZWT_OrcadSymbol.zip


HDK Quick Start

A digital version of the Quick Start Guide included in the kit is available here: TMS570LS12x_HDK_Quick_Start_RevE.pdf

HDK User Guide

A digital version of the User Guide included in the kit is available here: TMS570LS12x_HDK_USerGuide.pdf


Example Programs

HDK LED blinky example programs for CCS5.2 IDE can be found here: TMS570LS12x_HDK_Blinky_Sample_Code.zip (This link doesn't work!!!)


Example Expansion Board Design

HDK Experimenter


Support


Important Links

  • Visit the TMS570 Homepage www.ti.com/tms570 for the latest information on upcoming products and TMS570 announcements.