Talk:CC2541 SensorTag

From Texas Instruments Wiki
Jump to: navigation, search
For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article CC2541 SensorTag here.

Comments on Bluetooth SensorTag


Schneiderham said ...

Looks great! Where can we get the CC2541 and iOS source code?

--Schneiderham 12:31, 15 November 2012 (CST)

Jboe said ...

The iOS source code is added to this site under the SensorTag App chapter. The CC2541 source code will be included in the TI BLE stack v1.3 and newer

--Jboe 02:14, 23 November 2012 (CST)

Schneiderham said ...

Thank-You Jboe. May I ask when v1.3 is expected to be released?


--Schneiderham 10:10, 29 November 2012 (CST)

Cbandarrinha said ...

Hi Jboe ... Could you tell us when is V1.3 expected to be released? We desperately need the source code for the CC2541 sensortag.

--Cbandarrinha 20:10, 6 December 2012 (CST)

Jboe said ...

The Bluetooth low energy stack including the SensorTag source code is now released and can be downloaded on the BLE stack page, http://www.ti.com/tool/ble-stack


--Jboe 07:45, 14 December 2012 (CST)

Jareilly said ...

Does the iPad Mini work as a client for the SensorTag. It is listed as "not tested", perhaps someone has tested whether or not it works by now?

--Jareilly 07:17, 2 January 2013 (CST)

Jboe said ...

iPad mini is tested and working well, the text is now updated. Thanks for pointing out

--Jboe 14:36, 3 January 2013 (CST)

Echomrg said ...

Hi, i wanted to ask if there's some kind of official support or forum/community support for the product. I bought one and I'm having huge problems with it (it either freezes and completely stop responding or still show up on the ios app but with no sensors enabled).

--Echomrg 08:51, 29 January 2013 (CST)

Jboe said ...

You can find the forum here: http://e2e.ti.com/support/low_power_rf/f/538.aspx


--Jboe 15:47, 29 January 2013 (CST)

GammaPoint said ...

The SensorTag app generates the source code when connected to the SensorTag device.

The source code is under:

Connected Devices->Profiles->Generate Source Code

--GammaPoint 19:04, 12 February 2013 (CST)

McBrave said ...

Seems like the "Source code for MAC OS X application example" download does not contain any source code at all... Is it available elsewhere?

--McBrave 14:49, 7 March 2013 (CST)

Klaus said ...

Developed a weight training application using the sensor tag, find application here http://tinyurl.com/nlhyoes. The application detects how many repetitions the user does and distinguishes between pushes and pulls (e.g. pulls often train the back and pushes are more for chest and legs). Going forward I will also support curls. Have a look at my project site https://sites.google.com/site/weighttraininggenie/


--Klaus 20:32, 30 May 2013 (CDT)

Jboe said ...

Thanks for sharing your app, I have added it to the app support list on this site

--Jboe 07:30, 7 June 2013 (CDT)

JoeK said ...

How many SmartTags can we pair with one iPhone?

--JoeK 16:02, 18 June 2013 (CDT)

JoeK said ...

Actually, I am trying to create a method where I have a set of tags and a set of iphones. I would like that the iPhone reads all sensor info when it detect a tag in its presence. The tag can move from on iPhone location to another. And, the tag can be in multiple iPhone range. Can such a config be supported for this tag? Will the tag talk to multiple iPhones and an iPhone talk to multiple tags without having to click on the "pair" button?

--JoeK 09:06, 21 June 2013 (CDT)

There are no threads on this page yet.