Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Talk:Eclipse Concepts

From Texas Instruments Wiki
Jump to: navigation, search
For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Eclipse Concepts here.

Comments on Eclipse Concepts


A074107 said ...

I think the last paragrapgh: "This differs from the concept of adding a file to a CCSv3 project" It should read instead: "This differs from the concept of linking a file to a CCSv3 project"

Where "linking" sounds more appropriate...

--A074107 04:05, 17 August 2009 (CDT)

A0322160 said ...

You should add some text stating that you can create subdirectories in the project directory with include files, etc. This may be obvious but the following statement makes it seem like you can't have your include files in your project directory, "The 'Binaries' and 'Includes' folders that appear in the view also are just references." For example, you could create a subdirectory called 'Includes' in your project directory and place header files their and then you will have two 'Includes' in the project view.

--A0322160 14:29, 22 October 2009 (CDT)

Will.friesen said ...

In the second paragraph after "Perspective" is this sentence: Perspectives can easily switched between perspectives by clicking on the perspective icons in the upper right corners. To "be" or not to "be" and an extra s.

I might have said: Users can easily switch between perspectives by clicking on the perspective icons in the upper right corner.


--Will.friesen 21:42, 21 June 2011 (CDT)

There are no threads on this page yet.