Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Talk:TMDXEVM6678L EVM Hardware Setup

From Texas Instruments Wiki
Jump to: navigation, search
For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article TMDXEVM6678L EVM Hardware Setup here.

Comments on TMDXEVM6678L EVM Hardware Setup


Bharath374 said ...

Is this statement in step #6 incorrect? "Both shunts should be moved to the top 2 pins for the RS232 Cable. If the shunts are moved to the bottom 2 pins , then the USB port is enabled." Shunts should be in the top two pins for USB, correct?

--BRY 02:24, 16 August 2011 (CDT)

Crescent said ...

Bharath374 From the picture showed below "6. Attach the serial port cable" in this page, the statement about the shunts' position is wrong. I suppose saying that is referencing the PCB's view.

--Crescent 04:21, 16 August 2011 (CDT)

Lwmcgl said ...

How are the shunts to be positioned for RS232 Cable instead of USB serial port?

--Lwmcgl 10:27, 18 January 2012 (CST)

Andrewp said ...

For UART over USB: Short COM_SEL1.1 to COM_SEL1.3 and short COM_SEL1.2 to COM_SEL1.4.

For UART over RS-232: Short COM_SEL1.3 to COM_SEL1.5 and short COM_SEL1.4 to COM_SEL1.6.

Pin 1 is on the edge of the PCB. Pin numbers are assigned in zig-zag fashion, unlike IC's where they are typically counted along an edge.

ASCII art diagram:

======== (PCB EDGE)

[1] [2]

[3] [4]

[5] [6]

Lwmcgl said ...

thanks andrewp for the quick response

--Lwmcgl 13:27, 18 January 2012 (CST)

There are no threads on this page yet.