Tips for using printf

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

The printf family of functions are standard C functions used to output text. Basic information about the printf family is widely available online and in introductory C textbooks. However, users of the TI toolchain need to be aware of certain implementation-specific details.

Contents

What is C I/O?

C I/O is a broad term referring to the input and output functions in the RTS; and also to the ABI between the low-level RTS functions and the debugger, which allows the debugger to service the user's I/O requests.

All C I/O is funneled through very low-level functions which eventually reach one of two required two breakpoints, at label C$$IO$$ or C$$EXIT. The debugger watches for one of these breakpoints to be reached, at which point the debugger performs an I/O request for the program.

The C standard specifies many input and output functions, and related support functions. This is a partial list.

C standard I/O functions:

  • fopen, fclose, fread, fwrite, fflush, freopen
  • fseek, fgetpos, fsetpos, ftell, rewind
  • perror
  • remove, rename
  • tmpfile, tmpnam

Other C standard using the C I/O ABI:

  • getenv
  • gmtime, localtime, time, ctime, clock
  • exit, abort

C standard I/O-related utility functions:

  • setbuf, setvbuf, clearerr, feof, ferror

The following low-level Unix-style I/O functions are not part of the C standard, but are considered part of the C I/O functions in the RTS:

  • open, close, read, write, lseek

Getting C I/O working / Troubleshooting

C I/O is one of the more complicated things in the RTS. It has several layers of abstraction, invokes dynamic memory allocation, has lots of helper functions, and requires intervention from a host debugger to even work at all. For details about the implementation of C I/O, see the Optimizing C Compiler User's Guide section on the C I/O functions.

The typical symptom of not getting everything right is that printf silently fails, and no output is visible in CCS - specifically the "Stdout" window in CCS will not open.

Hello, world!

Start with a simple "hello, world" test to make sure you have configured your system correctly.

#include <stdio.h>
int main() { puts("Hello, world!"); }

Include stdio.h

Every module which uses a C I/O function should include stdio.h. Failure to do so can make C I/O functions, particularly printf, fail with no warnings generated by the compiler, linker, or debugger. The printf function is a variadic function, and calling such a function without a valid prototype in scope invokes undefined behavior. Use the option "-pdsw225" to see warnings for all functions used without a valid prototype.

Stack Size

Make sure the stack is large enough. Depending on the version of the compiler, calling one of the *printf functions requires more than 400 bytes of stack. Make sure the stack is in valid read/write data memory.

Heap Size

Most of the standard C I/O functions operate on streams. A stream is stdout, stdin, stderr, or any file opened with fopen. Each stream needs its own I/O buffer, and if you do not provide one, one will be automatically dynamically allocated for you when you perform the first read or write. This buffer is of size BUFSIZ (defined in stdio.h) and is by default 256 bytes for all targets.

For projects not using DSP/BIOS: Under Project -> Properties -> C/C++ Build -> Linker -> Basic Options -> Heap Size(-heap) enter the heap size, e.g. 0x400

If using DSP/BIOS:

  1. Open your tcf file in the configuration tool.
  2. Right click on Memory Section Manager and go to Properties.
  3. Uncheck the "No Dynamic Heaps" box if it is not already unchecked. Click OK to exit the dialog.
  4. Right-click on the memory section where you would like to create a heap, e.g. DDR2 and go to Properties.
  5. Click the "Create a heap in this memory" box and enter the size. Click OK to exit the dialog.
  6. Right-click once again on Memory Section Manager and set the "segment for malloc/free" to a valid section, e.g. DDR2.

The heap is located in the .sysmem data section. Make sure that the linker command file properly allocates the .sysmem (and .esysmem for C2000) sections to valid read/write data memory.

C I/O communication buffer placement

The .cio data section contains the buffer _CIOBUF_, used by the C I/O functions and the debugger to communicate with each other. You must allocate the .cio section to valid read/write data memory.

Note: This section is rather small, which means that large reads and writes may require many hits of the C$$IO$$ breakpoint to be performed. This buffer can be increased, but the limiting factor is the debugger needs to be able to resize its own internal buffer.

Special Breakpoints

For C I/O to work, the debugger must be able to set breakpoints at the two special labels C$$IO$$ (in function writemsg) and C$$EXIT (in function abort). It's not necessary that these breakpoints be in RAM, but it is necessary that the debugger be able to set these breakpoints. If the bulk of the RTS .text is placed where breakpoints cannot be set, you must separate the input section containing writemsg (trgmsg.obj on most targets, ankmsg.obj on C2000, ldmsg.obj on C5400) and abort (exit.obj) and place them into valid read/write program memory.

SECTIONS 
{
    .text:cio : { rts*.lib<trgmsg.obj exit.obj>(.text) } > RAM
    .text:rts : { rts*.lib(.text) } > ROM
    .text > PMEM
    ...
}

Make sure you allow setting of CIO breakpoints at load:

In CCS 3.3, under Option -> Customize -> Program/Project Load -> Program make sure the Do Not Set CIO Breakpoint At Load is not checked. If this is checked, you will not see any CIO activity.

In CCS v4, under Project Debug Properties -> Target tab make sure the Enable CIO function use is enabled.

Note: The downside of allowing the setting of CIO break-points is that when debugging from Flash, it will use one hardware break-point. You may need to move C I/O code to RAM to avoid this issue.

Flushing

If you set a breakpoint in a program after a C I/O function, you may not see the output taking effect if the stream is buffered. If you need to see the output, you need to make sure the buffer is flushed. You can do this for an _IOLBF stream by making sure to end each printf format string with a '\n' (new line). Since the stdout stream is line buffered this will cause the buffer to be flushed. See the Buffering modes section for further details.

Alternatively, you can flush the buffer manually:

fflush(stdout); // This will flush any pending printf output
fflush(FilePointer); // This will flush any pending fprintf output

A stream's buffer is automatically flushed when it is closed, and all streams are automatically closed during exit(). If you call abort() (or otherwise prevent the program from reaching exit()) some buffers may not be flushed.

Built-in limits on number of files

The RTS has a pretty low limit on the number of files you can have open simultaneously. Always check the return value of fopen(), tmpfile(), and open() to make the file was opened successfully. If an attempt to open a file fails, check the number of open files. There are two limits on the number of open files.

The first limit is FOPEN_MAX, which applies to streams opened with fopen(). Streams are represented by a FILE pointer. The three standard streams stdout, stdin, and stderr count against this total, so if FOPEN_MAX is 10, you may only open 7 more streams without closing one of them. If too many streams are already open, fopen() will return NULL.

The second limit is _NSTREAM, which applies to the low-level C I/O function open(). The open() function returns an integer representing a file descriptor. If too many file descriptors are already open, open() will return -1.

Note that fopen() calls open() to create a file descriptor for the stream, so each call to fopen() counts against the limit for open(), as well. Also note that even if the number of files opened with fopen() is less than FOPEN_MAX, you may not be able to open a new FILE if there are too many open file descriptors opened with open().

Finally, note that these limits can be changed by modifying and rebuilding the rts libraries. This forum post provides some details on that process.

Binary files

If the file you are opening is a binary file, be sure to open the file with a binary mode such as "rb". If you do not, and the file contains data with a '0' byte, the RTS will mistake that for the end of the file. For more see the last paragraph of this discussion on binary data handling.

Avoid C I/O inside interrupt handler functions

Generally, using any kind of C I/O function from within an interrupt handler is unsafe, because the interrupt may occur during a different call to a function performing C I/O. That is, the C I/O functions are not reentrant.

DOS vs. Unix format

Reading a "foreign" format poses problems. See...

Reading 8-bit binary data on 16-bit targets

Poses problems. See Reading and Writing Binary Files on Targets With More Than 8-Bit Chars

Performance Considerations

There are many performance considerations when using the C I/O in an embedded system.

Buffered I/O

The C I/O functions are buffered for two reasons:

Buffering modes

The C standard provides 3 buffering modes with different performance characteristics:

Use setvbuf() to change the buffering mode for any stream. For example:

setvbuf(stdout, NULL, _IONBF, 0); // turn off buffering for stdout

For further information about setvbuf, see here.

Dynamic memory allocation in C I/O

Each stream needs its own buffer, and if you do not provide one, one will be automatically dynamically allocated (i.e. malloc) for you when you perform the first read or write. This buffer is of size BUFSIZ (defined in stdio.h) and is by default 256 bytes for all targets. To avoid dynamic allocation by C I/O functions, you must provide a static buffer for each stream you will read or write to. For example:

char static_array[20];
setvbuf(stdout, static_array, _IOLBF, sizeof(static_array));

Note: even if you set a buffer to _IONBF, you still have to provide a two-byte static array, or the RTS will allocate a buffer of size BUFSIZ to handle ungetc().

Low-level I/O functions

The low-level I/O functions read() and write() do not use an I/O buffer. If the request exceeds the size of the _CIOBUF_ buffer, only the first BUFSIZ bytes will be read or written, and the return value will indicate how many bytes were read or written. Thus, if you need to write a large buffer with write(), you need to be prepared to place it in a loop.

Stop-mode C I/O

The current C I/O ABI works by setting a breakpoint at C$$IO$$. When this breakpoint is hit, the CPU is halted. The debugger then reads the contents of the .cio buffer through JTAG, performs the requested C I/O operation, writes the results back to .cio, and restarts the CPU. This is a very expensive operation in terms of cycles, and can be very disruptive in real-time systems.

String formatting

The printf command has a major impact on real-time systems:

Other General Tips

Reducing printf code size with --printf_support

Reduce code size of printf by dropping features...

Using freopen()

If you have a bunch of calls to printf(), but you want the output to go to a file instead of to the standard output, you can reopen stdout with freopen. This will cause all printf() output to go to the new file without having to change all of the printf() calls to fprintf().

if (freopen("output.txt", "w", stdout) == NULL)
    fputs("failed to reopen stdout\n", stderr);

Using printf() to output to a user-defined device

You can install a user-defined driver so that you can use the sophisticated buffering of the high–level C I/O functions on an arbitrary device, such as a UART.

The user-defined driver will not use the C I/O ABI to communicate with the debugger; the driver will need to provide some other means of output, such as controlling a peripheral.

  1. Get/write a device driver for outputting data from the UART (or whatever interface you choose).
  2. Write the low-level functions as described in Chapter 8.2 The C I/O Functions of the C Compiler User's Guide.
  3. Call add_device() to add your functions to the stream table (i.e. in addition to stdin, stdout, stderr).
  4. Open your stream.
  5. Redirect your stream to stdout using freopen.
  6. Specify what buffering is to be used for your stream by calling setvbuf.

For example:

ret_val = add_device("uart", _SSA, uart_open, uart_close, uart_read, uart_write, uart_lseek, uart_unlink, uart_rename);
fid = fopen("uart","w");
freopen("uart:", "w", stdout); // redirect stdout to uart
setvbuf(stdout, NULL, _IONBF, 0); // turn off buffering for stdout
printf("Hello world!\r\n");

See also RAMDISK: A Sample User-Defined C I/O Driver

Additional Tips for DSP/BIOS Users

DSP/BIOS users should also read more about calling RTS functions from BIOS.

DSP/BIOS users have an alternative called LOG_printf(). See this FAQ for information on switching from printf() to LOG_printf().

Leave a Comment

Comments

Comments on Tips for using printf


Praetor said ...

Please add a section with instructions on how to do setup the heap in BIOS6 which does not use tcf files

--Praetor 11:55, 24 November 2009 (CST)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox