UniFlash v4 Quick Guide

From Texas Instruments Wiki
Jump to: navigation, search

Applicability

This guide applies to UniFlash v4. For other UniFlash releases, please see here.


Quick Start Guide

You can chose to use the standalone desktop version, or the cloud version. The desktop version is available from http://www.ti.com/tool/uniflash. The cloud version is available from the cloud tools portal (http://dev.ti.com).

The first time you access a device from the Cloud using either UniFlash or the Cloud IDE, you will be prompted to install TI Cloud Agent. For more details you can refer to TI Cloud Agent.

A guide specific to IWR14xx/IWR16xx devices can be found here. (This is a PDF document.)

Session

To perform flash operations on your device, you will need to launch a flash session configured for that device. You can start a new session by:

  • Selecting a Launchpad or device/connection combination. When you select a Launchpad, the connection is automatically choosen for you.
  • Loading a previously saved session. Loading a session will restore your previous selection (Device, connection, and settings).
  • Selecting a CCXML file created by CCS. This is useful if you have configuration settings in the CCXML file beyond a simple device and connection selection.

Start a new session from this page:

Welcome.png


Program the device

Choose a program to flash by clicking the Browse button, and you can either load the program or use it to verify against the content on the device.

Click on the “Binary” checkbox if you want to load the file as binary, a start address is needed for this.

Click on the “+” icon to add and load multiple flash images. Only the checked images will be flashed. The user need to be sure that the images does not overwrite each other in the target memory.

Program.png


Erase the device and other settings and utilities

In the Settings and Utilities view, you can find various settings to configure your operation. To quickly navigate this page, use the search filter to find the relevant items.

A commonly used Erase Flash utility is also found here under the Erase Section. You can pin this Erase button to the quick settings in the Program view discussed earlier in section 2.

To do that, click on the Pin Options button right at the end of search filter line. A column of “+” buttons will appear to allow you to customize on what to be added to the quick settings. Once you are done, you can use this in the Program view.

Settings.png


Memory browser and memory export

The Memory View allows you to quickly browse through the target memory. The view is read only.

Click on the “Export” button to export a range of memory into either a binary (.BIN) file or a COFF (.out) file. COFF format allows multiple memory sections to be exported.

Memory browser.png

CLI Device Detector

In offline install of UniFlash, there is a command line utility in the root installation folder called "detect-devices.bat" or "detect-devices.sh" to help you detect the list of plugged in devices and their COM port. Example output:

 C:\ti\uniflash_4.2.2.1689>detect-devices.bat
 0) Unknown TIMSP430-USB
 1) CC2650 LaunchPad rev 1.0 TIXDS110_Connection L1000610 COM36


Standalone Command line tool

Often in production line environment all you really want is a CLI tool that does one job: Flash the device with verification. This new UniFlash v4 feature is tailor made for this use case.

After you have chosen the image you would like to flash and configured the flash settings accordingly, go to the “Standalone Command line” view to choose the deployment platform for the CLI tool. Hit “Generate Package” and a zip file will be created; containing everything you need for the deployment platform to flash your target.

You might need to run the driver installation script if the deployment machine does not have the drivers installed. Otherwise, just run “dslite” from the zip package to flash the target with the file you were working on in the GUI tool with the same flash settings.

While the cloud version of UniFlash can generate CLI package for all deployment platforms, the offline version of the tool can only generate package of the current platform. Standalone cli.png

Updating USB Entry in Generated MSP430 Package

To switch between USB1, USB2,or USB3 connection in a generated MSP430 package, you can open up the connection XML file in your generated package (\ccs_base\common\targetdb\connections\TIMSP430-USB*.xml).

Look for the line <property Type="hiddenfield" Value="101" id="portAddr1"/>, and change the value field manually (101 for USB1, 102 for USB2, 103 for USB3).

Command Line Interface

UniFlash Desktop comes with a Command Line Interface (CLI) in the package. To access CLI, go to the install directory and look for the DSLite startup script (dslite.bat for Windows and dslite.sh for Linux/OSX).

DSLite comes with a few different modes, with the default mode being 'flash', use for flash programming on your device. Other modes might be added in the future to expand the functionality. To see the list of available modes, use the --listMode option.

Available Modes for UniFlash CLI:

 * flash [default] - on-chip flash programming
 * memory          - export memory to a file
 * load            - simple loader [use default options]
 * mspflasher      - support MSPFlasher command line parameters [deprecated]

Flash mode

The Flash mode (default) can be used for Flash Programming.

Usage:

 dslite flash --config=ccxml-file [options] [flash-file1 ...]


Options:

 -c [ --config ] arg                Target Configuration (ccxml) file, must be
                                    supplied other than running --help. CCXML
                                    file can be generated and exported using
                                    the Uniflash GUI or Code Composer Studio.
 -n [ --core ] arg (=0)             Zero based index of core to operate on.
 -S [ --list-settings ] arg         Takes a regex and list the final values
                                    applied to the matching settings. (ie; use
                                    .* to list all available settings)
 -p [ --list-ops ]                  List the available flash operations.
 -I [ --list-device-cmds ]          List the available device commands, if
                                    any.
 -l [ --load-settings ] arg         Apply settings file generated by UniFlash
                                    GUI.
 -s [ --setting ] arg               Override a specific setting by using
                                    id=value.  Can be specified multiple
                                    times.
 -b [ --before ] arg                Operation(s) to perform before loading.
                                    Can be specified multiple times, and are
                                    performed in the order they appear on the
                                    command line. Get a list of operations by
                                    using --list-ops.
 -f [ --flash ]                     Load the file(s) specified at the end of
                                    the command line to flash.  This is
                                    assumed to be set unless verify is set.
 -v [ --verify ]                    Verify the file(s) specified at the end of
                                    the command line.
 -a [ --after ] arg                 Optional operation to perform after
                                    loading.  Can be specified multiple times,
                                    and are performed in the order they appear
                                    on the command line. Get a list of
                                    operations by using --list-ops.
 -O [ --post-flash-device-cmd ] arg Execute the given device command. Get a
                                    list of device commands by using
                                    --list-device-cmds.
 -t [ --timeout ] arg               Timeout in seconds, infinite if
                                    unspecified.
 -g [ --log ] arg                   Enable detailed logging to the specified
                                    file.
 -e [ --verbose ]                   Outputs progress messages to the console.
 -h [ --help ]                      Print this message.

Tutorial and Examples

The easiest way to create a CLI package that by default flashes a particular file, given a particular set of setting, is to use the "Generate CLI Package" feature (see Standalone Command line tool).

Once you unzip the package, you can find the target configuration file in the user_files/configs folder. The image you have selected in the program tab of the GUI is in the user_files/images folder, and all the device/flash settings you have applied in the GUI are saved in user_files/settings/generated.ufsettings.

By default, running dslite without any argument will automatically use the generated.ufsettings file to configure the device and apply the device/flash settings, and flash the target with the image file you have selected in the GUI.

What dslite does behind the scene is calling dslite.exe with the following command, for example:

 dslite.exe -c user_files/configs/cc2650f128.ccxml -l user_files/settings/generated.ufsettings -e -f -v user_files/images/cc2650_modem_onepass.out 

Where

  • -c is specifying the config file,
  • -l is specifying the user settings file,
  • -e is for verbose mode,
  • -f is specifying that we want to flash,
  • -v is specifying that we want to verify after flashing.

At the end of the options, we specify the image files to be flashed.

When running dslite.bat with arguments, it basically calls dslite.exe and forward your argument to the executable instead of using the generated ones shown above. Since all actions need -c to be specified (except when bringing up help with -h), if you are only working on one device, you can skip that part by writing you own batch/shell script to launch dslite.bat with a fixed .ccxml file.

Sometimes certain devices have device-specific commands. To view them, use:

 dslite.bat -c <your ccxml file> --list-device-cmds

This will show a list of available commands, which may look different from device to device. For example, with CC13xx and CC26xx, it may look like the following:

 ------ Device Commands --------------------------
   PinReset: CC13xx and CC26xx specific reset.
 -------------------------------------------------

Dslite may return an error if no device-specific commands exist:

 Failed: 'GEL_CLI_ListCommands()' not found

To call a device-specific command, use:

 dslite.bat -c <your ccxml file> --post-flash-device-cmd <CMD_NAME>

In the C13xx and CC26XX case,

 dslite.bat -c <your ccxml file> --post-flash-device-cmd PinReset

Memory mode

The Memory mode allows you to export device memory to a file

Usage:

 dslite --mode memory [options] --config=ccxml-file --range=address,length --output=output-file

Options:

 -c [ --config ] arg    Configuration (ccxml) file.
 -f [ --coff ]          Output in coff format.  Default format is binary.
 -r [ --range ] arg     Memory location and length to read in the form
                        'address,length' or 'address@page,length'.  This can
                        be specified multiple times if using the coff format.
 -s [ --size ] arg (=8) Bit size of each memory value to read (for endianness
                        considerations, binary format only).
 -o [ --output ] arg    File to write the extracted memory to.
 -t [ --timeout ] arg   Timeout in seconds, infinite if unspecified.
 -g [ --log ] arg       Enable detailed logging to the specified file.
 -e [ --verbose ]       Outputs progress messages to the console.
 -r [ --core ] arg (=0) Zero based index of core to operate on.
 -h [ --help ]          Print this message.

Load mode

The Load mode can be used for a simple load operation (with default options)

Usage:

 dslite --mode load --config=file.ccxml [options] coff-or-binary-file1

Options:

 -c [ --config ] arg    Configuration (ccxml) file.
 -f [ --file ] arg      Elf, coff or binary file(s) to flash or verify.  To
                        specify a binary file, append ',address' after the
                        file.  This option exists only for compatibility - the
                        file to load can instead just be passed as the last
                        token on the command line.
 -t [ --timeout ] arg   Timeout in seconds, infinite if unspecified.
 -g [ --log ] arg       Enable detailed logging to the specified file.
 -r [ --core ] arg (=0) Zero based index of core to operate on.
 -h [ --help ]          Print this message.

MSPFlasher mode

The MSPFlasher mode supports all of the same options and features of the existing mspflasher standalone flashing tool. This mode is deprecated as the Flash mode can be used to program MSP430 devices as well.

Scripting

The command line interface can be called from the scripting language of your choice.

For complex scripting tasks, Debug Server Scripting (DSS) is supported in UniFlash v4. To use DSS, go to your <installDir>\deskdb\content\TICloudAgent\{os}\ccs_base\scripting\bin\ folder in your install directory, and start dss using the dss.bat/dss.sh script.

Note: A Java Runtime Environment (JRE) is needed to run DSS (32-bit JRE on Windows, 64-bit JRE on Linux and Mac). This was included as part of UniFlash v3, but is not included in the v4 installer. More information is available at this link: UniFlashv4_DSS

Defect Reporting and Logging

If you think you have encountered a bug, please report it in the e2eforum here: https://e2e.ti.com/support/development_tools/code_composer_studio/

Please send in the logs with your post as well as they will make things much clearer.

To turn on the logs:

1. go to the welcome/new session page(where you setup the device and connection type) and click on refresh to reload the uniflash app

2. launch your session

2. go to "Settings" on the top right nav bar and click on "Enable" under the "Debug Server Logging". This may take a while and display a path to the DS log. Now close the popup.

3. operate the GUI to reproduce the bug

4. go back to "Settings", click on "Download Log" under "GUI Logging" to obtain the GUI debug log, then go obtain the log file shown as the path under "Debug Server Logging", send both files by attach to your post. Uniflashv4 logging.png