Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Updating CCSv4

From Texas Instruments Wiki
Jump to: navigation, search

Overview

Code Composer Studio v4 uses the Eclipse update manager to check for updates. This allows you to check for updates to Code Composer Studio, third party emulation drivers as well as updates to other Eclipse plug-in packages that you have installed.

CCS will automatically check for updates once a week. This default setting for the check can be changed via the Preferences dialog by going to Windows->Preferences->Install/Update->Automatic Updates. You can also manually check for updates through the Help menu (Help->Software Updates->Find and Install).

CCS knows what updates to check for based on update sites that have been installed with the product.

Versions prior to CCS 4.1.2 only show the Code Composer Studio Updates, Spectrum Digital Emulation Updates and Blackhawk Emulation Updates(if those packages were selected during installation).

Only Minor Updates are Shown

When manually checking for updates through the Help menu (Help->Software Updates->Find and Install), only minor version updates are shown (for example, from compiler 7.0.3 to 7.0.4). To see major version updates, select Search for new features to install instead of Search for updates of the currently installed features.

Compiler Updates

  • For CCS version 4.1.2 and earlier, updates for the compiler are not shown. Download updates separately from the Compiler Download page.
  • Starting with version 4.1.2, CCS checks for compiler updates automatically.
  • For CCS versions before 4.2.4, the code size limited tools (C2000) are missing the update site. Follow this procedure to to have CCS search for new features and find the compiler updates.

BIOS and Target Content Updates

  • For CCS version 4.1.2 and earlier, updates for BIOS are not shown. Download updates separately from the BIOS download page.
  • Starting with CCS version 4.2.0, CCS checks for Target Content updates automatically.

Proxy Configuration

If your computer resides behind a firewall you may have to setup the proxy information so that CCS can get to our Eclipse update site. CCS attempts to get this information from your internet browser but sometimes you have set it up manually. To setup the proxy settings go to Windows->Preferences and the type "proxy" in the search box at the top left of the preferences dialog. This filters the preferences dialog to only things that have to do with "proxy". Select "Update/Install" in the tree. Then fill in your proxy settings in the screen that appears on the right.

Installing Patch Downloads

If you download the patch from CCS download page to update your CCS version, then follow this process to install the patch:

  • Go to CCS menu Help->Software Updates->Find and Install
  • Select "Search for new features to install", click Next
  • Select New Local Site and point to the directory where you unzipped the patch
  • The patch version should now appear in the list which you can then select and install