Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

WL18xx TX Testing

From Texas Instruments Wiki
Jump to: navigation, search

Introduction

This section will review the calibrator commands that may be useful when performing transmission (TX) testing on the WL18xx.

Prerequisites:

1. Your kernel and modules must be compiled with CONFIG_NL80211_TESTMODE=y. You can check this at run-time as follows:

root@am335x-evm:/usr/share/wl18xx#  zcat /proc/config.gz | grep NL80211_TESTMODE
CONFIG_NL80211_TESTMODE=y

NoteNote: If you don't have that configured, be sure to copy over your kernel and reinstall all modules.

2. The wlan0 interface must be shut down. Run ifconfig wlan0 down to disable it and then run ifconfig one more time to verify it has properly shut down.

3. Before using any of the WLAN commands listed below, you should enter the WL18xx device into PLT mode using the following command:

cd /usr/share/wl18xx/
calibrator wlan0 plt power_mode on


Tune Channel

Purpose

The purpose of the tune_channel command is to configure the WL18xx chip to operate in a specific Wifi band and channel.

Method

The tune_channel command can be called using the following format:

 calibrator wlan0 wl18xx_plt tune_channel  <channel> <band> <bandwidth>
Where:
  • <channel> is the channel within the wifi band. See the picture below for details.
  • <band> is the wifi band. Ex: 0 means we are in g band equal to 1 means we are in a band
  • <bandwidth> is the bandwidth allocation. Use one of the following values


Channel Band Bandwidth
1-14 0 (2.4GHz)

0/1 (20MHz)
2 (40MHz Upper Primary)
3 (40MHz Lower Primary)

8(J8), 12(J12), 16(J16),

36, 40, 44, 48, 34(J34),
38(J38), 42(J42), 46(J46),
52, 56, 60, 64, 100, 104
108, 112, 116, 120, 124,
128, 132, 136, 140, 149,
153, 157, 161, 165

1 (5GHz)

0/1 (20MHz)
2 (40MHz Upper Primary)
3 (40MHz Lower Primary)

16(J1), 12(J2), 8(J3), 4(J4) 2 (4.9GHz)

0/1 (20MHz)
2 (40MHz Upper Primary)
3 (40MHz Lower Primary)


NoteNote: Channel tune must be executed before any other calibrator activities. There is no default channel tuned.

Examples

The following tune_channel example configures the chip to operate in the 2.4 GHz band at channel 1 without high-throughput.

 calibrator wlan0 wl18xx_plt tune_channel 1 0 0




Set TX Power

Purpose

The set_tx_power command can be used to set the transmission power of the Wl18xx device.

Method

To set TX power, first boot into PLT mode using the power_mode command, then select the channel to use with the tune_channel command. Finally, you can set the power using the set_tx_power command in the following manner:

 calibrator wlan0 wl18xx_plt set_tx_power <output_power> <level> <band> <primary_channel> <2nd_channel> <antenna>
<non_serving_channel> <channel_limitation> <internal> <gain_calculation> <analog_gain_control_id> <post_dpd_gain>
Where:
Parameter Options Description Remarks
output_power 0: (0-20000)
1: (0-20000)
2: (-15000 - (-4000))
According to parameter 10 (gain_calculation):

0 (Normal): Desired output power supplied in dBmX1000 at 125 resolution (1/8 dB) i.e. 16.125[dBm] = 16125
1 (Debug): Desired output power supplied in dBmX1000 at 125 resolution (1/8 dB) i.e. 16.125[dBm] = 16125
2 (Override): Desired BO from PSAT supplied in dBmX1000 at 125 resolution (1/8 dB) i.e. -10.375[dBm] = -10375

Override mode is supported from FW version 8.9.0.0.20 and calibrator version 0.80
level 0-3 System support for different pre-configurable power levels in operational mode.
For PLT usage power level should be configured to 0
band 0: 2.4GHz
1: 5GHz
2: 4.9GHz (JP)
Operation Band
channel_number Channel according to used band Channel according to used band Same as configured in channel of tune channel command
primary_channel_location -1: 40MHz Lower Primary
0: 20MHZ
1: 40MHz Upper Primary
20/40MHz usage Same as configured in bandwidth of tune channel command:
-1 = 3 (40MHz Lower Primary)
0 = 0/1 (20MHz)
1 = 2 (40MHz Upper Primary)
antenna 0-3 Used for TX antenna select:

0: Auto Mode: The FW will automatically selects which TX paths to calculate the power for (based on how many antennas are assembled, band, BW and etc.)
1: TX1: Force TX power calculation for TX1 path
2: TX2: Force TX power calculation for TX2 path
3: Both TX1&TX2: Force TX power calculation for both TX paths

non_serving_channel 0-1 0: Serving
1: Non Serving

The power settings will be set only for non serving rate groups (basic rates only)

channel_limitation 0-1 0: Disabled
1: Enabled

Disable/Enable whether to use the channel power limits from the ini file

internal Not Supported Internal Usage Default 0
gain_calculation_mode 0-2 0: Normal - The BO (digital gain) and the analog gain (VGA/iPA/mixer) are being calculated and set using FW defines

1: Debug - No BO limits at max analog gain settings - at max gain combination there will be no limits for the available BO (digital gain)
2: Override - The analog gain and the digital gain are overridden, i.e. the use can choose which of the analog gain combinations he wants to use (choose 1 of the 4 available combinations) and the user can set the digital gain (digital BO as required)

Option 2 is supported starting from FW 8.9.0.0.20 and calibrator version 0.80
analog_gain_control_id 0-4 Analog settings index For debug purpose only: This indicator is used to indicate the user's chosen analog gain
post_dpd_gain Not Supported Not Supported Default 0


NoteNote: There are no default values.


Examples

One example that matches the 'tune_channel' example above is:

 calibrator wlan0 wl18xx_plt set_tx_power 16125 0 0 1 0 0 0 0 0 0 0 0


TX Continuous Test

Purpose

The purpose of the TX Continuous test to perform continuous transmission to evaluate the WLAN transmission quality.

Method

TX Continuous test sends packets of data to the air, where the data packets parameters are controlled by the PLT command and include parameters such as transmitted rate, transmitted power, destination MAC address, etc...

calibrator wlan0 wl18xx_plt start_tx <delay> <rate> <size> <mode> <data_type> <gi> <options1>
<options2> <source MAC> <dest MAC> <channel_width>
Where
  • <delay> Delay between packets in microseconds
  • <rate> Tx rate, supported rates are given in table below
  • <size> Size of data field in MPDU (in bytes, up to FW 8.9.0.0.19 and Calibrator 0.79: 0-2000, from FW 8.9.0.0.20 and Calibrator 0.80: 0-4065)
  • <mode> Number of packets (0 - endless)
  • <data_type> Not Supported -  default 0
  • <gi> Guard interval
  • 0 – long
  • 1 - short
  • <options1> Unused Field   - default 0
  • <options2> Supported options according to bitmap:  
  • Bit 1: Override CCA (FW 8.9.0.0.2: 0-Don't override, 1-Override)
  • Bit 2: Fixed/Incremental Sequence Number (FW 8.9.0.0.20: 0-Incremental, 1-Fixed)
  • <source MAC> Source MAC address (xx:xx:xx:xx:xx:xx)
  • <dest MAC> Destination MAC address (xx:xx:xx:xx:xx:xx)
  • <channel width> Channel width
  • 0 – 20 MHz
  • 1 – 40 MHz



<rate> transmission rate:

            11b              11g                         11n                             MIMO / 40M
 0 = 1.0 Mbps  4 = 6.0 Mbps  12 = 6.5 Mbps (MCS0)  20 = MCS8 / MCS4 at 40MHz
 1 = 2.0 Mbps  5 = 9.0 Mbps  13 = 13.0 Mbps (MCS1)  21 = MCS9 / MCS5 at 40MHz
 2 = 5.0 Mbps  6 = 12.0 Mbps  14 = 19.5 Mbps (MCS2)  22 = MCS10 / MCS6 at 40MHz
 3 = 11.0 Mbps  7 = 18.0 Mbps  15 = 26.0 Mbps (MCS3)  23 = MCS11 / MCS7 at 40MHz
 8 = 24.0 Mbps  16 = 39.0 Mbps (MCS4)  24 = MCS12 / MCS7,40MHz SGI
 9 = 36.0 Mbps  17 = 52.0 Mbps (MCS5)  25 = MCS13
 10 = 48.0 Mbps  18 = 58.5 Mbps (MCS6)  26 = MCS14
 11 = 54.0 Mbps  19 = 65.0 Mbps (MCS7)  27 = MCS15


Examples

The following is an example on how to use the start_tx command (and other commands) to generate packets.

To set the system in PLT mode, use the power_mode command. This command also loads the PLT firmware if not previously loaded.

The next step is to define channel, band, and bandwidth using the tune_channel command & set the desired TX_power.

Use the start_tx command to generate packets. It is important that each start_tx command is followed by the tx_stop command, which stops the transmission. Finally, use the power_mode command to reset the system to operational mode.


NoteNote: Correct antenna setting are taken from loaded FW with INI settings. assure settings with:

cd /lib/firmware/ti-connectivity/

wlconf -i /lib/firmware/ti-connectivity/wl18xx-conf.bin --get                                                                                      // list all system parameters 

If needed set the correct num of Ant (example for 2x2.4G(MIMO), 1x5G):
wlconf -i /lib/firmware/ti-connectivity/wl18xx-conf.bin --set wl18xx.phy.number_of_assembled_ant2_4=0x02         // Set 2 Ant for MIMO
wlconf -i /lib/firmware/ti-connectivity/wl18xx-conf.bin --set wl18xx.phy.number_of_assembled_ant5=0x01            // Set 1 Ant for 5G


All TX examples are 50% DC and include "channel limits" to compensate the limitations from ini_file

2.4GHz TX:

Modulation types latest.png


(0) 11B

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel  7 0 1
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 7 0 0 0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 500 3 500 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0

(1) 20MHz

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel  7 0 1
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 7 0  0  0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 400 19 3000 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0

(2) 20MHz Primary Upper

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel  7 0 2
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 7 1  0  0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 400 19 3000 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0

(3) 20MHz Primary Lower

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel  7 0 3
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 7 -1  0  0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 400 19 3000 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0

(4) 40MHz Primary Upper

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel  7 0 2
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 7 1  0  0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 300 19 4000 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 1

(5) 40MHz Primary Lower

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel  7 0 3
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 7 -1  0  0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 300 19 4000 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 1


20MHz MIMO

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel 7 0 1
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 7 0 0 0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 300 27 4065 0 0 0 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0


5GHz TX:
20MHz

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel 36 1 1
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 1 36 0 0 0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 400 19 3000 0 0 0 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0

40MHz Upper Primary

calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel 36 1 2
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 1 36 1 0 0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 400 19 3000 0 0 0 0 0 00:11:22:33:44:55 01:02:03:04:05:06 1


TX Tone Test

Purpose

The purpose of the tx_tone command is to create and transmit a carrier wave that can be modulated with a fixed audio tone.

Method

The tx_tone command can be called using the following format:

 calibrator wlan0 wl18xx_plt tx_tone_start <mode> <bin index> <antenna mode> <gain index> 

The tx_tone command can be stopped using the following format:

 calibrator wlan0 wl18xx_plt tx_tone_stop 
Where:
NewTxTone.jpg


Note:
1. Silence – TX chain is ON and operational but no signal is transmitted.
2. Carrier Feed Through – TX chain is ON and operational and the LO leakage is transmitted.
3. Single Tone – TX chain is ON and operational and a sinusoidal signal is transmitted with the following configuration options:
    a. Analog Gain Step
    b. Offset from carrier frequency (in OFDM bins)

Examples

The following examples show how to use the tone test:

// 2.4GHz Transmit Silence
calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt tune_channel 6 0 0
calibrator wlan0 wl18xx_plt tx_tone_start 0 0 0 0
calibrator wlan0 wl18xx_plt tx_tone_stop

// 2.4GHz Transmit Carrier Feed Through
calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt tune_channel 6 0 0
calibrator wlan0 wl18xx_plt tx_tone_start 1 0 0 0
calibrator wlan0 wl18xx_plt tx_tone_stop

// 2.4GHz Transmit Single Tone
calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt tune_channel 6 0 0
calibrator wlan0 wl18xx_plt tx_tone_start 2 0 0 0
calibrator wlan0 wl18xx_plt tx_tone_stop

// 2.4GHz Transmit Single Tone with -5MHz offset from the LO
calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt tune_channel 6 0 0
calibrator wlan0 wl18xx_plt tx_tone_start 2 -5 0 0
calibrator wlan0 wl18xx_plt tx_tone_stop

// 2.4GHz Transmit Single Tone with -5MHz offset from the LO on lowest PA gain step
calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt tune_channel 6 0 0
calibrator wlan0 wl18xx_plt tx_tone_start 2 -5 0 4
calibrator wlan0 wl18xx_plt tx_tone_stop


Older Versions

(TX Tone Command for Version R8.3)

Method

The tx_tone command can be called using the following format:

 calibrator wlan0 wl18xx_plt tx_tone 

NoteNote:

  • The 11b/g/n patterns generated by the modem has power control (digital gain and VGA) with tx power command.
  • The WLAN CW is generated by injecting DC signal to the local oscillator (LO) input thus gain of the CW is determined by the DC level and not controlled in tx_tone command.
  • The CW tone is used only for phase noise measurement and therefore the power level control isn’t required.
  • For FCC, ETSI and other certification tests use 11b/g/n start_tx command.

Examples

The following example set shows how to send a CW.

NoteNote: There is no stob_tone command (to halt the tone use start_tx or power_mode off)

calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt tx_tone

ANT1 & ANT2 Assembly Validation for Production

Purpose

A simple, fast and cheap solution to assure both RF paths are functional. The target is to establish connection with remote AP once using SISO scheme, first on ANT1 and later on ANT2.

Method

The procedure should be very simple:

  1. Download the WLAN driver, change wl_conf (INI) parameter that modified the main antenna to be (ANT2 SISO, BG1)
  2. Establish connection with AP using BG2 (ANT2 - MIMO)
  3. Configure the platform back to the original configuration
  4. Establish Connection with AP after booting using the main antenna (ANT1 SISO, BG2)

The following sequence will be required for the testing procedure:

* Configuration changed to BG1 primary #
 sh sta_stop.sh
 sh unload_wlcore.sh
 cd /usr/sbin/wlconf
 ./wlconf -i /lib/firmware/ti-connectivity/wl18xx-conf.bin -o /lib/firmware/ti-connectivity/wl18xx-conf.bin --set wl18xx.phy.spare0=0x08
* Connected to the AP with SSID = "AP_NAME" using BG1 #
 cd /usr/share/wl18xx
 sh load_wlcore.sh
 sh sta_start.sh
 sh sta_connect-ex.sh "AP_NAME"
* Configuration changed back to BG2 primary #
 sh sta_stop.sh
 sh unload_wlcore.sh
 cd /usr/sbin/wlconf
 ./wlconf -i /lib/firmware/ti-connectivity/wl18xx-conf.bin -o /lib/firmware/ti-connectivity/wl18xx-conf.bin --set wl18xx.phy.spare0=0x00

Re-connect to AP with default SISO on ANT1.