Watchpoints for C28x in CCS 4

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Introduction

This page describes how to setup Hardware watchpoints in CCS 4 for the C28x CPU.

This feature was made available for C28x as of CCS V4.1.2. It was not available in earlier CCS 4 releases.

This short video clip shows how to set up C28x data watchpoints in CCSv5 which is similar to the process in CCSv4.
C28x Data Watchpoint

Other Resources

Configure a Data Watch Point

Make sure you have Code Composer Studio 4.1.2 or later. This feature was not implemented for C28x in prior releases of CCS V4.

Step 1: Make sure you have configured CCS 4 for a C28x target and have connected to the target.

Step 2: In the Debug Perspective, Open the breakpoint dialog: View->Breakpoints

Step 3: Use the pulldown to select a new breakpoint and choose Hardware Watchpoint

Wp001.jpg



Step 4: Specify the address you want to watch, and if it is a read or write access.

Wp002.jpg



Step 5: Right click on the watchpoint and select Properties.

Wp003.jpg



Step 6: From this dialog box you can further configure the watchpoint:

  • Configure a data read/write of a particular value from the address.
  • Configure the size of the data
  • Configure a mask value (bits that will be ignored)




Wp004.jpg
E2e.jpg For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article Watchpoints for C28x in CCS 4 here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox