XDAIS sample algorithm

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Intro

Although XDAIS has existed since 1999, its surprisingly difficult to find a good sample algorithm to use as a baseline for your own algorithm development.

This topic fills that gap, supplying a FIR filter written by vendor TI, built and tested for the c64 Instruction Set Architectures. (porting it to another ISA is simple since its straight C code)

Before venturing into this we suggest you first take a look at the XDAIS docs.

Build & test information

This FIR_TI XDAIS algorithm was built with: -

It was tested with the C6416 Device Cycle Accurate Simulator.

The directory layout is as follows: -

align="center"
Directories in attached sample algorithms
Directory Description
src/fir_ti FIR_TI sample algorithm. Source + CCS Project.
src/api Sample ALG library for clients to use to instantiate XDAIS algorithms
include/ Public include directory
lib/ Public libraries/archives directory
apps/firtest1 Sample application invoking the XDAIS algorithm. Ultra-simple.

CCS projects are available so you can rebuild it.

To run it simply: -

You will see a bunch of FIR filtered result values.

Using FIR_TI as a baseline for your own algorithm

The intent of this topic is not to repeat the high quality XDAIS documentation in describing FIR_TI's usage of the XDAIS concepts. Instead it is intended as a find-replace start-point. i.e. for your own Barcode Scanner algorithm you could start with a find-replace of FIR to BARCODE and then TI to VENDORNAME.

The next step would be to modify your algorithm to implement IALG according to your algorithm's needs i.e. how many buffers do you need, are they scratch/persistent etc.

spru352 and spru360 are the right documents to use to understand how to implement this most efficiently.

Compliance testing

Once you're happy with your new XDAIS algorithm, you want to be sure it really is compliant to the XDAIS standard.

From XDAIS 6.x there is a new freely available tool QualiTI which lets you check this.

This tool will check for namespace compliance, appropriate library names, correct interface points and also print out helpful footprint information.

Making it work in Codec Engine

TI supplies a very powerful framework named Codec Engine (CE) that supports many platforms.

Algorithms that implement predefined interfaces simply 'plug in' to Codec Engine, however if you have a barcode scanner there may not be a standard interface available. In this case you need to either use the IUNIVERSAL interface, or implement custom stubs & skeletons which is described in the Codec Engine Algorithm Creator's User Guide. The SCALE example describes this flow.

It is beyond the scope of this topic to describe this process.

Attachments

Media:firtest.tar.gz

Leave a Comment

Comments

This sample seems to be out of date; it uses an ALG layer instead of DSKT2. Is a more recent sample algorithm available? - Jcoombs 23:03, 28 October 2009 (UTC)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox