XDS560 Trace

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

What is XDS560 Trace useful for?

Find previously “invisible” complex, intermittent, context-sensitive real-time bugs

Fine tune code performance and cache optimization of complex switch intensive multi-channel applications

There is a summary presentation here that describes how XDS560 Trace works, what it is useful for, and provides some examples. : Trace_Introduction-ext-01.pdf

For use in Code Composer Studio, see: Unified Breakpoint Manager

How large of a Trace Buffer should be used?

The XDS560 trace pod comes with 64MB of Buffer memory. However, you can configure trace to use any of the following values: 256Kb, 512kB, 1Mb, 2Mb, 4Mb, 8Mb, 16Mb, 32Mb, 64Mb.

Why not just use the largest buffer (64Mb)?

With a 64Mb buffer, you will capture the maximum amount of data. Keep in mind, though, this is 64Mb of compressed data. It is estimated that a 64Mb buffer could potentially hold 1.5 Billion PC Trace data samples, which could require up to an estimated 135 GBs of disk space for the Trace Display to decompress, with estimated decode time on the order of 12 hours. And then, once it's decompressed, there is still more processing to do to make the data useful.

The problem with the existing trace display is that it decodes the entire buffer and tries to display it. It must keep all samples around, and thus uses up gigabytes of disk space storing it all. There will be other decoding solutions that provide for simultaneous decoding and processing of the data that will alleviate the disk space requirement. However, now there is more burden on the processing application to gather the necessary data prior to discarding each piece of decoded data. This can have an impact on the decoding time.

The recommendation is to start with a small buffer and see if it gets you enough data. If it does not, gradually increase the size of the data and run again until you see desired results. Efficient use of AET triggers allows trace to capture only data that is interesting to your scenario and to eliminate data that is not applicable. Clever triggering can allow the user to reduce the size of the capture buffer.

Using the Embedded Trace Buffer (ETB)

Some devices feature the Embedded Trace Buffer. If you use the ETB you do not need the XDS560 Trace hardware, just a JTAG connection through an emulator to use Trace.

XDS560 Trace Pod Technical Requirements

The XDS560 Trace unit utilizes the 60-pin TI JTAG Connectors. The 60-Pin Emulator Header User's Guidedescribes the 60-pin connector and target board electrical requirements for XDS560 Trace and JTAG support. Also see your Emulator manufacturer's documentation for emulator specific information. Users may also want to read the "Common Trace Transmission Problems and Solutions" at tidoc:SPRAAK6.

Debugging with Trace

Detailed documentation on the trace system, trace configuration and setting up trace jobs using Standard (PC, data and timing) and Event trace for debug can be found at Debugging with Trace.

Debugging with Trace provides:

XDS560 Trace Display

TracewithETBDVTAnalyzer.jpg

XDS560 Trace Software Versions

Conference Presentations

Publications & Articles

Related



Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox