XDS560v2 LAN Configuration

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Background

Most XDS560v2 emulators can be configured to use USB or Ethernet.  Ethernet a number of benefits such as being able to remotely debug a board that is located in a lab or another location that is not directly connected to your workstation.  Another key benefit is that it allows you to share boards between different users.

Setup

If you are going to setup your XDS560v2 emulator on a network , you could use DHCP or static IP address.

If the DHCP assigned IP address is changing often, then a static IP address would be a better option. This is because when connecting to the emulator in CCS you need to specify the IP address to use, thus if it is changing you will need to be continually updating your CCS target configuration.

Dynamic IP Address

Get the IP Address


 

Static IP Address

Talk to your IT Administrator

Provide the MAC address of the emulator (written on the bottom) to your IT administrator and request a static IP address and a name for the device. You will also need the address of the gateway for your network or sub-net. If you explain exactly what you are trying to do it will help your IT admin to provide the necessary information.

Configuring the Emulator

Now you need to configure your emulator.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox