DM814x AM387x PSP User Guide
From Texas Instruments Embedded Processors Wiki
DM816x refers to DM816x/AM389x devices unless specified.
DM814x refers to DM814x/AM387x devices unless specified.
DM81xx refers to both DM816x, DM814x and DM813x.
Read This First
1) HDVPSS binaries are no longer packaged with release tar ball, instead they can be downloaded from the PSP Software Download page
2) Suspend to memory/resume is supported, if UART wake-up/resume is desired then "no_console_suspend" needs to be passed as part of bootargs.For more details refer to Suspend to Memory
About this Manual
This document describes how to install and work with Texas Instruments' Platform Support Package (PSP) for the DM8148 platform. This PSP provides a fundamental software platform for development, deployment and execution on DM8148 EVM. It abstracts the functionality provided by the hardware. The product forms the basis for all application development on this platform.
In this context, the document contains instructions to:
- Install the release
- Build the sources contained in the release
The document also provides detailed description of drivers and modules specific to this platform - as implemented in the PSP.
Important
This release has been tested on DM8148 EVM (Base board + daughter card required to verify NOR)
Installation
Prerequisites
Before you begin with the installation of the package please make sure you have met the following system requirements:
- Windows machine
- Host machine running a version of Linux such as RedHat Enterprise Linux or Ubuntu.
- DM8148 EVM
The Windows machine is used for running CCSv4, which will be used to build flash writers and also to burn the boot images (U-Boot) onto the flash using the flash writers provided.
The Linux host is used for the following:
- Recompiling U-Boot and the Linux kernel.
- Hosting the NFS server to boot the EVM with NFS as root filesystem
You can use either the Windows machine or the Linux host for
- Hosting the TFTP server required for downloading kernel and file system images from U-Boot using Ethernet.
- Running a serial console terminal application
Software Overview
To begin developing applications, you need to install PSP package and the toolchain.
Package Contents
Important
The values of MM, mm, pp and bb in this illustration will vary across the releases and actually depends on individual component versions
Extract the contents of release package on your Linux host with the following command:
$ tar -xvfz TI814x-LINUX-PSP-MM.mm.pp.bb.tgz
This creates a directory TI814x-LINUX-PSP-MM.mm.pp.bb with the following contents:
\---TI814x-LINUX-PSP-MM.mm.pp.bb |----TI814xPSP_Software_Manifest +----docs | |----DM814x_AM387x_PSP_MM.mm.pp.bb_Release_Notes.pdf | |----DM814x_AM387x_PSP_User_Guide.pdf | |----DM81xx_AM38xx_Audio_Driver_User_Guide.pdf | |----DM81xx_AM38xx_EDMA_Driver_User_Guide.pdf | |----DM814x_AM387x_PSP_U-Boot.pdf | |----DM814x_AM387x_VPSS_Video_Driver_User_Guide_PSP_MM.mm.pp.bb.pdf | |----DM81xx_AM38xx_PSP_McSPI_Driver_Guide.pdf | |----DM814x_AM387x_PSP_MM.mm.pp.bb_Feature_Performance_Guide.pdf | |----DM81xx_AM38xx_PSP_MMC_SD_Support.pdf | |----DM816x_AM389x_HDMI_User_Guide.pdf | |----DM81xx_AM38xx_PCI_Express_Root_Complex_Driver_User_Guide.pdf | |----DM81xx_AM38xx_PCI_Express_Endpoint_Boot_Driver_User_Guide.pdf | |----DM81xx_AM38xx_USB_User_Guide.pdf | |----DM81xx_AM38xx_PSP_WDT_Support.pdf | |----DM814x_AM387x_PSP_Flashing_Tools_Guide.pdf | |----DM81xx_AM38xx_PSP_TouchScreen_Driver_Guide.pdf | |----DM814x_AM387x_PM_Suspend_resume_overview.pdf +----host-tools | |----nand-flash-writer.out | |----nor-flash-writer.out | |----spi-flash-writer.out | |----mksd-ti814x.sh | |----DM814x_gel.zip | +----src | | |----nandflash-MM.mm.pp.bb.tar.gz | | |----norflash-MM.mm.pp.bb.tar.gz | | |----spiflash-MM.mm.pp.bb.tar.gz +----images | +----kernel | | +----ti814x | | | |----uImage | +----u-boot | | |----ti814x | | | |----u-boot.bin | | | |----u-boot.min.nand | | | |----MLO | +----examples | | |----pcie | | | |----saBootApp +----src | +----kernel | | |----ChangeLog-MM.mm.pp.bb | | |----diffstat-MM.mm.pp.bb | | |----kernel-patches-MM.mm.pp.bb.tar.gz | | |----linux-MM.mm.pp.bb.tar.gz | | |----ShortLog | | |----Unified-patch-MM.mm.pp.bb.gz | +----u-boot | | |----ChangeLog-MM.mm.pp.bb | | |----diffstat-MM.mm.pp.bb | | |----ShortLog | | |----u-boot-patches-MM.mm.pp.bb.tar.gz | | |----u-boot-MM.mm.pp.bb.tar.gz | | |----Unified-patch-MM.mm.pp.bb.gz | +----examples | | |----examples.tar.gz | | |----pcie | | | |----bootscript.txt | | | |----saBootApp.c | | | |----Makefile | | | |----README
Few points to note about the above structure:
Assuming the release package is extracted inside directory represented as $TI814x-PSP-DIR:
- U-Boot source tarball is u-boot-MM.mm.pp.bb.tar.gz needs to be extracted on Linux build host. This will create U-Boot source base for TI814x
$ cd $TI814x-PSP-DIR/TI814x-LINUX-PSP-MM.mm.pp.bb/src/u-boot $ tar -xvfz u-boot-MM.mm.pp.bb.tar.gz
- Similarly kernel source tarball linux-MM.mm.pp.bb.tar.gz from TI814x-LINUX-PSP-MM.mm.pp.bb/src/kernel directory needs to be extracted to have kernel source directory setup for building kernel and/or modules
$ cd $TI814x-PSP-DIR/TI814x-LINUX-PSP-MM.mm.pp.bb/src/kernel $ tar -xvfz linux-MM.mm.pp.bb.tar.gz
- Various Video and Audio example sources are included inside $TI814x-PSP-DIR/examples/examples.tar.gz
- Additionally, PCIe Endpoint boot application is provided in pcie directory inside $TI816X-PSP-DIR/examples
Toolchain
To build U-Boot and the Linux kernel, you will need to download and install CodeSourcery ARM tool chain version 2009-q1. For additional documentation on installing the CodeSourcery tools, please visit the CodeSourcery website.
To help you get started quickly the PSP package comes with pre-built binaries. However, after making any changes to U-Boot and Linux Kernel you need to cross-compile them using the CodeSourcery toolchain and use the new binaries that are generated
Environment Setup
After you have installed the CodeSourcery toolchain you need to setup the environment in the Linux host.
- Set the environment variable PATH to contain the binaries of the CodeSourcery cross-compiler tool-chain.
- For example, in bash:
$ export PATH=/opt/toolchain/2009-q1/bin:$PATH
- Add the location of U-Boot tools directory to the PATH environment variable (required for mkimage utility that is built as part of U-Boot build process and is needed to generate uImage when building the kernel)
- For example, in bash:
$ export PATH=/opt/u-boot/tools:$PATH
Note
Actual commands to be used for setting the environment variables will depend upon your shell and location of the tools
Flashing Tools
On DM8148 EVM, the Cortex-A8 core boots up first. On boot-up, the ARM core runs the U-Boot image which need to be present in the flash memory of the EVM.
The flash-writers are a part of the PSP package. Instructions on how to use the flash-writers in CCSv4/v5 can be found in PSP Flashing Tools Guide (DM814x_AM387x_PSP_Flashing_Tools_Guide.pdf).
U-Boot
Please refer to U-Boot User Guide for details about U-Boot in the context of DM814x.
Linux Kernel
This chapter describes the steps required to build and configure the Linux kernel. It also provides basic steps to boot kernel on the EVM.
Compiling Linux Kernel
Change to the base of the Linux source directory.
Choose default kernel configuration for your platform.
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8148_evm_defconfig
Initiate the build.
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm uImage
Note
For the kernel image (uImage) to be built, mkimage utility must be included in the path. mkimage utility is generated (under tools folder of U-Boot) while building the U-Boot binary.
On successful completion, file uImage will be created in the directory ./arch/arm/boot.
Copy this file to the root directory of your TFTP server.
Modifying Kernel Configuration
DM8148 EVM
This section describes the steps to configure the kernel for DM8148 EVM and illustrates related configuration items for reference.
Start with the default configuration for your platform
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8148_evm_defconfig
To view configuration interactively:
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm menuconfig
From the onscreen menu, select System Type and press ENTER:
General setup ---> [*] Enable loadable module support ---> -*- Enable the block layer ---> System Type ---> Bus support ---> Kernel Features ---> ... ...
Select ARM system type
ARM system type (TI OMAP) ---> TI OMAP Common Features ---> TI OMAP2/3/4 Specific Features --->
You will be presented with various ARM based SoCs. Select OMAP as
(X) TI OMAP
After pressing ENTER, you will be presented earlier menu. Select "TI OMAP2/3/4 Specific Features" and press ENTER. Select various options as shown below (marked with '[*]') by pressing Y on each item after selecting it.
[*] Typical OMAP configuration [ ] TI OMAP2 [ ] TI OMAP3 [ ] TI OMAP4 [*] TI 81XX [ ] TI816X support [*] TI814X support ... *** TI81XX Board Type *** [*] TI8148 Evaluation Module
Note that the "TI814X support" option will be shown only if you enable "TI 81XX". Similarly, "TI8148 Evaluation Module" option will be presented only after selecting "TI814X support"
Choose Exit successively to return to previous menu(s) and eventually back to the shell. Make sure to save the changes you have made when prompted at exit.
Some of the key drivers which may be enabled in the default configuration are:
- Serial port
- SATA
- Ethernet
- I2C
- Audio
- MMC/SD
- NAND
- PCI Express Root Complex
- PCI Express Boot Driver
- PCI Express EP Driver (mutually exclusive with RC driver)
If you are looking for some particular functionality please double-check that it is enabled in the config options.
Auto detection of Kernel Load Address and Run Time RAM Base Determination
Note: This section is only applicable to 04.01.00.07 DM814x and onwards release of Linux kernel.
By default, the DM814x kernel is built to be loaded at physical address 0x80008000 in RAM and take start of RAM as 0x80000000.
It is possible to load the kernel at a different location in RAM with kernel automatically determining RAM base depending upon the load address.
This is achieved by the combination of two features added the kernel:
- Run time PHYS_OFFSET determination: This feature enables determining physical to virtual translations dynamically depending upon the position of kernel in system memory.
- Auto calculation of address for uncompressed kernel: This feature enables the compressed kernel entry code (part of kernel zImage) to determine the address to uncompress the kernel depending upon the location it is loaded (started from).
Subsequent sub-sections assume that you have already downloaded and extracted the kernel snapshot from above mentioned link/page or set up git working directory with latest PSP kernel from repository associated with the above page. It is also assumed that the environment for kernel build is setup and 'mkimage' executable utility from U-Boot is available in the PATH (this utility gets built with U-Boot and available inside 'tools' directory form U-Boot source base).
Configuring the Kernel
Note: The run time physical offset support is treated as EXPERIMENTAL feature currently. The default kernel configurations for DM8148 EVM have this feature enabled in latest source. You can follow steps similar to those described below and build the kernel to enable this support for any custom board as well as to view/disable this feature as per the need.
Generate default config for the Board
For DM8148 EVM:
BUILDHOST$ make ARCH=arm ti8148_evm_defconfig
The above steps should configure the kernel to include run time physical to virtual translation support (CONFIG_ARM_PATCH_PHYS_VIRT=y) and auto detection of load address (CONFIG_AUTO_ZRELADDR=y).
If you desire to view the exact configuration options to be controlled to enable or disable these features, read the next steps.
Enter the configuration menu
BUILDHOST$ make ARCH=arm menuconfig
You will be presented with configuration menu as shown below:
[*] Patch physical to virtual translations at run time (EXPERIMENTAL) General setup ---> [*] Enable loadable module support ---> ... Kernel Features ---> Boot options --->
Enable/Disable runtime physical to virtual translation feature
Ensure that the "Patch physical to virtual translations..." option is highlighted and press 'n' key (without quotes) to disable it (the default kernel configuration done in the earlier step had enabled this option).
[ ] Patch physical to virtual translations at runtime (EXPERIMENTAL) General setup ---> [*] Enable loadable module support ---> ...
Pressing 'y' on this option will (again) enable it.
Enable/Disable auto calculation of decompressed kernel location
Now navigate to "Boot options --->" option by using DOWN arrow key and press SPACE to enter the sub-menu shown below.
Here, using DOWN ARROW key, navigate to the option "Auto calculation..." and press 'y' to enable or 'n' to disable it. You should see a '*' in the box '[ ]' in front of that option when 'y' is pressed (enable) otherwise the box will be empty (disabled) when 'n' is pressed.
(0) Compressed ROM boot loader base address (0) Compressed ROM boot loader BSS address () Default kernel command string [ ] Kernel Execute-In-Place from ROM [ ] Kexec system call (EXPERIMENTAL) [*] Auto calculation of the decompressed kernel image address
Using RIGHT arrow key, highlight the 'Exit' option on the menu page and press ENTER key subsequently till you are asked to save the configuration. Now ensure that 'Yes' is highlighted and press ENTER again to save and exit the configuration.
Building the Kernel
Use following command to build the kernel:
BUILDHOST$ make ARCH=arm zImage
Notice that we are building the standard zImage (compressed kernel image) instead of usual uImage. This is so because the uImage built as part of kernel build will have the load address and entry point @0x80008000 by default while, in this case we desire to load the kernel at different load address. Hence we build a zImage and then pass the desired address to 'mkimage' to get uImage as shown below.
Here we use 0x90008000 as the kernel load address and entry point.
Note: You can chose any other address as per your requirement and available RAM space but please refer next section Points to Note/Restrictions for various important points and constraints.
Use 'mkimage' to generate uImage. Note that the command is run from the kernel source base after zImage is built successfully.
BUILDHOST$ mkimage -A arm -O linux -T kernel -C none -a 0x90008000 -e 0x90008000 -n 'Linux-2.6.37' -d arch/arm/boot/zImage uImage
Image Name: Linux-2.6.37
Created: Mon Oct 29 21:05:21 2011
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2570504 Bytes = 2510.26 kB = 2.45 MB
Load Address: 90008000
Entry Point: 90008000
You can build the zImage once and just execute the 'mkimage' step for different load address requirements with same kernel.
Alternate Method: Single Step Build
You can still achieve the above in single step as part of kernel build by passing zreladdr-y=<desired-load-address> to make when building the uImage.
For example, to build the uImage with load address 0x90008000 considered in earlier case:
BUILDHOST$ make ARCH=arm zreladdr-y=0x90008000 uImage
The above command will build the kernel zImage and then uImage by internally invoking 'mkimage' with the specified load address (passed as zreladdr-y).
Note: In any case, you need to rebuild the uImage for specific load address.
Points to Note/Restrictions
- Load address and entry point parameter passed to 'mkimage' must be same, that is, values passed for '-a' and '-e' must be same.
- The auto address calculation of load address is only possible when using compressed kernel image (zImage) and thus, the uImage must be built from zImage - using uncompressed kernel image (Image) will not support this feature.
- The run time physical RAM base calculation support (called as p2v) adds a string "p2v8" to module version and thus the modules built without p2v support cannot be loaded on the kernel built with p2v support enabled and vice verse. This prevents incompatible modules being loaded mistakenly.
- This feature may not be used with XIP kernels.
- Run time physical offset determination feature is an EXPERIMENTAL feature presently.
- The kernel compressed entry code which determines the address for loading uncompressed kernel considers that the compressed kernel image (zImage) is loaded within first 128MB of the RAM, this also means that the RAM base is determined by masking least significant (LS) 27 bits of the load address.
- There must be at least 32KiB space available *after* the determined RAM base (see above point) and *before* the kernel load address specified when preparing uImage.
Refer Choosing Load Address and Determination of RAM Base section below for details and examples.
Choosing Load Address and Determination of RAM Base
As mentioned earlier, the load address must be chosen such that it leaves at least 32KiB space below it from the RAM base. This is required since the kernel uses this region of RAM below the image to store page tables (in normal execution as well as during decompress).
Also note that since the RAM base is calculated by truncating to the nearest 128MiB boundary (masking LS 27 bits of the load address), the LS bits getting masked need to evaluate to at least 32K offset from the RAM base (that is, 0x8000 minimum).
Following are some examples of correct load addresses (with automatically calculated RAM base) followed by a few incorrect ones:
Correct Load Addresses
| Load Address | Calculated RAM Base |
|---|---|
| 0x90008000 | 0x90000000 |
| 0x90010000 | 0x90000000 |
| 0x91000000 | 0x90000000 |
| 0x98100000 | 0x98000000 |
| 0x98104000 | 0x98000000 |
| 0x80008000 | 0x80000000 |
| 0x88100000 | 0x88000000 |
Incorrect Load Addresses
Following addresses would result into a non bootable kernel (kernel will hang/halt during boot):
| Load Address | Problem Area |
|---|---|
| 0x90000000 | Calculated RAM base = 0x90000000 (masking to 0xF8000000), which means the 32KiB requirement for load address is not met |
| 0x98000000 | RAM base = 0x98000000, 32KiB requirement not met |
| 0x98004000 | RAM base = 0x98000000, only 16KiB available below the load address |
Modifying Pin Mux settings
On DM814x devices, the pins are tri-stated and set to Mode 0 or any other mode as required for specific module (e.g., MMC) in U-Boot. If you desire to use a particular pin to any other function than Mode 0 or override any other pin mode which was already set in U-Boot, the kernel needs to be modified and rebuilt.
You can change default mux mode by adding specific mux entry in the beginning of board_mux array in arch/arm/mach-omap2/board-ti8148evm.c or calling omap_mux_init_signal() during initialization (e.g., in device specific initialization function called from omap2_init_devices() in arch/arm/mach-omap2/devices.c).
The names of multiplexed signals are specified in arch/arm/mach-omap2/mux814x.c file in kernel source directory.
e.g., for setting xref_clk0 pin (mode 0) to usb1_drvvbus (mode 7 or FUNCTION 8), add
TI814X_MUX(XREF_CLK0, OMAP_MUX_MODE7)
to board_mux structure in board file or call
omap_mux_init_signal("xref_clk0.usb1_drvvbus", 0)
Note: The string passed above should be mode0_name.desired_mode_name format.
The API approach is useful if you desire to set the pin-mux run time depending upon the board/hardware detected without need of maintaining separate kernel binaries.
Note: On DM814x devices, the bit positions for pull up/down are different and hence use macros TI814X_PULL_DIS (to disable pull up/down) or TI814X_PULL_UP to select pull up.
Alternatively, you can set particular pins by passing respective pinmux details to kernel command line in following format
omap_mux=<mode0_name>.<signal_name>=<value>,<mode0_name>.<signal_name>=<value>
E.g., to set mmc1_cmd_mux0 (mode 0) pin to gpio0_0 and enable pull down, append following to kernel command line passed from the boot loader:
omap_mux=mmc1_cmd_mux0.gpio0_0=0
For pull up (set bit 17):
omap_mux=mmc1_cmd_mux0.gpio0_0=0x20000
You can pass configuration for multiple pins separated by comma.
For details about this boot parameter, refer Documentation/kernel-parameters.txt in kernel source directory.
Distinguish between chip revisions run time
Sometimes a kernel module/driver may require to do specific handling depending upon DM814x chip revision. To achieve this, the exported kernel API omap_rev() can be used as shown in following example:
- Ensure that plat/cpu.h file is included in your driver file
#include<plat/cpu.h>
- Use following kind of block to handle specific configuration for chip revisions which or PG 2.0 and onwards:
... if (omap_rev() != TI8148_REV_ES1_0) /* Handle non PG 1.0 device configurations */ else /* Do the configuration for PG 1.0 devices */ ...
You can find all the supported chip revision macros by searching for "TI8148_REV_ES" (without quotes) in arch/arm/plat-omap/include/plat/cpu.h file from kernel source.
Using The Correct Console Device
On the latest kernel packaged in this release, the serial device names are changed from ttySx to ttyOx. Thus, the serial port associated with UART0 is now referred as ttyO0.
- This means you will need to update 'bootargs' as passed to kernel to use ttyS0 as console. For example, change
console=ttyS0,115200n8
to,
console=ttyO0,115200n8
- The subsequent example 'bootargs' use the new console name and will not work with kernel from older releases.
- Similarly, you will need to update the
/etc/inittabfile in the filesystem used for kernel by replacing lines with 'ttySx' by 'ttyOx'. For example, replace following
S:2345:respawn:/sbin/getty 115200 ttyS0
by,
S:2345:respawn:/sbin/getty 115200 ttyO0
Note: The character 'O' in the serial port names stands for "OMAP UART Port".
Updating the DHCP Script
The latest (2.6.37-rc3) kernel has changed the entry for root filesystem name as appear in /proc/mounts file. This might impact boot process if some of the init scripts in your filesystem read this entry to determine the root device type.
The existing scripts checking /proc/mounts may not work as intended.
One such case is the /etc/udhcpc.d/50default script in the filesystem, which skips sending DHCP requests if the root device is a network mounted filesystem.
If you face any issue where the filesystem is mounted successfully but hangs after showing udhcpc related prints. The issue is most likely with incompatibility between latest kernel and the udhcpc script.
To fix this, open the /etc/udhcpc.d/50default in your DM81xx filesystem and check if a check like the one shown below exists:
root_is_nfs() {
grep -qe '^/dev/root.*\(nfs\|smbfs\|ncp\|coda\) .*' /proc/mounts
}
Update the above fragment by replacing the check as below:
root_is_nfs() {
grep -qe 'nfs\|smbfs\|ncp\|coda.*' /proc/mounts
}
Proceed to use this filesystem with kernel.
Booting Linux Kernel
Kernel along with root filesystem can either be booted from on board storage device or can be fetched over the Ethernet or UART to RAM using TFTP or serial protocols like YMODEM and booted from there. Also, the root filesystem can be formatted as JFFS2 or UBIFS, flashed and mounted. Please refer to the U-Boot User Guide for details about flashing and supported storage devices.
Following sections describe various kernel boot options possible.
- Note: The offsets and MTD partition numbers used in examples below may vary depending upon actual partition layout used on particular storage device. Also, selecting multiple storage device support in kernel (e.g., NAND & SPI) may change the effective partition number to be used as root partition.
Boot from NAND
Make sure the Boot Mode/Configuration Select Switch is set for the NAND boot mode as described in Booting U-Boot section.
Power on EVM and wait for U-Boot prompt of the 2nd stage (TI8148_EVM#) to come up on the serial console.
When kernel uImage and JFFS2 or UBIFS filesystem are flashed on the NAND device:
TI8148_EVM# nand read.i 0x81000000 280000 500000 For JFFS2 file system: TI8148_EVM# setenv bootargs 'mem=128M console=ttyO0,115200n8 noinitrd root=/dev/mtdblock9 rw rootfstype=jffs2 ip=dhcp' For UBIFS file system: TI8148_EVM# setenv bootargs 'console=ttyO0,115200n8 noinitrd mem=256M rw ubi.mtd=9,2048 rootfstype=ubifs root=ubi0:rootfs init=/init' TI8148_EVM# bootm 0x81000000
When kernel image is flashed on the NAND device, and NFS mounted filesystem is being used:
TI8148_EVM# nand read.i 0x81000000 280000 500000 TI8148_EVM# setenv bootargs 'console=ttyO0,115200n8 root=/dev/nfs nfsroot=172.24.179.98:/nfs_root,nolock rw mem=128M' TI8148_EVM# bootm 0x81000000
Boot from SPI
Make sure the Boot Mode/Configuration Select Switch is set for the SPI boot mode as described in Booting U-Boot section.
Power on EVM and wait for U-Boot prompt of the 2nd stage (TI8148_EVM#) to come up on the serial console.
Assuming kernel image is flashed on the SPI flash @0x42000 and NFS based root filesystem is used:
TI8148_EVM# sf read 0x81000000 0x42000 0x200000 TI8148_EVM# setenv bootargs 'console=ttyO0,115200n8 root=/dev/nfs nfsroot=172.24.179.98:/nfs_root,nolock rw mem=128M' TI8148_EVM# bootm 0x81000000
Boot from NOR
Make sure the Boot Mode/Configuration Select Switch is set for the NOR boot mode as described in U-Boot User Guide.
Power on EVM and wait for U-Boot to come up on the serial console.
Assuming kernel uImage and JFFS2 filesystem are flashed on the NOR device @0x08060000 (Partition 2) and @0x08460000 (Partition 3) respectively:
TI8168_EVM# cp.w 0x08060000 0x81000000 0x200000 TI8168_EVM# setenv bootargs 'mem=128M console=ttyO2,115200n8 noinitrd root=/dev/mtdblock3 rw rootfstype=jffs2 ip=dhcp' TI8168_EVM# bootm 0x81000000
Boot over Network (Ethernet)
Note
When setting a MAC address please ensure that the LS-bit of the 1st byte is not 1 i.e. when setting the MAC address: y in xy:ab:cd:ef:gh:jk has to be an even number. For more info this refer to the wiki page http://en.wikipedia.org/wiki/MAC_address
When kernel image and ramdisk image are fetched from a TFTP server:
- Ensure that the EVM is connected to network with DHCP and TFTP server set up
- Set 'ethaddr' U-Boot environment variable with proper ethernet address in format 'xx:xx:xx:xx:xx:xx' (replace 'xx' with proper hexadecimal values)
- Copy kernel image and ramdisk to TFTP server's root directory.
- Ensure that the "Options Negotiation" box in the tftp server settings is not checked.
- Execute following commands at U-Boot prompt. We assume kernel image name as 'uImage' and ramdisk file name as 'ramdisk.gz'
TI8148_EVM# setenv autoload no TI8148_EVM# dhcp TI8148_EVM# setenv serverip <Server IP Address> TI8148_EVM# tftp 0x81000000 uImage TI8148_EVM# tftp 0x82000000 ramdisk.gz TI8148_EVM# setenv bootargs 'mem=200M console=ttyO0,115200n8 root=/dev/ram0 initrd=0x82000000,40M ramdisk_size=32768 ip=dhcp' TI8148_EVM# bootm 0x81000000
- Alternatively, kernel can be made to use the same IP address as assigned to U-Boot instead of doing DHCP request again by setting U-Boot parameters as follows:
TI8148_EVM# print ethaddr <-- Check if MAC address is assigned and is unique
TI8148_EVM# setenv ethaddr <unique-MAC-address> <-- Set only if not present already, format xn:yy:zz:aa:bb:cc
TI8148_EVM# setenv bootcmd 'dhcp;run addip; tftp 81000000 uImage;bootm'
TI8148_EVM# setenv hostname <unique-hostname>
TI8148_EVM# setenv addip 'setenv bootargs ${bootargs} ip=${ipaddr}:${nfsserver}:${gatewayip}:${netmask}:${hostname}:eth0:off'
TI8148_EVM# setenv autoload no
TI8148_EVM# setenv nfsserver <nfs-server-ip> <-- Make sure the same NFS server IP is used below
TI8148_EVM# setenv bootargs 'console=ttyO0,115200n8 root=/dev/nfs nfsroot=<nfs-server-ip>:<path-to-nfs-share>,nolock rw mem=128M'
TI8148_EVM# setenv serverip <tftp-server-ip>
TI8148_EVM# saveenv
TI8148_EVM# boot
- After saving the environment variables, you need not set them again on reboot unless a change is required.
- Note that the above example uses NFS mounted root file system accessed over 'eth0' interface (as available on the base EVM)
Note: You need not set 'ethaddr' for devices having valid MAC IDs set. In such cases, U-Boot will automatically detect and set the ethernt address (should show message like "Detected MACID:...").
Power Management
Note: On PG 1.X revisions of DM814X chip, only clock framework is supported, other PM features are not supported
Clock details
H/W Details
DM814x has two on chip oscillators which are the main source of clock, OSC0 - 20 MHz and OSC1(20-30MHz). Centaurus has 13 PLLs, by default OSC0(20 MHz) provides the input clock source for all PLLs.These PLLs are configured to generate higher frequencies required for interface and functional clocks of various modules on the device.Clock out from PLLs is distributed to various modules as per the hardware connections and requirements, with divider at place where lower frequencies are required.
Clock Framework Overview and Usage
For clock framework software implementation, features and usage refer to Clock Framework User Guide
Suspend to Memory
NOTE: Lowest 1 KB(1024 Bytes from the end) of OCMC RAM is used by Suspend code to execute from OCMC when DDR is placed in Self-refresh mode during suspend/resume.This memory area will be over-written by Suspend code when kernel is loaded, during SRAM initialization so drivers should avoid using the lowest 1KB of OCMC RAM
Suspending a system drives the system to a low power state there by saving power as and when desired by the user. For overview of Suspend to memory implementation, features and usage refer to DM814x AM387x Suspend Resume User Guide
GPIO Driver
DM814X has four GPIO modules provides 32 dedicated general-purpose pins with input and output capabilities, total 0 - 127 pins are available for usage.
GPIO Driver User Guide have more details of driver usage
EDMA3 Driver
Audio Driver
The audio driver in the PSP package conforms to the ASoC framework in the Linux kernel. The current driver supports audio capture and playback using the AIC3106 codec on the EVM. For more details on the audio driver refer to the following page:
SATA Driver
The SATA subsystem supports one 3Gbps SATA host port capable of supporting Port Multiplier and direct connect SATA devices.
SATA driver in the Linux kernel has support for
- HDD
- CD/DVD
- Port Multiplier
NOTE: In case of external RAID storage towers (via ahci), the storage tower should be configured using the windows/Linux(x86) tool before connecting it to TI8148 EVM
Features not supported,
- Port Multiplier support has some issues when port 0 of port multiplier is used. Do not use port 0 of PM and connect devices to other ports in PM, OR hotplug devices after Linux is up. These are just workarounds.
Note: Refer SATA FAQ for more information.
USB Driver
The USB subsystem includes two USB(mentor) controller.
Note for DM814X: For EVMs with PG2.1 silicon, there is jumper J22/J23 for usb0/usb1 ports respectively. For usb host mode, short the jumper J22/J23 for usb0/usb1 ports and connect the mini-A to A-receptacle connector to usb0/usb1 port. For device mode operation, J22/J23 shall be left open(do not short) and connect mini-B to standard A plug to usb0/usb1 port of EVM to usb-host/PC. If EVM has micro connector use micro-A to A-receptacle (for host mode) and micro-B to standard-A plug (for device mode).
USB_ID configuration: The USB0-ID/USB1_ID input to DM814X decides the role of usb mode to be either host or device for USB0/USB1 mentor usb controllers. USBx_ID should be floating (open) for device mode and grounded for host mode operations The configuration of USBx_ID pin can be done by
- software control (only supported on DM814X PG1.x revision)
- usb plug type inserted to usb connector (micro/mini-A plug for host mode, micro/mini-B plug for device mode).
- by on board USBx_ID jumper setting to either short/open the ID pin for force host/device mode respectively.
The USBx_ID is always software controlled for DM814X PG1.x silicon. In PG2.0 onwards USBx_ID is configured through either external usb plug type or onboard jumper setting. This configuration is done by chosing appropriate configuration through USBx_ID menuconfig selection. more information refers to USB Configuration page
SD driver
SD Driver supports SD/SDHC/uSD cards. HSMMC peripheral (and driver) has support for 4 data lines at the max operating frequency of 48MHz. HSMMC is a slave DMA peripheral and uses EDMA to move data between SD card and system memory.
Supported Features
- SD
- SDHC
- uSD
- uSDHC
Not supported Features
- PIO mode of operation
Please refer MMC/SD guide for more details.
Ethernet Switch Driver
Ethernet Switch driver follows standard Linux Network Interface Architecture.
Please refer Ethernet Switch User Guide for more details.
VPSS Video Driver
VPSS Video Capture driver
VPSS Video Capture Driver User Guide
NOTE: V4L2 capture driver is added in PSP04.00.01.13 for DM816x class of devices and
PSP04.01.00.06 for DM814x class of devices.
HDMI Driver
McSPI Driver
Please refer DM81xx_AM38xx_PSP_McSPI_Driver_Guide.pdf in the release package or refer online McSPI Driver Guide.
NOR Flash Support
NOR Porting Guide
Refer to NOR Porting guide for interfacing NOR on various daughter boards to DM81xx.
Board Modification
Following board modifications have to be done in the Catalog board (CATA_x) / Base Board for NOR to work.
1. catalog board: Replace the resistor R230 in the with 0-ohm
This is required for NOR XIP (Execute in place) to work.
NOTE:
Without the above board modifcation(1), NOR boot will not work.
2. DM814X Base board: Remove the resistors R410, R248 (Both values are 22 ohms)
This is required to access the entire NOR memory. NOR address lines (A22 and A23) and HDMI lines are shared.
a) Populating the resistors R410, R248 (Both are 22 ohms) will enable HDMI
b) removing the resistors will disable the HDMI and enable the NOR address lines.
By default, resistors R410, R248 are populated and HDMI is enabled. This puts limitation on the size of NOR memory that can be accessed. With HDMI enabled, NOR device lines A22 and A23 cannot be used and hence the maximum addressible memory is 2^22 = 4 MB. Hence, if the entire NOR memory has to be accessed, then the above modification (2) has to be done.
NOTE: HDMI will not work after this modifcation(2).
NOR Driver Guide
Please refer DM81xx_AM38xx_PSP_NOR_Driver_Guide.pdf in the release package or refer online NOR Driver Guide.
PCI Express Root Complex Driver
Please refer the PCIe RC Driver User Guide for particular release in PDF format from the release package. The latest document is available online.
PCI Express Endpoint Boot Driver
Please refer the PCIe Boot Driver User Guide in PDF format from the release package for details about booting DM814x PCIe Endpoint connected to DM814x/DM816x PCIe Root complex using PCIe boot driver (running on RC). The latest document is available online.
PCI Express Endpoint Driver
Please refer the PCIe Endpoint Driver User Guide in PDF format from the release package for details about using this driver on DM814x PCIe Endpoint part of PCIe topology. The latest document is available online.
TouchScreen Driver
Please refer DM81xx_AM38xx_PSP_TouchScreen_Driver_Guide.pdf in the release package or refer online TouchScreen Driver Guide.
Watchdog Timer (WDT)
The following document covers the details regarding the watchdog timer in DM81xx:
Please refer WDT guide.
TILER
TILER driver has dependency on Multimedia. TILER support is disabled in defconfig. TILER driver can be enabled from,
Device Drivers --->
<*> Multimedia support --->
<*> TI TILER support --->
--- TI TILER support
(128) Allocation granularity (2^n) (NEW)
(4096) Allocation alignment (2^n) (NEW)
(40) Memory limit to cache free pages in MBytes (NEW)
(1) Process security (NEW)
(0) Use SSPtr for id (NEW)
[ ] Secure TILER build (NEW)
[*] Expose SSPtr to userspace (NEW)
Leave the default values as those are the one's which were validated for this release.
Following features are supported in the current TILER driver,
- Single PAT and run-time memory allocation
Features not supported,
- Dual PAT
- PAT by-pass mode