RTSC Codec And Server Package Wizards

From Texas Instruments Embedded Processors Wiki

Revision as of 16:50, 6 November 2009 by DanRinkes (Talk | contribs)
(diff) ← Older revision | Current revision (diff) | Newer revision → (diff)
Jump to: navigation, search


  • Image:Google-16x16.png Search for an article here:


Contents

Introduction

The RTSC Codec Package Wizard and RTSC Server Package Wizard are utilities designed to rapidly create XDC Codec Packages and Codec Engine compatible test servers (containing a single codec).

Both utilities run on Windows and Linux with both GUI and command line options.They are provided with the ceutils (see below)

Note that as of Codec Engine 2.20 a RTSC Combo Package Wizard is now available. It is provided with the Codec Engine and NOT part of ceutils. Customers should gradually migrate to this tool. For consistency/migration many of the same options were preserved. Eventually the server wizard may be deprecated however point-release bug fixes will continue for some time due to it's widespread usage. Additionally the combo wizard requires >= CE 2.20 hence the server wizard will still be necessary for customers using e.g. >= CE 1.20.02. Note that this applies purely to the server wizard (genserver) - the codec package wizard in ceutils below is still the recommended tool for codec packaging.

Download

  • ceutils is available here
    • ceutils v1.07 - released Feb 2009
      • Bug fix update to both the RTSC Codec and Server Package Wizards - see the readme for detailed information
    • ceutils v1.06 - released Sept 2008
      • Ease-of-use update - added top-level Makefile so you can:
        • Run the wizards via a simple "make genpackage" or "make genserver"
        • Avoid typing in a long XDCPATH - an XDCPATH is created for you from the Rules.make in your DVSDK
        • Build your RTSC Codec/Server Package via "make" instead of XDC commands
        • No changes were made to the content produced by RTSC Codec Package or Server Wizards
    • ceutils v1.05 - released Aug 2008
      • Contains: RTSC Codec Package Wizard v0.5.2 and RTSC Server Package Wizard v0.2.3
      • RTSC Server Package Wizard has updated templates to support OMAP3
      • No changes were made to the RTSC Codec Package Wizard
    • ceutils v1.04 - released March 2008
      • Contains: RTSC Codec Package Wizard v0.5.2 and RTSC Server Package Wizard v0.2.2
    • ceutils v1.03 - released Nov 2007
      • Contains: RTSC Codec Package Wizard v0.5.1 and RTSC Server Package Wizard v0.2.1

Prerequisites

The RTSC Package Wizards recommend the following components be installed:

  • CG_XML v1.20 - released Nov 2007
    • CG_XML v1.20 or later is required -- Earlier versions will not work with the wizards
    • A wiki topic on how cg_xml works can be found here

Without Codec Engine and either Codec Engine's CE Tools or xDAIS, the RTSC Codec Package Wizard and RTSC Server Package Wizard will not run at all. Without CG_XML and Code Gen Tools, the RTSC Codec Package Wizard will not be able to determine stack size, section information, or the names of xDAIS functions. Without DSP/BIOS, the server that results from building the output of the RTSC Server Package Wizard cannot be created.

Wizard Instructions

Other Wizard Documents

XDAIS for Codecs

The new QualiTI XDAIS compliance tool is now available in XDAIS 6.10.

References

  • CE User's Guides
    • Codec Engine Algorithm Creator User's Guide - sprued6c
    • Codec Engine Server Integrator's User's Guide - sprued5b
    • Codec Engine Application Developer User's Guide - sprue67d
  • DVTB User Guide available in DVSDK_Install_Dir/dvtb_vX_YY_ZZ/docs

For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article RTSC Codec And Server Package Wizards here.
Leave a Comment