System Requirements
From Texas Instruments Embedded Processors Wiki
C674x/OMAPL1x Introductory Information > Talk:CE DEBUG > Code Generation Tools FAQ > QualiTI > System Requirements
Contents |
Code Composer Studio v4
Below are the system requirements for Code Composer Studio v4
Hardware Requirements
| Minimum | Recommended | |
| Memory | 1GB | 2GB |
| Disk space | 300MB* | 2GB |
| Processor | 1.5GHz single core | Dual core |
- Disk space listed depends on features selected during installation. Does not include temporary space required by the installer.
- Note that the most important requirement is memory. You really want to have 2GB of memory, it will run with 1GB but it will be slow.
Operating System Requirements
CCSv4 supports XP, Vista and Windows7. The details as to which specific version supports each OS and 32bit/64bit configurations are available on the FAQ_-_CCSv4#Operating_System_Support FAQ.
Code Composer Studio v3
Below are the system requirements for Code Composer Studio v3
Hardware Requirements
| Minimum | Recommended | |
| Memory | 512MB | 2GB |
| Disk space | 300MB* | 1.5GB |
| Processor | 1.5GHz | 2GHz |
- Depends on features selected during installation. Does not include temporary space required by the installer.
Operating System Requirements
Windows 2000
Windows XP
Windows Vista**
- There are some known issues when working with Windows Vista and CCSv3
Leave a Comment