NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

CC3100 & CC3200 Frequency Tuning

From Texas Instruments Wiki
Jump to: navigation, search

Adjusting the center frequency error in SimpleLink WLAN[edit]

Why is it needed[edit]

WLAN standards for 802.11b/g specifies the maximum frequency error to be within 25ppm. Beyond this the device may have difficulty in interoperability with multiple access points. Hence it is important to restrict the frequency error to a small value and ensure that the average frequency error across multiple boards is centered around 0ppm.

The frequency at which a crystal oscillates, depends on the net capacitance load seen between the crystal pins. This capacitance includes the shunt capacitors added on the board , the PCB trace parasitic capacitance , the component pad capacitance, device pin capacitance etc. To achieve the specified frequency from the crystal (eg: 40Mhz) , the net capacitance load should exactly match the specified CL spec of the XTAL. For eg: the “Q24FA20H00396” XTAL speced for Cl of 8pF would resonate at 40Mhz accurately only when the net capacitance between the XTAL P/M pins is accurately 8pF. As the capacitance moves away from 8pF the frequency error changes (a typical plot is shown below indicates the ppm error with variation in Cl).

Frequency error vs Load capacitance

The CC31xx/CC32xx uses the 40Mhz XTAL to derive the RF frequency. Based on the 802.11 IEEE standard the max allowed ppm error in the channel frequency is 25 ppm (for 11b/g/n standards). This ppm error includes the offset frequency error in XTAL, the variation due to temperature and aging (all provided in the XTAL datasheet). Any frequency error caused due to capacitance load error is additional to the errors mentioned in the datasheet of the XTAL and should be minimized.


Adjusting the 40Mhz XTAL shunt caps in CC3x00/CC3x20[edit]

Based on the PCB trace capacitance and the 40 Mhz XTAL part used on final product , the shunt caps on the XTAL may need to be adjusted in order to make sure the net capacitance load on the XTAL is exactly what is required.

Adjust the values as per recommendation from crystal manufacturer. If the crystal specifies a 8pF load capacitor, then each capacitor on the crystal pin = 2x8 = 16pF as the capacitors would be in series. Out of this 16pF, account for 2 to 3pF for the board parasitic. Then the CC31xx/CC32xx device input has 5 to 6pF per pin. This calls for a total added capacitor of 7-9pF on each pin. Fine tune this based on TX output frequency. Never tune the crystal by monitoring the crystal itself. Loading the crystal with a oscilloscope probe will reduce the frequency of oscillation


Procedure to measure the ppm error:[edit]

  • Connect the device using Radio Tool (CC3100/CC3200 Radio Tool shown). Transmit a unmodulated sin wave using TX CW mode. Select the “Tone” as 1.

Radio Tool Gui

  • This would transmit a RF sine wave at Channel frequency + 312.5 Khz. Eg: On CH6 the sine wave would be at 2437.3125 Mhz.
  • Measure the actual frequency on a spectrum analyzer and the delta from the expected frequency gives the frequency error. Eg: if the measured frequency is 2437.3225 Mhz then the frequency error = 2437.3225 – 2437.3125 = 0.01Mhz (10 Khz). For accurate measurement set a low span in the spectrum analyzer , like 100Khz and RBW of 100Hz.
  • To convert this to ppm -> (Freq error/expected frequency) * 10^6 -> (0.01/2437.3125) * 10^6 = 4.1 ppm.
  • Adjust the onboard shunt cap to bring the frequency error to as low value as possible (at 25C). A positive ppm error (larger frequency) indicates you need to increase the cap and negative ppm error indicates you need to decrease the cap. Note that the two shunt caps effectively come is series. For fine adjustments the two capacitors can have different values.
E2e.jpg {{
  1. switchcategory:MultiCore=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article CC3100 & CC3200 Frequency Tuning here.

Keystone=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article CC3100 & CC3200 Frequency Tuning here.

C2000=For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article CC3100 & CC3200 Frequency Tuning here. DaVinci=For technical support on DaVincoplease post your questions on The DaVinci Forum. Please post only comments about the article CC3100 & CC3200 Frequency Tuning here. MSP430=For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article CC3100 & CC3200 Frequency Tuning here. OMAP35x=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article CC3100 & CC3200 Frequency Tuning here. OMAPL1=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article CC3100 & CC3200 Frequency Tuning here. MAVRK=For technical support on MAVRK please post your questions on The MAVRK Toolbox Forum. Please post only comments about the article CC3100 & CC3200 Frequency Tuning here. For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article CC3100 & CC3200 Frequency Tuning here.

}}

Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity