NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

Checking Linux Dependencies for CCSv5

From Texas Instruments Wiki
Jump to: navigation, search

Overview[edit]

When installing CCS v5.4 and v5.5 on Linux, you may find CCS will not install or will not work because not all the required Linux packages have been installed. The script described here provides a way to determine what dependencies are required and check if these dependencies are installed.

The dependency checker is built into the CCSv6.0 and up installer, so you do not need to run it separately.

Checking Dependencies (CCSv5.4 and v5.5)[edit]

To check if you have all the required dependencies, download and unpack the attched TAR file into a local folder. In a terminal window, run the ./check_depends.sh script. The output will look something like this:

Installed versions of glibc and glibcxx: GLIBC_2.15, N/A
Required versions of glibc and glibcxx: GLIBC_2.7, GLIBCXX_3.4.16
Checking availability of libraries in ext-depends.txt ...
Failed to find lib: libhistory.so.4
Failed to find lib: libnotify.so.1
Failed to find lib: libodbcinst.so
Failed to find lib: libodbc.so
Failed to find lib: libreadline.so.4
Done.

The main difference between CCSv5.4 and v5.3 w.r.t. dependencies is v5.4 includes a version of libstdc++ with the install.

Generating the List of Required Dependencies[edit]

The script works by reading a list of dependencies from a text file and checking if these libraries can be loaded. If you have a CCS install for which you want to regenerate this dependency list, you can do this by editing the generate_depends.sh script to point to the CCS install location and then running the script. After the script completes, re-run the check_depends.sh script.

Script Download[edit]

http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/scratchpad/depends_0.2.tar.gz


Searching for and installing missing packages[edit]

Each Linux family has a different way of searching for and installing packages. The list below explains how to do this for particular distibutions. This list is a work in progress and will grow over time. Feel free to add to this list.

(1) Ubuntu

## To search for packages containing libjpeg8
# dpkg -l|grep libjpeg8

ii libjpeg8:amd64       8c-2ubuntu7    amd64 Independent JPEG Group's JPEG runtime library (dependency package)
ii libjpeg8:i386        8c-2ubuntu7    i386  Independent JPEG Group's JPEG runtime library (dependency package)

## Alternatively:
# apt-cache search "libjpeg8"
libjpeg-turbo8 - IJG JPEG compliant runtime library.
libjpeg8 - Independent JPEG Group's JPEG runtime library (dependency package)
libjpeg8-dbg - Independent JPEG Group's JPEG runtime library (dependency package)
libjpeg8-dev - Independent JPEG Group's JPEG runtime library (dependency package)

## We want libjpeg8:i386, IE the 32-bit version of libjpeg8. To install it
# apt-get install libjpeg8:i386



Change log:

Apr 17/2013: (v0.1) First version

Apr 25/2013: (v0.2) Add an exclusion list so libraries that are not actually used don't appear as requirements.

E2e.jpg {{
  1. switchcategory:MultiCore=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article Checking Linux Dependencies for CCSv5 here.

Keystone=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article Checking Linux Dependencies for CCSv5 here.

C2000=For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article Checking Linux Dependencies for CCSv5 here. DaVinci=For technical support on DaVincoplease post your questions on The DaVinci Forum. Please post only comments about the article Checking Linux Dependencies for CCSv5 here. MSP430=For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article Checking Linux Dependencies for CCSv5 here. OMAP35x=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article Checking Linux Dependencies for CCSv5 here. OMAPL1=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article Checking Linux Dependencies for CCSv5 here. MAVRK=For technical support on MAVRK please post your questions on The MAVRK Toolbox Forum. Please post only comments about the article Checking Linux Dependencies for CCSv5 here. For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Checking Linux Dependencies for CCSv5 here.

}}

Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity