NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

IPC Users Guide/List Module

From Texas Instruments Wiki
Jump to: navigation, search
{{#switchcategory:MSP430=<McuHitboxHeader/>|C2000=<McuHitboxHeader/>|Stellaris=<McuHitboxHeader/>|TMS570=<McuHitboxHeader/>|MCU=<McuHitboxHeader/>|MAVRK=<MAVRKHitboxHeader/>|<HitboxHeader/>}}


Table of Contents IPC User's Guide Previous; The ti.sdo.utils Package MultiProc Module Next


API Reference
Links
Book config.png
Book run.png

The ti.sdo.utils.List module provides support for creating lists of objects. A List is implemented as a doubly-linked list, so that elements can be inserted or removed from anywhere in the list. Lists do not have a maximum size.

NOTE

List module use is the same for Concerto F28M35x devices as for other devices.

Basic FIFO Operation of a List[edit]

To add a structure to a List, its first field needs to be of type List_Elem. The following example shows a structure that can be added to a List. A List has a "head", which is the front of the list. List_put() adds elements to the back of the list, and List_get() removes and returns the element at the head of the list. Together, these functions support a FIFO queue.

Run-time example: The following example demonstrates the basic List operations--List_put() and List_get().

<syntaxhighlight lang='c'>/* This structure can be added to a List because the first

* field is a List_Elem. Declared globally. */

typedef struct Rec {

   List_Elem elem;
   Int data;

} Rec;

...

List_Handle myList; /* in main() */ Rec r1, r2; Rec* rp;

r1.data = 100; r2.data = 200;

/* No parameters are needed to create a List. */ myList = List_create(NULL, NULL);

/* Add r1 and r2 to the back of myList. */ List_put(myList, &(r1.elem)); List_put(myList, &(r2.elem));

/* get the records and print their data */ while ((rp = List_get(myList)) != NULL) {

   System_printf("rec: %d\n", rp->data);

} </syntaxhighlight>The example prints the following:

<syntaxhighlight lang='c'>rec: 100 rec: 200 </syntaxhighlight>

Iterating Over a List[edit]

The List module also provides several APIs for looping over a List.

List_next() with NULL returns the element at the front of the List (without removing it). List_next() with an elem returns the next elem. NULL is returned when the end of the List is reached.

Similarly, List_prev() with NULL returns the tail. List_prev() with an elem returns the previous elem. NULL is returned when the beginning of the List is reached.

Run-time example: The following example demonstrates one way to iterate over a List once from beginning to end. In this example, "myList" is a List_Handle.

<syntaxhighlight lang='c'>List_Elem *elem = NULL; Rec* rp;

...

/* To start the search at the beginning of the List */ rp = NULL;

/* Begin protection against modification of the List */ key = Gate_enterSystem();

while ((elem = List_next(myList, elem)) != NULL) {

    System_printf("rec: %d\n", rp->data);

} /* End protection against modification of the List */ Gate_leaveSystem(key); </syntaxhighlight>

Inserting and Removing List Elements[edit]

Elements can also be inserted or removed from anywhere in the middle of a List using List_insert() and List_remove(). List_insert() inserts an element in front of the specified element. Use List_putHead() to place an element at the front of the List and List_put() to place an element at the end of the List.

List_remove() removes the specified element from whatever List it is in.

Note that List does not provide any APIs for inserting or removing elements at a given index in the List.

Run-time example: The following example demonstrates List_insert() and List_remove():

<syntaxhighlight lang='c'>/* Insert r2 in front of r1 in the List. */ List_insert(myList, &(r1.elem), &(r2.elem));

/* Remove r1 from the List. */ List_remove(myList, &(r1.elem)); </syntaxhighlight>Run-time example: The following example treats the List as a LIFO stack using List_putHead() and List_get():

<syntaxhighlight lang='c'>List_Elem elem[NUMELEM]; List_Elem *tmpElem;

// push onto the top (i.e. head) for (i = 0; i < NUMELEM; i++) {

   List_putHead(listHandle, &(elem[i]));

}

// remove the buffers in FIFO order. while((tmpElem = List_get(listHandle)) != NULL) {

   // process tmpElem

} </syntaxhighlight>

Atomic List Operations[edit]

Lists are commonly shared across multiple threads in the system, which might lead to concurrent modifications of the List by different threads, which would corrupt the List. List provides several "atomic" APIs that disable interrupts before operating on the List. These APIs are List_get() List_put(), List_putHead(), and List_empty().

An atomic API completes in core functionality without being interrupted. Therefore, atomic APIs are thread-safe. An example is List_put(). Multiple threads can call this API at the same time. The threads do not have to manage the synchronization.

Other APIs--List_prev(), List_next(), List_insert(), and List_remove()--should be protected by the application.


Table of Contents IPC User's Guide Previous; The ti.sdo.utils Package MultiProc Module Next



E2e.jpg {{
  1. switchcategory:MultiCore=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article IPC Users Guide/List Module here.

Keystone=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article IPC Users Guide/List Module here.

C2000=For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article IPC Users Guide/List Module here. DaVinci=For technical support on DaVincoplease post your questions on The DaVinci Forum. Please post only comments about the article IPC Users Guide/List Module here. MSP430=For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article IPC Users Guide/List Module here. OMAP35x=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article IPC Users Guide/List Module here. OMAPL1=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article IPC Users Guide/List Module here. MAVRK=For technical support on MAVRK please post your questions on The MAVRK Toolbox Forum. Please post only comments about the article IPC Users Guide/List Module here. For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article IPC Users Guide/List Module here.

}}

Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity

{{#switchcategory:MSP430=<McuHitboxFooter/>|C2000=<McuHitboxFooter/>|Stellaris=<McuHitboxFooter/>|TMS570=<McuHitboxFooter/>|MCU=<McuHitboxFooter/>|MAVRK=<MAVRKHitboxFooter/>|<HitboxFooter/>}}