NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

IPC Users Guide/NameServer Module

From Texas Instruments Wiki
Jump to: navigation, search
{{#switchcategory:MSP430=<McuHitboxHeader/>|C2000=<McuHitboxHeader/>|Stellaris=<McuHitboxHeader/>|TMS570=<McuHitboxHeader/>|MCU=<McuHitboxHeader/>|MAVRK=<MAVRKHitboxHeader/>|<HitboxHeader/>}}


Table of Contents IPC User's Guide Previous; MultiProc Module Porting IPC Next


API Reference
Links
Book config.png
Book run.png

The NameServer module manages local name/value pairs. This enables an application and other modules to store and retrieve values based on a name.

The NameServer module maintains thread-safety for its APIs. However, NameServer APIs cannot be called from an interrupt (that is, Hwi context). They can be called from Swis (BIOS-only) and Tasks.

This module supports different lengths of values. The NameServer_add() and NameServer_get() functions support variable-length values. The NameServer_addUInt32() function is optimized for UInt32 variables and constants.

The NameServer module currently does not perform any endian or word size conversion. Also there is no asynchronous support at this time.

You can create NameServer instances dynamically. On BIOS, you can also create NameServer instances statically.

Creating NameServer Instances Statically (BIOS-only)[edit]

To create a NameServer instance statically, you can add statements similar to the following to your XDCtools configuration script:

<syntaxhighlight lang='javascript'> var NameServer = xdc.useModule('ti.sdo.utils.NameServer');

var nameServerParams = new NameServer.Params; nameServerParams.maxRuntimeEntries = 10; nameServerParams.maxNameLen = 32; var nameServer0 = NameServer.create("nameServer0", nameServerParams); </syntaxhighlight>

If you want to specify the heap to be used by the NameServer module and a NameServer instance, use configuration statements similar to the following:

<syntaxhighlight lang='javascript'> var NameServer = xdc.useModule('ti.sdo.utils.NameServer'); var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');

var heapParams = new HeapMem.Params; heapParams.size = 1024; var heapMem = HeapMem.create(heapParams);

var nameServerParams = new NameServer.Params; nameServerParams.tableHeap = heapMem; var nameServer = NameServer.create("staticNameServer", nameServerParams); </syntaxhighlight>

To create a NameServer instance dynamically, initialize a NameServer_Params structure with NameServer_Params_init() and customize the values as needed. The parameters include the following:

  • checkExisting. If true, NameServer check to see if a name already exists in the name/value table before adding it.
  • maxNameLen. Specify the maximum length, in characters, of the name field in the table.
  • maxRuntimeEntries. Specify the maximum number of name/value pairs this table can hold. If you set this parameter to NameServer_ALLOWGROWTH, then NameServer allows dynamic growth of the table.
  • maxValueLen. Specify the maximum length, in MAUs, of the value field in the table.
  • tableHeap. The heap to allocate the name/value table from when allocating dynamically. If this parameter is NULL, the heap used for object allocation is also used here.

After setting parameters, use NameServer_create() to create an instance. Each NameServer instance manages its own name/value table.

Book config.png

The latest version of the NameServer module configuration documentation is available online.

Creating and Removing NameServer Instances Dynamically[edit]

The following C example creates a NameServer instance dynamically. The instance allows a maximum of 10 runtime entries (instead of using ALLOWGROWTH). This example also specifies where to allocate the memory needed for the tables (instead of using the default).

<syntaxhighlight lang='c'>NameServer_Handle NSHandle; NameServer_Params params;

NameServer_Params_init(&params); params.tableHeap = HeapStd_Handle_upCast(myHeap); params.maxRuntimeEntries = 10; NSHandle = NameServer_create("myTable", &params); if (NSHandle == NULL) {

   // manage error

} </syntaxhighlight>

This example C code adds and removes entries at run-time:

<syntaxhighlight lang='c'> Ptr key;

key = NameServer_addUInt32(NSHandle, "volume", 5); if (key == NULL) {

   // manage error

}

NameServer_removeEntry(NSHandle, key); // or NameServer_remove(NSHandle, "volume"); </syntaxhighlight>

Book run.png

The latest version of the NameServer module run-time API documentation is available online.

Searching NameServer Instances[edit]

The following example searches the NameServer instance pointed to by "handle" on the specified processor for a name-value pair with the name stored in nameToFind. It returns the value of the pair to valueBuf.

<syntaxhighlight lang='c'> /* Search NameServer */ status = NameServer_get(NSHandle, nameToFind, valueBuf, sizeof(UInt32), procId); </syntaxhighlight> Using different parameters for different table instances allows you to meet requirements like the following:

  • Size differences. The maxValueLen parameter specifies the maximum length, in MAUs, of the value field in the table. One table could allow long values (for example, > 32 bits), while another table could be used to store integers. This customization enables better memory usage.
  • Performance. Multiple NameServer tables can improve the search time when retrieving a name/value pair.
  • Relax name uniqueness. Names in a specific table must be unique, but the same name can be used in different tables.

When you call NameServer_delete(), the memory for the name/values pairs is freed. You do not need to call NameServer_remove() on the entries before deleting a NameServer instance.

Other NameServer APIs[edit]

In addition to the functions mentioned above, the NameServer module provides the following APIs:

  • NameServer_get() Retrieves the value portion of a local name/value pair from the specified processor.
  • NameServer_getLocal() Retrieves the value portion of a local name/value pair.
  • NameServer_remove() Removes a name/value pair from the table given a name.
  • NameServer_removeEntry() Removes an entry from the table given a pointer to an entry.

NameServer maintains the name/values table in local memory, not in shared memory. However the NameServer module can be used in a multiprocessor system. The module communicates with other processors via NameServer Remote drivers, which are implementations of the INameServerRemote interface. The communication to the other processors is dependent on the Remote drivers implementation. When a remote driver is created, it registers with NameServer via the NameServer_registerRemoteDriver() API.

The NameServer module uses the MultiProc module to identify different processors. Which remote processors to query and the order in which they are queried is determined by the procId array passed to the NameServer_get() function.


Table of Contents IPC User's Guide Previous; MultiProc Module Porting IPC Next



E2e.jpg {{
  1. switchcategory:MultiCore=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article IPC Users Guide/NameServer Module here.

Keystone=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article IPC Users Guide/NameServer Module here.

C2000=For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article IPC Users Guide/NameServer Module here. DaVinci=For technical support on DaVincoplease post your questions on The DaVinci Forum. Please post only comments about the article IPC Users Guide/NameServer Module here. MSP430=For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article IPC Users Guide/NameServer Module here. OMAP35x=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article IPC Users Guide/NameServer Module here. OMAPL1=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article IPC Users Guide/NameServer Module here. MAVRK=For technical support on MAVRK please post your questions on The MAVRK Toolbox Forum. Please post only comments about the article IPC Users Guide/NameServer Module here. For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article IPC Users Guide/NameServer Module here.

}}

Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity

{{#switchcategory:MSP430=<McuHitboxFooter/>|C2000=<McuHitboxFooter/>|Stellaris=<McuHitboxFooter/>|TMS570=<McuHitboxFooter/>|MCU=<McuHitboxFooter/>|MAVRK=<MAVRKHitboxFooter/>|<HitboxFooter/>}}