Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Invicta Pro-Diver Quartz Chronograph Silver Dial 0071 Men s Watch

From Texas Instruments Wiki
Jump to: navigation, search

Amidst a plethora of popular, classic dive watches, Invicta procured a safe position for itself just because it delivers professional standard utility without costing like the Rolex Submariner or the Omega Seamaster. They are an affordable option for real use and are welcomed by sensible watch lovers who don't have thousands of dollars to risk.

Invicta, just as it name means, is an invincible watch provided you don't land it under several thousand pounds of rock. They have been made that way since their first day; the Swiss art of watch making makes itself evident from every aspect in the Invicta. Quality, design and materials - all come together to give the Invicta Excursion Reserve Chronograph Silver Dial 0071 an uncompromising bold stature.

This particular Invicta is not only a jewel that's worthy of the deep seas but also a piece that gets into easily several stylistic scenarios. Richly complemented by a high polish, painstakingly carved details and top-end solidity, it's an assortment of functionality and aesthetics that sends an invite to plunge into the unprecedented deep excursions - in the water or out in the world - without worrying about damaging it under extreme conditions.

The Invicta Russian Diver Silver Dial 0071 is an all-round watch that's not just good for the waters but also for the fashion domains. It's a design to last for decades and give you the freedom to wear any kind of outfit that you may like. Its classy bracelet links in alternative brushed and shining polish and deeply grooved-in, spreading-outward crown makes it fir for some very dressy situations while its bold, sporty look makes it fit the playgrounds with ease. The sturdily built quartz movement also keeps parity with the precision and its external toughness; it has been made to withstand more than a few hard knocks and bumps. If you have an eye for the oversized trend, it will suit your needs in an awesome way. But lovers of moderate sized watches will also like it because of its elegant, classic details and its smooth transition from the case to the band. Together with the luminous hands and markers, which are rather larger than the usual ones, it makes for a good visibility when in the dark.

To end, the Invicta Lupah Quartz Chronograph Silver Dial 0071 is a good option to them who are looking for a more than modest dive watch that also serves their fashion purposes. As much suitable for the desk-diver, it is a good choice for recreational water sports enthusiasts who are not ready to invest heavily on a timepiece that they want to put to use. A great value at a very modest price, its remarkable construction and a reliable quartz movement is all about showcasing some good judgement.

We are a well-established online retailer of watches with customers from all around the world. Being a trusted dealer of Citizen, Seiko, Casio, Tissot and www.fmconsulting.net Polar brands of watches, all our watches are 100% genuine and brand new. Click Here For More Information : Invicta Excursion Reserve