Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Invicta Quartz Chronograph 17887 Men Watch Dress Chrono Meant For Real Life Adventures

From Texas Instruments Wiki
Jump to: navigation, search

What's likeable 'bout it?

Very few watches can get colorful and yet retain the seriousness within a sporty parameter. The Invicta Quartz Men's Watch does just that and becomes an important component of any watch collection comprising all-time-wear sporty timepieces.

Prime USP:

A fluid and fast design gives the Invicta Quartz Men's Watch a cheerful, peppy appeal that takes out the stress factor from all demanding assignments. The bold colors make it come alive and with any dressing style you choose.

A short description:

Easy to read, operate and www.mixcloud.com maintain, the Invicta Quartz Men's Watch brings back the focus and life throws you off-balance. The refreshing, intricate design owes to an intelligent layout of the sub-dials, which adds a certain amount of boldness to the watch face. The blue accents keep things both soothing and upbeat, while the unidirectional bezel approves of its full diving utility. Sitting within the bezel is a synthetic-sapphire dial window with a magnified section for an easy viewing of the date, while the markers and the main three hands offer a flawless view under low and no light condition due to the Tritnite lume applied all over them. The 48mm diameter case is made from surgical grade, 316L stainless steel case with 18kt gold-plating.

The Invicta Watch is run by an ISA 6371C Swiss Quartz movement, which ensures its accurate, fail-proof timekeeping. The 3'o clock sub-dial shows the regular advancements of seconds while the 9'o clock sub-dial functions as the minute totalizer for the chronograph. The 6'o clock sub-dial records the elapsed hours for 12 hours.

The polyurethane strap with metal inserts adds to its durability and provides firm yet comfortable grip even when wet. It is large enough to fit wrist sizes up to 9 inches and a half. The 600 feet of water resistant makes the watch fit for quite few professional marine activities and every surface water sports.

Who should go for it?

Anyone who wants a good diving watch without bothering about it getting broken or stolen should give the Invicta Quartz Men's Watch a thought. It allows you to take plunges without the fear of ruining your timepiece; it's stylish, classic and exhibits a good amount of confident prowess. Thanks to its heavy and solid feel; it makes the whole unit very impressive to wear and hold. Take it to the club, to a game of tennis or to the water park, the Invicta Quartz Chronograph Men's Watch makes for a fine companion to any place that requires putting in quite a bit of muscle.

CreationWatches.sg is Singapore's premier ecommerce store for Wrist Watches. We source our watches in bulk from suppliers around the world, and that allows us to get great deals and keep the prices low. We offer FREE Ta-Q-Bin courier delivery on all domestic orders.
Click Here For More Information : Invicta Quartz Chronograph Men's Watch And Invicta Watch