NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

Processor SDK Linux Training: Hands on with the Linux SDK

From Texas Instruments Wiki
Jump to: navigation, search
{{#switchcategory:MSP430=<McuHitboxHeader/>|C2000=<McuHitboxHeader/>|Stellaris=<McuHitboxHeader/>|TMS570=<McuHitboxHeader/>|MCU=<McuHitboxHeader/>|MAVRK=<MAVRKHitboxHeader/>|<HitboxHeader/>}}

TIBanner.png

Introduction


This lab is going to give you a hands on tutorial of the Processor Linux SDK. Each of the following sections below will walk you through a particular part of the SDK describing the actions that are about to be performed, the key points to take away, and the step-by-step instructions to complete the lab. If you have questions or feedback please e-mail the sdk_feedback@list.ti.com mailing list.

NOTE: In this guide commands to be executed for each step will be marked in BOLD

Lab Configuration[edit]

The following are the hardware and software configurations for this lab. The steps in this lab are written against this configuration. The concepts of the lab will apply to other configurations but will need to be adapted accordingly.

Hardware[edit]

NOTE

This lab has also been validated with the AM437x EVM-SK (TMDXSK437X) and AM572x EVM (TMDXEVM5728). Other target boards can be used, but the steps below related to serial and ethernet connections may differ.
  • Router connecting AM335x EVM-SK and Linux Host (For Remote Matrix lab)
  • USB cable connection between AM335x EVM-SK and Linux Host using the micro-USB connector (J3/USB0) for serial communication
  • 5V power supply (12V power supply required for use with AM57x EVM)

Software[edit]

  • A Linux host PC. For more information, see the Processor SDK Linux Getting Started Guide.
  • Processor Linux SDK installed. This lab assumes the latest Processor Linux SDK is installed in /home/sitara. If you use a different location please modify the below steps accordingly. For more information, see the Processor SDK Linux Installer.
  • SD card with Processor Linux SDK installed.
  • CCSv6 installed. This lab assumes CCS has been installed in /home/sitara. If you use a different location please modify the below steps accordingly.
    • The CCS installer can be downloaded from the SDK for Sitara Processors page. If extracted into the same directory as the SDK installer then the SDK installer can take care of installing CCS as well.


Out-Of-Box Experience[edit]

Description[edit]

This section will cover the steps to boot the target board and how to use the Matrix application launcher, which is the default application run when the board is booted.

Key Points[edit]

  • How to boot the target board
  • Navigating Matrix using the touchscreen
  • Navigating Matrix using the remote interface

Lab Steps[edit]

  1. Connect the cables to the EVM. For details on where to connect these cables see the Quick Start Guide that came with your EVM.
    1. Connect the USB cable between your Linux host and the mini-USB connector of the EVM.
      NOTE

      This will provide the serial connection. For other boards you may need to use a different cable such as a straight serial cable.
    2. Connect the network cable.
      NOTE

      To ensure you receive a valid ipaddr when using the AM335x EVM-SK, be sure to connect the ethernet cable to the port closest to the User Push Buttons.
    3. Insert the SD card with Processor Linux SDK installed into the SD connector. For more information, see Processor SDK Linux create SD card script.
    4. Insert the power cable into the 5V power jack.
  2. Power on the AM335x EVM-SK. For power button position, consult your Quick Start Guide. Allow the boot process to finish. You will know when the boot process has finished when you see the Matrix application launcher on the LCD screen.
    NOTE

    You may be required to calibrate the touchscreen. If so follow the on screen instructions to calibrate the touchscreen.
    Sitara-linux-training-matrix-main-menu.png
  3. Navigate Matrix using the touchscreen.
    • The icons on the screen will either launch an application or will display a submenu of applications to launch. To select an item just touch the icon on the screen. Touch the ARM icon to open the ARM submenu and display the applications available within that menu.
      Sitara-linux-training-matrix-arm-menu.png
    • Whenever you enter a submenu or the description screen of an application (if that application has a description screen) you will see two additional icons appear.
      • The "Up Arrow" Icon (highlighted in green) will return you to the previous screen. This is equivalent to a Back functionality. Touch the Up Arrow to be returned to the main matrix menu and then select ARM again to come back to the ARM submenu.
      Sitara-linux-training-matrix-up-arrow.png
      • The "Multi" Icon (Highlighted in green) will return you to the Matrix main menu. This is equivalent to a Home functionality.
      Sitara-linux-training-matrix-multi-icon.png
    • To run an application touch the application's icon. If the application has a description screen, you will be shown the description and given a Run button (highlighted in green). If the application does not have a description touching the application's icon will start execution of that application. Touch the Dhrystone application to see the Dhrystone application description screen then touch the RUN button to launch the application.
      Sitara-linux-training-dhrystone-screen.png
    • When Dhrystone finishes running you can review the output on the LCD. Touch the Multi Icon to return to the Matrix main menu.
    • Where there are more applications available in Matrix than can be displayed on the screen you will see arrows appear in the upper-right and upper-left corners. Touching these arrows will switch pages to the next page. Touch the Right arrow to see the next page of applications.
      Sitara-linux-training-right-arrow.png
    • To return to the previous page touch the left arrow.
      Sitara-linux-training-left-arrow.png
  4. Navigating Matrix using the remote interface is similar to navigating Matrix with the touchscreen.
    • IMPORTANT

      Do NOT use your browser's back or home buttons as this will navigate you away from the Matrix page.
      NOTE

      Refreshing the page will restart your connection with Matrix.
    • In order to connect to the remote Matrix interface, you will need to know the IP address of your EVM. To find this perform the following actions in Matrix.
      IMPORTANT

      On the AM335x EVM-SK, please insure the ethernet cable is plugged into the port closest to the user push buttons. Otherwise you will not receive a valid ipaddr for the board.
      • Touch the Settings icon from the Matrix main menu.
      • Touch the Network Settings icon from the Settings Submenu.
      • You should see output like the following. The EVM IP address has been highlighted in green.
      Sitara-linux-training-ipaddr.png
    • To connect to Matrix you should enter the EVM IP address obtained in the previous step into your browser's address bar. You can launch a browser in your Linux host by clicking the firefox icon highlighted in the image below.
      Sitara-linux-training-remote-matrix.jpeg
    • You should be prompted to select whether your EVM has a display device attached. Since the LCD is attached to the EVM select OK.
    • The reason this question is asked is because Matrix does not support shipping graphical data over the remote interface. Applications which are graphical such as the 3D demos will need to be viewed on the LCD attached to the board. An answer of no (pressing Cancel) will prevent graphical applications from being launched from remote Matrix.
      NOTE

      You can change your selection at any time by pressing the Refresh button on your browser to re-connect to Matrix.
      Sitara-linux-training-remote-matrix-gui-select.png
  5. When you are finished exploring remote Matrix close the browser.



Using the Built-in GCC Toolchain[edit]

Description[edit]

This section will walk you through the location of the built-in GCC toolchain found in the SDK. You will also learn how and when to use the environment-setup script to configure your environment to use this toolchain. Additional information on using this toolchain can be found at Processor Linux SDK GCC Toolchain.

Key Points[edit]

  • The cross-compiler is now located within the SDK in the linux-devkit directory
  • There are many libraries pre-built for the ARM core available in the linux-devkit directory as well
  • Sourcing the environment-setup script configures you system to use this cross-compiler and pre-built libraries
  • How to identify when the environment-setup script has been sources
  • How example applications use the environment-setup script

Lab Steps[edit]

  1. Open a terminal window by clicking on the Terminal icon on the Launcher toolbar.
  2. The cross-compiler is located in the linux-devkit/sysroots/<Arago Linux>/usr/bin directory of the SDK installation directory. In the terminal window enter the following commands, replacing the <machine>, <version>, and <Arago Linux> fields with the target machine you are using and the SDK version installed. The <Arago Linux> version may be x86_64-arago-linux.
    NOTE

    You can use TAB completion to help with this.
    cd /home/sitara/ti-processor-sdk-linux-<machine>-<version>/linux-devkit/sysroots/<Arago Linux>/usr/bin
    ls
  3. You should see a listing of the cross-compile tools available like the one below.
    Linux-SDK-training-cross-tools.png
  4. To locate the pre-built ARM libraries perform the following commands:
    cd /home/sitara/ti-processor-sdk-linux-<machine>-<version>/linux-devkit/sysroots/<Arago Linux>/usr/lib
    ls
    You should now see a listing of all the libraries (some are contained within their individual sub-directories) available as pre-built packages within the SDK.
  5. In order to make it easier to perform cross-compilations and ensure linking with the proper cross-compiled libraries instead of the host system libraries the environment-setup script has been created in the linux-devkit directory. This script will configure many standard variables such as CC to use the cross-compile toolchain, as well as adding the toolchain to your PATH and configuring paths for library locations. To utilize the setting provided by the environment-setup script you will need to source the script. Perform the following commands to source the environment-setup script and observe the change in the CC variable:
    echo $CC
    cd /home/sitara/ti-processor-sdk-linux-<machine>-<version>/linux-devkit
    source environment-setup
    echo $CC
    You should have observed that the CC variable now contains the value of arm-linux-gnueabihf-gcc after the sourcing of the environment-setup script. There was also another change that occurred which was that your standard prompt changed from sitara@ubuntu to [linux-devkit]. The purpose of this change is to make it easy to identify when the environment-setup script has been sourced. This is important because there are times when you DO NOT want to source the environment-setup script. A perfect example is when building the Linux kernel. During the kernel build there are some applications that get compiled which are meant to be run on the host to assist in the kernel build process. If the environment-setup script has been sourced then the standard CC variable will cause these applications to be built for the ARM, which in turn will cause them to fail to execute on the x86 host system.
  6. As mentioned above sometimes it is not appropriate to source the environment-setup script, or you only want to source it during a particular build but not affect your default environment. The way this is done in the SDK is to source the environment-setup script inside of the project Makefile so that it is used only during the build process. To see this perform the following actions:
    • Close the open terminal since it already has the environment-setup script sourced.
    • Open a new terminal
    cd /home/sitara/ti-processor-sdk-linux-<machine>-<version>/example-applications/matrix-gui-browser-2.0
    gedit Makefile.build
    In the Makefile.build file you can see that we set a variable called ENV_SETUP which points to the environment-setup script. In the qmake build target we perform the action "@. ${ENV_SETUP}". That line uses the "@" symbol, which in make says to execute a shell command, and the "." notation, which is another way of sourcing a file, to source the environment-setup script prior to calling the qmake2 command.
  7. To see this work use the following commands to cross-compile the matrix-gui-browser project:
    • Close the gedit window if you have not already done so.
    make -f Makefile.build
    Notice in the output that the arm-linux-gnueabihf-g++ compiler was called during the build. Also notice that your prompt still shows sitara@ubuntu which means that while the environment-setup script was sourced for the build, the effects disappeared after the make was finished.
    NOTE

    If you see a "Nothing to be done for..." output, it means you have previously built this file with a make command. Run the command make clean first to see the noted output.
  8. To verify that the matrix_browser executable that was built was in fact cross-compiled we can use the following command:
    file matrix_browser
    You should see output similar to the following which shows that this program was compiled for ARM.
    matrix_browser: ELF 32-bit LSB executable, ARM, version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.32, not stripped

Using the Top-level Makefile[edit]

Description[edit]

This section will cover the top-level Makefile found within the root of the Processor Linux SDK. We will discuss how it is used, key variables, and then build some targets. You can find more information at Processor Linux SDK Top-Level Makefile.

Key Points[edit]

  • Location of top-level Makefile
  • Additional settings in Rules.make file
  • Determining the available build targets
  • Building an individual target

Lab Steps[edit]

  1. If you do not already have a terminal window open, then open one and change directory to the root of the Processor Linux SDK.
    cd /home/sitara/ti-processor-sdk-linux-<machine>-<version>
  2. The top-level Makefile is located in the root of the SDK along with a complementary file called Rules.make. The Rules.make file provides variables and settings used by the top-level Makefile as well as the individual project Makefiles. Open the Rules.make file using the following command:
    gedit Rules.make
    Inside of the Rules.make file, you will find variables that describe the target system such as PLATFORM and ARCH. You will also find variables that point to the root of the SDK install, the location of the linux-devkit directory, and the cross-compiler.
  3. Close the gedit session and open a new gedit session for the Makefile.
    gedit Makefile
  4. The important items to notice in this window are:
    • This Makefile includes the Rules.make file with the "-include Rules.make" line.
    • The all target shows the individual make targets that you can call to build individual components instead of always building everything.
  5. How to build an individual component perform the following commands to only build the u-boot and SPL bootloaders.
    • Close the gedit window if you have not already done so.
    make u-boot-spl
    NOTE

    We do not build all of the targets in this lab due to time constraints, but you could also just type make to build all of the components.



Understanding the board-support Directory[edit]

Description[edit]

This section will teach you about the key components of the board-support directory within the Processor Linux SDK.

Key Points[edit]

  • Pre-built images are available which have been validated with the SDK
  • Linux kernel ships with a configuration file matching the configuration used for the SDK
  • There is no longer an x-loader program, instead MLO comes from u-boot
  • Additional drivers are located in the extra-drivers directory

Lab Steps[edit]

  1. If you do not already have a terminal open then open a Linux terminal.
  2. Change directory to the board-support directory.
    cd /home/sitara/ti-processor-sdk-linux-<machine>-<version>/board-support
  3. List the contents of the directory.
    ls
    Linux-SDK-training-board-support.png
  4. List the contents of the prebuilt-images directory.
    ls prebuilt-images
    Linux-SDK-training-prebuilt.png
    These images have been pre-compiled and tested to work on the target device. They represent a known good starting point.
  5. When building a Linux system it is often helpful to start with a kernel configuration that is known to be working, and then add and remove pieces to optimize the system. In the Processor Linux SDK, we provide the kernel configuration that was used to build the pre-built kernel image inside of the prebuilt-images directory. This configuration can be seen using the command below (replacing the version with the actual kernel version).
    ls linux-<kernel version>/arch/arm/configs/tisdk_*
    You should see a file with the format tisdk_<machine>_defconfig. You can use this configuration as the base configuration for your own kernel builds.
  6. In the latest SDKs there is no longer a separate code base to generate the MLO bootloader. Instead this bootloader is now part of the u-boot code base and is generated using the second program loader (SPL) functionality of u-boot. In the previous Lab you compiled u-boot using the make u-boot command. If you look at the contents of the u-boot directory using the command below you will notice that there exists both the MLO file as well as the u-boot.img file. These were both built during the u-boot build operation.
    ls u-boot-<version>
    Linux-SDK-training-uboot.png
    In the above image the MLO and u-boot.img files were highlighted. Both of these files were created during the single u-boot build operation. The benefit is that you are now able to share the same u-boot code to build a initial boot loader as well as to build the full featured u-boot boot loader.
  7. For devices with out of tree modules those device drivers are located in the extra-drivers directory. This is done to group items that require rebuilding when the kernel configuration changes into a single directory, the board-support directory. You can see the out of tree drivers using the command below:
    ls extra-drivers


Preparing to Develop using the setup.sh Script[edit]

Description[edit]

This section will cover how to use the setup.sh script inside of the Processor Linux SDK to configure your board for development with TFTP and NFS. Due to time limitations some operations will be skipped since they will have already been done for you. These operations that have been done already will be called out in the section below. For more information see Processor SDK Linux Setup Script.

Key Points[edit]

  • Installation of required software to setup development environment
  • Creation of NFS file shares
  • Setup of TFTP for kernel transfers
  • Configuring the EVM using minicom scripts

Lab Steps[edit]

The following steps will help you validate that you have a valid serial connection with your target board.

IMPORTANT

These steps are written for boards like the EVM-SK and Beaglebone which use an FTDI USB-to-Serial adapter. For boards with a straight UART connection you can ignore the steps for /dev/ttyUSBx and instead just use the serial port on your Linux host that is connected to the board.
  1. Connect the USB cable between your Linux host and your target board
    IMPORTANT

    On the AM335x EVM-SK, the USB cable enables a USB-to-serial interface to the Linux host PC. If using a virtual machine, please ensure the AM335x EVM-SK is a selected USB device.

    If you are running your VMWare image with Windows 7, some USB-to-Serial adapters do not properly work with Windows 7. Make sure that your adapter specifically says that it supports Windows 7. You may also need to install an additional driver for your adapter.
  2. Open a terminal and run the following command to find the USB serial adapters available on the system. The FTDI chip used on the board presents two serial interfaces to the Linux host. The first interface is the JTAG interface and the second one is the serial console interface.
    ls /dev/ttyUSB*
    You should see output like:
    /dev/ttyUSB0
    /dev/ttyUSB1
    NOTE

    If using VMWare, you may need to pass the "Future Technology Devices" device into the VMWare image
  3. Since the board's serial interface is the second interface, you will want to open a serial console to the second device node. In this case that is /dev/ttyUSB1. This can be done by doing:
    minicom -w -s
    Select Serial port setup and press ENTER
    Press A to modify the Serial Device and change the device to /dev/ttyUSB1. Press ENTER
    Press ENTER to exit the serial setup
    Select Exit and press ENTER
  4. You should now see a minicom window.
  5. Power on the board. Depending on your board, you may see a boot sequence or simply a "ccccc" being printed in the minicom window. This means the serial connection is working as expected. You may leave this console RUNNING in the background.
    NOTE

    For the Beaglebone the board will power on as soon as the USB cable is connected. You can reset the board by pressing the reset button which should provide you with the expected output.
  6. If you have not already done so, close any open minicom windows using CTRL+A then Z, then press X and select Yes to leave the minicom.
  7. In a terminal window execute the following commands:
    cd /home/sitara/ti-processor-sdk-linux-<machine>-<version>
    ./setup.sh
    • You will be warned that this script requires administrator priveledges (sudo access) to run. This is required to allow installation of packages and system configuration for NFS and TFTP
      • Press ENTER to continue
    • If you are prompted for the [sudo] password for sitara: then use password sitara. If you have a different user account, use that user account password.
      NOTE

      You will see the system attempt to update the host software. This step has already been done for you so that access to an internet connection is not required. You can review the list to see which host packages which were previously installed using setup.sh.
    • You will now be prompted for the directory to install the target file system. The default should look like /home/sitara/ti-processor-sdk-linux-<machine>-<version>/targetNFS.
      • Press ENTER to take this default.
      • Press ENTER when warned that sudo permissions are required.
    • To save extraction time for the root file system the file system may have already been extracted for you. In this case you will be asked if you was to rename the existing file system, overwrite the file system, or skip the file system extraction.
      • Select s and press ENTER to skip the extraction since the file system has been extracted already.
    • Next the setup script will inform you that a default path for binary installation has been configured in the Rules.make file.
      • Press ENTER to continue.
    • You will now be warned that sudo access is required to add the NFS file system that was just created to the /etc/exports file. This is so it can be used as a root file system for the target device to boot over NFS.
      • Press ENTER.
    • You will see the system stop and then start the NFS server to that the file system is exported.
    • You will now be prompted about which directory to make your TFTP root directory.
      • Press ENTER to take the default of /tftpboot
    • You will be warned that sudo access is required to configure the TFTP server.
      • Press ENTER.
    • You will be told that the uImage file already exists. This was pre-copied to save time.
      • Press s to skip copying this image again.
    • You will see the system setup stop and start the xinetd (TFTP server).
    • You will now be prompted to enter the serial port for the board so that minicom can connect to the board. Since you are using a board with a built in USB-to-Serial adapter you do not need to enter the serial port as it will be detected later.
      • Press ENTER to continue.
    • You will now be prompted for your host IP. This is required to configure u-boot to boot images from your host system. You should take the default IP address.
      • Press ENTER.
    • Now you will select where to obtain the Linux kernel from. In this lab we will be configuring to boot from TFTP.
      • Type 1 and press ENTER.
    • The next prompt will ask you where the root file system should come from. In this lab we will use NFS.
      • Type 1 and press ENTER.
    • You will now be presented with the list of kernel images available in the /tftpboot directory. You should use the default image for your TFTP image of uImage-am335x-evm.bin
      • Press ENTER.
    • You will notified that a Beaglebone/EVM-SK has been detected. Select yes to configure for the EVM-SK .
      • Type y and press ENTER.
    • You will be asked if you would like to reboot the board with these new settings.
      • Press ENTER to reboot the board.
        IMPORTANT

        This script expects the board to NOT be logged in. If you have logged in the board, the reboot will fail. In this case, you can reboot the board manually.
  8. Your target device will now be booting the Linux kernel from the TFTP server on your host machine with an NFS root file system from the targetNFS directory inside of your SDK installation.
    • You can verify that your device is booted from NFS using the command below:
      1. Press ENTER to see the Arago Project prompt and login using root
      2. cat /proc/cmdline you should see the output list the root as /dev/nfs and the nfsroot should be configured to the NFS share you just created.
        NOTE

        You can also use the mount command to verify that your root partition was mounted over NFS.
  9. You system is now configured. You can always re-run the setup.sh script to change your board configuration.
    IMPORTANT

    If you want to reset your u-boot environment back to the default you can do the following in minicom

    1. Login to the board using root
    2. Reboot the board using init 6
    3. When asked to Hit any key to stop autoboot stop the boot process to enter the u-boot prompt.
    4. Reset the default boot environment using env default -f -a
    5. You can now boot the board with the default boot arguments using the boot command.

    These changes will be lost on the next boot. To permanently make changes you should either delete the uEnv.txt file or re-run the setup.sh script.


Working with the Example Applications[edit]

Description[edit]

This lab will show you how to work with the example applications using the Linux command line. We will also explore some of the techniques used in the example applications to make cross compiling easier.

Key Points[edit]

  • Example applications have CCS/Eclipse project files
  • Building example applications from the command line
  • Verifying the executable was built for ARM

Lab Steps[edit]

  1. It is possible to rebuild the individual example applications using Makefiles. For example to rebuild the arm-benchmarks example application, open a Linux terminal and navigate to:
    cd /home/sitara/ti-processor-sdk-linux-<machine>-<version>/example-applications/arm-benchmarks-<version>
  2. Then you can use the following commands:
    make clean
    make
  3. After the build has finished you can verify that the executables were build for the ARM device using the file command.
    file dhrystone/Release/dhrystone
    As we saw earlier the output lists that the dhrystone executable was for an ARM device:
    dhrystone/Release/dhrystone: ELF 32-bit LSB executable, ARM, version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.32, not stripped
  4. The individual benchmarks also have CCS/Eclipse project files in them when can be used to build these projects using CCS. To see these project files do:
    cd dhrystone
    ls -la
  5. You should see files like .cproject and .project listed. These files allow building the dhrystone project using CCS.


Importing Example Applications into CCS[edit]

Description[edit]

This section will cover how you can use the CCS/Eclipse project files seen in the previous section to import the example application projects into CCS and build them. For more information see the Code Composer Studio page.

Key Points[edit]

  • Example applications have existing CCS/Eclipse project files that can be imported.
  • CCSv6 can be used to compile the example applications

Lab Steps[edit]

  1. Launch CCSv6 using the following steps:
    • Double-Click the Code Composer Studio v6 icon on the desktop. You will see a splash screen appear while CCS loads.
      CCSv6 splash.png
    • The next window will be the Workspace Launcher window which will ask you where you want to locate your CCSv6 workspace. Use the default value.
      CCS workspace launcher.png
    • CCS will load the workspace and then launch to the default TI Resource Explorer screen.
      CCS getting started.png
    • Close the TI Resource Explorer screen. This screen is useful when making TI CCS projects which use TI tools. The Processor Linux SDK uses open source tools with the standard Eclipse features and therefore does not use the TI Resource Explorer. You will be left in the Project Explorer default view.
      CCS project explorer.png
  2. From the main CCSv6 window, select File -> Import... menu item to open the import dialog.
  3. Select the General -> Existing Projects into Workspace option.
    CCS import.png
  4. Click Next.
  5. On the Import Projects page click Browse.
    CCS import browse.png
  6. In the file browser window that is opened navigate to the <SDK INSTALL DIR>/example-applications directory and click OK.
    CCS example apps.png
  7. The Projects: list will now be populated with the projects found.
    NOTE

    Uncheck the following projects. They are Qt projects and are imported using a different method. For more information, see the Hands on with QT training.
    • matrix_browser
    • refresh_screen
  8. Select the projects you want to import. The following screen capture shows importing all of the example projects for an ARM-Cortex device, excluding the matrix_browser project.
    CCS example uncheck.png
  9. Click Finish to import all of the selected projects.
  10. You can now see all of the projects listed in the Project Explorer tab.
    CCS projects added.png
  11. In order to build one of the projects use the following steps. For this example we will use the mem-util project.
    • Right-Click on the mem-util project in the Project Explorer.
    • Select the build configuration you want to use.
      • For Release builds: Build Configurations -> Set Active -> Release
      • For Debug builds: Build Configurations -> Set Active -> Debug
    • Select Project -> Build Project to build the highlighted project.
    • Expand the mem-util project and look at the mem_util.elf file in the Debug or Release directory (depending on which build configuration you used). You should see the file marked as an [arm/le] file which means it was compiled for the ARM.
      CCS build memutil.png
    NOTE

    You can use Project -> Build All to build all of the projects in the Project Explorer.


Creating a New CCS Project[edit]

Description[edit]

This section will cover how to make a new project in CCS and cross-compile it for the ARM device. For more information see Code Composer Studio v5 Users Guide.

Key Points[edit]

  • How to create a new cross-compile project
  • How to add sources to the project and build them

Lab Steps[edit]

  1. From the main CCSv6 window, select File -> New -> Project... menu item.
  2. In the Select a wizard window, select the C/C++ -> C Project wizard.
    CCS new project.png
  3. Click Next.
  4. In the C Project dialog set the following values:
    Project Name: helloworld
    Project type: Executable -> Empty Project
    Toolchains: Cross GCC
    CCS C project.png
  5. Click Next.
  6. In the Select Configurations dialog, you can take the default Debug and Release configurations or add/remove more if you want.
    CCS config.png
  7. Click Next.
  8. In the Command dialog set the following values:
    Tool command prefix: arm-linux-gnueabihf-.
    NOTE

    Note the the prefix ends with a "-". This is the prefix of the cross-compiler tools as will be seen when setting the Tool command path.
    Tool command path: /home/sitara/ti-processor-sdk-linux-<machine>-<version>/linux-devkit/sysroots/<Arago Linux>/usr/bin
    Use the Browse.. button to browse to the Sitra Linux SDK installation directory and then to the linux-devkit/sysroots/<Arago Linux>/usr/bin directory. You should see a list of tools such as gcc with the prefix you entered above.
    CCS gcc command.png
  9. Click Finish.
  10. After completing the steps above you should now have a helloworld project in your CCS Project Explorer window, but the project has no sources.
    CCS pe helloworld.png
  11. From the main CCSv6 window select File -> New> Source File menu item.
  12. In the Source File dialog set the Source file: setting to helloworld.c
    CCS new source.png
  13. Click Finish.
  14. After completing the steps above you will have a template helloworld.c file. Add your code to this file like the image below:
    CCS helloworld.png
  15. Compile the helloworld project by selecting Project -> Build Project
  16. The resulting executable can be found in the Debug directory.
    CCS helloworld build.png


Configuring Remote System Explorer (RSE)[edit]

Description[edit]

Now that we have compiled the helloworld project it would be useful to execute the built results on the EVM. Since we are still booted from NFS we could just copy the helloworld executable to the NFS file system, but instead you will learn how to use remote system explorer (RSE) to transfer the file. The actual transfer steps are covered in the next section, but before the transfer can be done RSE must be configured first. For more information, see http://processors.wiki.ti.com/index.php/How_to_setup_Remote_System_Explorer_plug-in

Key Points[edit]

  • Creating a new RSE connection with the target device

Lab Steps[edit]

  1. Open the RSE perspective.
    • Go to Window -> Perspective -> Open Perspective -> Other...
    • CCS Debug Perspective.png
    • In the menu window select Remote System Explorer to open this perspective.
      CCS new RSE.png
    • Click OK.
    • You will now have the RSE view opened.
      CCS RSE view.png
  2. The following steps will create a new RSE connection to your target device.
  3. Click File -> New -> Other...
    • In the Select a wizard window select Remote System Explorer -> Connection.
      CCS new connection.png
    • Click Next.
    • In the Select Remote System Type window select the Linux system type.
      CCS connect linux.png
    • Click Next.
    • In the Remote Linux System Connection window enter.
      Host name: Enter the IP address of your target EVM.
      Connection name: The default value is the same as the host name, but this can be changed to a more human readable value like My Target EVM
      You can un-check Verify host name or leave it checked depending on whether you want to verify the IP address you entered for the Host name field.
      CCS connect host.png
    • Click Next.
    • Check ssh.files to use the Secure Shell protocol for communication
      CCS sshfiles.png
    • Click Next.
    • Check processes.shell.linux to use a shell to work with processes on the remote system.
      CCS processesshelllinux.png
    • Click Next.
    • Check ssh.shells to use Secure Shell to work will shell commands.
      CCS sshshells.png
    • Click Finish.
    • You will now see your EVM configuration in the RSE view.
      CCS EVMconfig.png
  4. When the RSE view was enabled you likely had your C/C++ view closed. In order to get that view back so that you can explore your project perform the following steps
    • Select Window -> Show View -> Other...
    • In the Show View dialog select C/C++ -> C/C++ Projects
      CCS choose C.png
    • Click OK.
    NOTE

    If you do not like the location of the C/C++ Projects view you can drag it to another location in CCS my dragging and dropping the Tab.
  5. You should now be able to switch between the RSE and C/C++ Projects view using the tabs in CCS.
  6. After the New Connection Wizard has been completed and the Remote System Explorer view has been opened, the new connection must be configured to communicate with the target EVM.
    • Right-Click on the My Target EVM node and select Properties from the context menu.
    • In the Properties window click on Host.
    • Change the Default User ID: to root
      CCS RSE properties.png
    • Click OK.
  7. The Remote System Explorer is now ready for use. The first time the target EVM file system is booted a private key and a public key is created in the target file system. Before connecting to the target EVM the first time, the public key must be exported from the target EVM to the Linux host system. To configure the key do
    • Right-Click the My Target EVM node and select Connect.
    • If you are prompted for a password, leave it blank.
      CCS RSE password.png
    • Click OK.
    • A dialog like the one shown below may appear. Click Yes to accept the key.
      CCS RSA key.png
    • If prompted that /home/sitara/.ssh/known_hosts does not exist select Yes to the dialog boxes.



Transferring Files with RSE[edit]

Description[edit]

Now that the RSE connection to your target device has been configured you can use RSE to transfer files to the target system. In this section we will cover how to transfer the helloworld executable with RSE. In later sections we will learn how to use RSE with the CCSv6 debugging capability to automatically transfer the executables.

Key Points[edit]

  • RSE can be used to transfer files between the host and the target device
  • RSE can open terminals on the target device to allow running the executables

Lab Steps[edit]

  1. Switch back to the RSE view.
  2. Open Sftp Files -> Root -> /home -> root.
    CCS sftp root.png
  3. Switch to the C/C++ view using the tab. Expand helloworld to find the helloworld executable in the Debug directory.
    CCS helloworld executable.png
  4. Right-Click the helloworld executable and select Copy .
  5. Switch back to the RSE view and Right-Click on the root directory and select Paste .
  6. You should now have the helloworld executable transferred to your target device.
    CCS helloworld paste.png
  7. In order to execute the helloworld binary that was just transferred you need to open a terminal to the target device. Or, you could use some other terminal/console (i.e. Teraterm, minicom, etc.). Since CCS provides one built right in, let's use that one. The following steps will cover opening a new terminal to the target device.
    • Click on the "Open Terminal" icon on the toolbar:
      Hands On open terminal.png
    • Use the below settings to configure the terminal (make sure to use your target's IP Address):
      Hands On terminal settings.png
    • A terminal window will now be open:
      CCS launch terminal.png
  8. To run your helloworld application use the following commands in the terminal window:
    chmod +x helloworld
    ./helloworld
    CCS helloworld output.png
    • It is also possible to make a file executable using RSE by right-clicking the file in the RSE view and selecting Properties -> Permissions and enabling the Execute permission.
    Sitara-linux-training-rse-executable.png
    • Click Apply.



Debugging with CCS and GDB[edit]

Description[edit]

Now that you have learned to use CCS to create a project, build your sources for the ARM, transfer the executable to the target, and run that executable it would be useful to know what to do if there is something wrong with the executable. In this section you will learn how to configure CCS to debug the helloworld application.

Key Points[edit]

  • CCS can be configured to automatically build your project files.
  • RSE is useful for transferring files between the debug host and the target.
  • CCS has a terminal that can be used to run commands on the target, including starting gdbserver.
  • You can use break points to stop execution at a particular point.



Lab Steps[edit]

  1. First, start gdbserver on the target using the terminal in CCS:
    The command is gdbserver :10000 helloworld
    Hands On terminal start gdbserver.png
  2. Switch to the C/C++ Project view
  3. Right-Click the Debug/helloworld executable and select Debug As -> Debug Configurations...
    Hands On debug as configurations.png
  4. Right-Click C/C++ Remote Application and select New.
    CCS debug new.png
  5. By default you will have a helloworld configuration created. Change the Name to helloworld Debug.
    CCS helloworld change.png
  6. On the Main tab, add the Remote Absolute File Path to point to /home/root/helloworld. If the Connection is selected as Local, change it to My Target EVM
    CCS helloworld filepath.png
  7. Switch to the Debugger tab and modify the following settings:
    • GDB debugger: /home/sitara/ti-processor-sdk-linux-<machine>-<version>/linux-devkit/sysroots/<Arago Linux>/usr/bin/arm-linux-gnueabihf-gdb
      GDB command file: ti-processor-sdk-linux-<machine>-<version>/.gdbinit
    NOTE

    If you use the file browser, you will need to Right-Click and select Show hidden files to find the .gdbinit file.
    CCS debug gdb.png
  8. Now click on "Select Other..." next to Using GDB (DSF).
    CCS debug config select other.png
  9. Select the "manual configuration"
    CCS Hands on switch manual.png
  10. On the "connection" tab, set the server IP address:
    CCS gdb server IP.png
  11. Click Apply.
  12. Click Debug to compile the project and start the debug. You system should be halted at the first line of the main function. You can now use the controls on the top of the window to control the debug session.
    CCS debug controls.png
  13. Click on the Step Over button. You should see the active line move to the return 0 line and the Hello World message should be printed in the console output.
    CCS debug stepover.png
  14. Click the Resume button to finish execution and exit the program.
  15. Use the terminal to restart gdbserver on the target (it exited when the program finished running):
    Hands on relaunch gdbserver.png
  16. Now select Remote System Explorer in the upper-right corner of the window to leave the debugger view.
    CCS debug RSE.png
  17. Edit the helloworld.c file like the image shown below to add another printf line.
    CCS helloworld anotherline.png
  18. Right click on the grey column to the left of the new line and select Toggle Breakpoint.
    CCS toggle breakpoint.png
  19. Click the arrow next to the bug icon in the top toolbar and select the 1 helloworld Debug configuration.
    CCS debug button.png
  20. When prompted to save your changed to helloworld.c select OK.
    CCS save launch.png
  21. You will see the sources get compiled and the debug view will open automatically. Once again the current location will be the first line in the main function, but this time there will be a breakpoint shown in the sources as well. Don't forget to copy the executable to the target using RSE. Look back in the lab for a reminder, if needed.
    CCS breakpoint1.png
  22. Click the Run icon and notice that the program automatically stops at the breakpoint. The console output should say Hello World from Sitara!
    CCS breakpoint2.png
  23. Click the Step Over icon and notice that the second printf line which was just added is now executed, so the program on the target file system was updated with your changes.
    CCS breakpoint3.png
  24. You can now stop the debugger by pressing the Stop button.
  25. To restart the debugger click the Bug icon on the top toolbar to relaunch the application for debug.

Navigation[edit]

Return to Processor SDK Linux Software Developer’s Guide for additional information.


Archived Versions[edit]

E2e.jpg {{
  1. switchcategory:MultiCore=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article Sitara Linux Training: Hands on with the SDK here.

Keystone=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article Sitara Linux Training: Hands on with the SDK here.

C2000=For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article Sitara Linux Training: Hands on with the SDK here. DaVinci=For technical support on DaVincoplease post your questions on The DaVinci Forum. Please post only comments about the article Sitara Linux Training: Hands on with the SDK here. MSP430=For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article Sitara Linux Training: Hands on with the SDK here. OMAP35x=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article Sitara Linux Training: Hands on with the SDK here. OMAPL1=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article Sitara Linux Training: Hands on with the SDK here. MAVRK=For technical support on MAVRK please post your questions on The MAVRK Toolbox Forum. Please post only comments about the article Sitara Linux Training: Hands on with the SDK here. For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Sitara Linux Training: Hands on with the SDK here.

}}

Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity

{{#switchcategory:MSP430=<McuHitboxFooter/>|C2000=<McuHitboxFooter/>|Stellaris=<McuHitboxFooter/>|TMS570=<McuHitboxFooter/>|MCU=<McuHitboxFooter/>|MAVRK=<MAVRKHitboxFooter/>|<HitboxFooter/>}}