NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

StarterWare LIDD

From Texas Instruments Wiki
Jump to: navigation, search
{{#switchcategory:MSP430=<McuHitboxHeader/>|C2000=<McuHitboxHeader/>|Stellaris=<McuHitboxHeader/>|TMS570=<McuHitboxHeader/>|MCU=<McuHitboxHeader/>|MAVRK=<MAVRKHitboxHeader/>|<HitboxHeader/>}}

Introduction[edit]

The LCDC peripheral can be configured to operate in LIDD mode and interface with character displays to output ASCII characters or messages. The LCDC peripheral cannot operate in LIDD mode and raster mode simultaneously, so only one type of display can be used at a time.

Programming Sequence[edit]

  • Setup pin multiplexing for the LCDC peripheral in LIDD mode. This is done using the LIDDPinMuxSetup() API.
  • The Character LCD interfacing lines are muxed on the EVM with various other peripherals like the VPIF, ADC/DAC, Ethernet etc. Thus the on board mux TCA6416 needs to be configured to route the LCD lines to the character LCD. This, since is platform (EVM) dependent is abstracted in function LIDDDisplayEnable() in the platform library.
  • The clock for the LIDD needs to be configured so as to generate a proper ENABLE signal for the character LCD. This is done using the LIDDClkConfig() API.
  • Select LIDD mode to drive the character LCD. This is done using the LIDDModeSet() API.
  • Setup strobe timing parameters as required by the character LCD using the LIDDCSTimingConfig() API.
  • The character LCD needs to initialized with a series of commands (detailed in the character LCD manual). This command sequence series can be executed using the DisplayControlValueWrite() API.
  • Once the character LCD is initialized, messages can be displayed by calling LIDDDataWrite().
E2e.jpg {{
  1. switchcategory:MultiCore=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article StarterWare LIDD here.

Keystone=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article StarterWare LIDD here.

C2000=For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article StarterWare LIDD here. DaVinci=For technical support on DaVincoplease post your questions on The DaVinci Forum. Please post only comments about the article StarterWare LIDD here. MSP430=For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article StarterWare LIDD here. OMAP35x=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article StarterWare LIDD here. OMAPL1=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article StarterWare LIDD here. MAVRK=For technical support on MAVRK please post your questions on The MAVRK Toolbox Forum. Please post only comments about the article StarterWare LIDD here. For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article StarterWare LIDD here.

}}

Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity

{{#switchcategory:MSP430=<McuHitboxFooter/>|C2000=<McuHitboxFooter/>|Stellaris=<McuHitboxFooter/>|TMS570=<McuHitboxFooter/>|MCU=<McuHitboxFooter/>|MAVRK=<MAVRKHitboxFooter/>|<HitboxFooter/>}}