NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

SystemAnalyzerTutorial8

From Texas Instruments Wiki
Jump to: navigation, search

System Analyzer Tutorial 8: Monitoring Activity on Keystone Architecture Devices

Tutorial8 Keystone.gif

An important use of System Analyzer is to monitor the performance of the various subsystems that are involved in moving data around a device. In Keystone Architecture devices, some of the key subsystems that are involved are:

  • EDMA3: the DMA engine
  • EMIF: the External Memory Interface
  • MSMC: the Multicore Shared Memory Controller


Tutorial topics: In Tutorial 8, we will work through some examples that cover the following topics:

  • Tutorial 8A: Using UIA to monitor EDMA3 transactions
  • Tutorial 8B: Periodically logging Performance Monitoring Counters

Links