NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

Talk:AM35x-OMAP35x-PSP 03.00.00.05 UserGuide

From Texas Instruments Wiki
Jump to: navigation, search
For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article AM35x-OMAP35x-PSP 03.00.00.05 UserGuide here.

Comments on AM35x-OMAP35x-PSP 03.00.00.05 UserGuide


Prashantha said ...

In the section boot from MMC, When kernel image and filesystem (ramdisk) are available on the MMC card, the load address for ramdisk is set to 0x80000000. With this, it will overwrite the uImage. So the address can be 0x82000000 as below:

fatload mmc 0 0x82000000 ramdisk.gz


--Prashantha 08:51, 18 March 2011 (CDT)