NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

Talk:BIOS MCSDK 2.0 Getting Started Guide

From Texas Instruments Wiki
Jump to: navigation, search

Comments on BIOS MCSDK 2.0 Getting Started Guide


Gautamsridhar said ...

There is conflicting information about setting up DHCP / Static IP configuration. The "TMDXEVM6678L EVM Hardware Setup" http://processors.wiki.ti.com/index.php/TMDXEVM6678L_EVM_Hardware_Setup) indicates User switch 2 on SW9 needs to be changed - not "user switch 1"


--Gautamsridhar 14:19, 10 August 2011 (CDT)

AravindBatni said ...

Gautam, Thanks for the input. We updated the Getting Started Guide and the EVM Hardware Setup Guide and fixed this conflicting information.

--AravindBatni 09:46, 11 August 2011 (CDT)

Aymeric Dupont said ...

I struggled to get my board started even though this manual is very good. There is one step that is not required (use jtag to load the application, step 1). What is most important is that, after connecting to the core, run a CPU reset and/or system reset. After this reset, we can run the gel file and load the program. The board boots. Still have an error running the gel file but this is another story.


--Aymeric Dupont 12:22, 20 September 2012 (CDT)

Csmith said ...

Aymeric, that step, use JTAG to load application step 1, is required. The DIP switches along the side of the board need to be set to NO BOOT per the Hardware Setup Guide of your particular board or connecting via CCS will cause some issues. This might also be why it is necessary for you to reset (something you should not have to do).

Please make sure you are in NO BOOT and try the guide again.

--Casey Smith 15:18, 20 September 2012 (CDT)