NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

Talk:BIOS MCSDK 2.0 User Guide

From Texas Instruments Wiki
Jump to: navigation, search

Comments on BIOS MCSDK 2.0 User Guide


Bharath374 said ...

The steps in section 5.3.2 "Example 2 - Building and running your first tasking application using MCSDK and BIOS" do not seem to work as is. I do not see the "Empty RTSC Project" in the Project Templates screen. I am currently using CCS 5.0.3.0028 and mcsdk_2_00_01_12. Any idea? I remember that the correct option was available in CCS 5.0.2.

--BRY 02:40, 16 August 2011 (CDT)

AravindBatni said ...

Bharath, Thanks for the inputs. I moved this question to the forum http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/129233/462812.aspx#462812

to track this - and we are looking into this now.

--AravindBatni 10:36, 18 August 2011 (CDT)

Andrewp said ...

This page is really large (~200K), and takes a fair amount of time to load/render. Any chance it could be broken up into multiple pages?

--AMP 13:03, 31 January 2012 (CST)