NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

Talk:Grace Quick Start Guide

From Texas Instruments Wiki
Jump to: navigation, search

Comments on Grace Quick Start Guide


Scbrass said ...

This is a good idea, I have been using something similar for the SiLabs 80C51 for years. However theirs is a stand alone program that can be used with any IDE. Are there any plans to support other IDE's such as IAR Workbench? - Steve

--Scbrass 17:09, 29 August 2011 (CDT)

Mikemyti said ...

When will Grace support FRAM devices?


--Mikemyti 00:10, 30 August 2011 (CDT)

Jlschuck said ...

Really sucks Grace only supports a few devices. What about users who need to learn the 55 series?

--Jlschuck 21:24, 12 July 2012 (CDT)

Shanyi said ...

Please give us a roadmap for supporting the whole family of MSP430 devices. I'm working with the F5438A at the moment, but in general I'd like to know when we will be able to use grace in CCSv5 for all of them.

--Shanyi 09:03, 22 August 2012 (CDT)

HI said ...

I was using Grace on G2453 processor and configured as Active Mode on Port2 Intr Exit. The corresponding code generated for this is putting the processor in LPM4.

__bic_SR_register_on_exit(LPM4_bits);

--HI 05:25, 8 October 2012 (CDT)