NOTICE: The Processors Wiki will End-of-Life in December of 2020. It is recommended to download any files or other content you may need that are hosted on processors.wiki.ti.com. The site is now set to read only.

Talk:ITBOK

From Texas Instruments Wiki
Jump to: navigation, search

I have U-Boot 1.1.4 (May 2 2008) and there is no "diag" or itbok command. The response unknown command for both. Are these tests available? If so how do I run them?

DavidMeixner said ...

Is there ITBOK source for AM35xx?

--DavidMeixner 15:29, 23 February 2010 (CST)

Nssriharsha61 said ...

ITBOK source - AM35xx is available and is due for release with SDK.

--Nssriharsha61 07:18, 6 May 2010 (CDT)

Nssriharsha said ...

The U-Boot which you are using may not be having ITBOK Code inbuilt. Please try with the file "itbok.bin"(itbok integrated with u-boot) which is under "board_utilities/OMAP35x/" directory in PSP 1.0.2 release.

--Nssriharsha 02:01, 19 May 2010 (CDT)

Annie said ...

I did exactly what it said here to rebuild itbok but I got error complaining undefined reference to omap_nand_switch_cc in u-boot/cpu/arm_cortexa8/omap3/board.c. Either the steps are not accurate or something is missing from my build which was not mentioned here. Has anyone rebuild itbok on Red Hat with codesourcery toolchain?

--Annie 08:49, 16 September 2010 (CDT)