Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS BOOT K2H/E/L

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide BOOT K2H/E/L



Overview

User Interface

Application

Debug


Overview

K2H/K2E/K2L EVMs uses the Secondary Boot Loader (SBL) to configure board-related settings and execute a user application. The user application can be single core or multicore, and execute on either DSP cores or ARM cores. The only restriction is that the load sections must not overlap the memory space that SBL uses.

The K2H/K2E/K2L SBL supports ARM master boot using SPI NOR. Please refer to the boot mode dip switch settings in the respective EVM hardware page (link) to configure your EVM for NOR boot.

Flashing the Bootloader

SBL and user application needs to be flashed into SPI NOR.

Refer to Program EVM Guide for instructions on using the script, program_evm.js, to automatically flash your device.

Usage

  1. Flash the bootloader and user application. This can be done automatically with default files by using program_evm.js
  2. Set the EVM to ARM SPI boot mode
  3. Connect UART serial debug cable from EVM to your computer. Open a terminal such as HyperTerminal or TeraTerm to see console output
  4. Power on the EVM

Compilation

The recommended rule-of-thumb to compiling projects in the Processor SDK RTOS package is to use the makefiles provided. The makefiles are usable after setting up your shell/terminal/command prompt environment with the setupenv.bat or setupenv.sh script located in

 [SDK Install Path]/processor_sdk_rtos_<platform>_<version>

Refer to Building RTOS SDK page on how to setup your environment for building within any of the Processor SDK RTOS packages.

The SBL package can be found in:

 [SDK Install Path]/pdk_<platform>_<version>/packages/ti/boot/sbl

To build:

 cd [SDK Install Path]/pdk_<platform>_<version>/packages/ti/boot/sbl
 make all BOOTMODE=spi BOARD=<EVM> SOC=<platform>

<EVM> can be of values: evmK2H, evmK2E, evmK2L, or evmK2K

<platform> can be of values: K2H, K2E, K2L, or K2K

The resulting output will be in [SDK Install Path]/pdk_<platform>_<version>/packages/ti/boot/sbl/binary/<platform>/spi/bin directory.

Making Loadable User Application image (app)

For converting the compiled .out files to a format loadable by TI's Secondary Boot Loader (SBL), you must follow these two steps:

  1. out2rprc.exe [.out file] [rprc output]
  2. MulticoreImageGen.exe LE 55 [output name] 0 [rprc output]

Out2rprc.exe and MulticoreImageGen.exe are tools supplied by TI and can be located in the <PDK_INSTALL_DIR>/packages/ti/boot/sbl/tools folder. "rprc output" can be any spare name of your choosing. "output name" can also be any name of your choosing.

The '0' used in step 2 refers to the Core ID to boot. By default, '0' is MPU (Cortex A15) core 0. You can input a different value to boot to other cores. Valid values are:

K2H K2E K2L
Core Value Core Value Core Value
MPU Core 0 0 MPU Core 0 0 MPU Core 0 0
MPU Core 1 1 MPU Core 1 1 MPU Core 1 1
MPU Core 2 2 MPU Core 2 2 MPU SMP 4
MPU Core 3 3 MPU Core 3 3 DSP Core 0 5
MPU SMP 4 MPU SMP 4 DSP Core 1 6
DSP Core 0 5 DSP Core 0 5 DSP Core 2 7
DSP Core 1 6 DSP Core 3 8
DSP Core 2 7
DSP Core 3 8
DSP Core 4 9
DSP Core 5 10
DSP Core 6 11
DSP Core 7 12

If MPU SMP is chosen, the same boot image and entry will be used for all MPU cores. SBL can also parse multiple boot images that are concatenated together. Simply use MulticoreImageGen as such:

MulticoreImageGen.exe LE 55 [output name] [Core ID a] [rprc output a] [Core ID b] [rprc output b] [Core ID c] [rprc output c] ...

Flash Writers

SPI Writer

The SPI flash writer, spi_flash_writer.out, is a part of the SBL package and allows users to flash multiple images at different offsets into the board's SPI NOR flash memory.

Compilation

 cd [SDK Install Path]/pdk_<platform>_<version>/packages/ti/boot/sbl/
 make spi_flashwriter BOARD=<EVM> SOC=<platform>

The binary output will be at:

 [SDK Install Path]/pdk_<platform>_<version>/packages/ti/boot/sbl/tools/flashWriter/spi/bin/<platform>

Usage

  1. Copy the binaries that you want to flash to: [SDK Install Path]/pdk_<platform>_<version>/packages/ti/boot/sbl/tools/flashWriter/spi/bin/<platform>
  2. In that same directory, there is a file named config. Edit that file such that each line has 2 parameters: [name of binary to flash] [SPI NOR offset to flash to]
  3. Set your EVM to NO BOOT. Power on, launch target configuration in CCS, and connect to DSP Core 0
  4. Load and run [SDK Install Path]/pdk_<platform>_<version>/packages/ti/boot/sbl/tools/flashWriter/spi/bin/<platform>/spi_flash_writer.out
  5. You should see the flash progress output on UART terminal


Boot Example

Below is an example output of evmK2H booting after having images flashed in by program_evm.js:

**** PDK SBL ****
Boot succesful!
Begin parsing user application
Jumping to user application...


TMDXEVM6636K2H POST Version 01.00.00.08
------------------------------------------
SOC Information

BMC Version: 0000
EFUSE MAC ID is: B4 99 4C B6 E2 5B
SA is enabled on this board.
PLL Reset Type Status Register: 0x00000001
Platform init return code: 0x00000000

Power On Self Test

POST running in progress ...
POST I2C EEPROM read test started!
POST I2C EEPROM read test passed!
POST SPI NOR read test started!
POST SPI NOR read test passed!
POST EMIF16 NAND read test started!
POST EMIF16 NAND read test passed!
POST external memory test started!
POST external memory test passed!
POST done successfully!

POST result: PASS